New Features in CoMo Injection Process Monitoring System Make 100 % Injection Molding Quality Even Easier to Achieve

Kistler brings the quality-minded injection molder another substantial step closer to zero-defect production. The CoMo Injection Type 2869B… process monitoring system now offers many useful functions for faster production startups, even more efficient quality monitoring and – absolutely new – automatic quality prediction.


Automatic Online Prediction of Part Quality

The outstanding feature of the CoMo Injection system is the new module for automatic online prediction of part quality. Based on mold cavity pressure, contact pressure and process models, specific quality attributes of the part currently being produced are forecast. As early as the manufacturing stage, the CoMo Injection system with this new module predicts attributes such as the final dimensions of the molded part. This makes it possible to state during molding whether these dimensions will still be within tolerance when the part is actually used.

Manufacturers of injection molded parts can now take tolerance bands straight from the parts specification as criteria for the process monitoring system. Manufacturers of high-quality, hard-to-assemble or sensitive medical and other precision parts will profit most from this.

Monitoring Multicavity Molds and Automatic Mold Identification

When changing molds, the new automatic mold identification system simplifies and speeds up connection and setting up by automatically loading the mold and article data. It also makes it easier to detect connection mistakes.

Several CoMo Injection systems can now be cascaded to monitor multi-cavity molds with up to 64 cavities. Up to 33 digital outputs supply signals for part separation, alarms or switching. Setting up and visualization of all of the systems is performed by defining one as master then proceeding in the way familiar from a single system.

More Efficient Changeover with Mold Cavity Pressure

Retracing reference curves determined with parts of optimum quality guarantees rapid startup or resumption of production of high-grade products. This enables current production to be easily matched to the displayed reference curve. The reference curve can be read from the mold record or the database (CoMo DataCenter Type 2829B…), or obtained from cycles of "OK" parts of the current process.

New curve history functions enable scrolling through the last 3 000 cycles. Curve superimposition and a series of useful functions allow initial evaluation in the CoMo Injection system right at the injection molding machine.

The CoMo Injection system now has production control functions based on selectable criteria. This enables runs to be limited to a specified quantity of good parts, or stopped on the basis of certain criteria in the event of ongoing quality problems or process instabilities.

Simpler, Faster Operation

The CoMo Injection system can now be operated more quickly and easily. Visualization on the 12,1" color touch screen has been enhanced by dividing the display into two views, with the option of hiding or displaying individual channels. The cavity pressure curve can now be followed in real time, with the new zoom function making it possible to focus on critical sections. Quick links guide the user to frequently required pages.

Background: Quality Assurance with Mold Cavity Pressure

The cavity pressure curve is regarded as a fingerprint of the injection molding process. It is the most meaningful characteristic for evaluating part quality. Deviations from the optimum curve are clear indications of process fluctuations leading to part defects. These issues range from incomplete mold filling to flashing or dimensional discrepancies.

As the supplier with the largest and widest range of sensors for all methods of injection molding, simple connection technology and user-friendly, networkable systems, Kistler is the only manufacturer to offer the tools for integrated monitoring of this process from a single source. The group is the world's leading manufacturer of pressure and temperature sensors for use in the plastics processing industry.

Discover how Kistler contributes to face the great challenges of our times.
德国纽伦堡举办的SPS IPC Drives大会上,奇石乐首次展示了分析螺栓装配的实验室系统、扭矩工具的校准设备和测试系统,以及随机抽样测试的测量系统。
Discover our latest Kistler News online.
The latest issue of Kistler News is now online.
我们的产品和系统可以测量人类器官感觉不到的微小物理变化。这意味着我们关注的焦点是非常小的细节 – 因为重大成就总是始于一个小的开端。
Kistler Japan Celebrates its 30th Anniversary and Thanks Its Loyal Customers.
NCFR Joining Module Honored at Motek for Best Handling and Assembly
The latest issue of Kistler News is now online.
Download KiBox Cockpit V2.1 for free and discover new features.
Seminar zur Qualitätssicherung in der industriellen Fertigung – jetzt anmelden.
Kistler Automotive GmbH honored as one of Germany's most innovative companies
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...
A fascinating TV report on the trendy sport ‘Parkour’ – with Kistler force plates playing a hidden but...
Kistler partners with OEMs and keeps the finger on the pulse of Industry 4.0
奇石乐将于2015 SIAF展会上展出maXYmos系列高级版产品
Wide range of options for optimizing the quality assurance through documenting and evaluating production data...
Users obtain a full range of force–displacement measurement systems from one source
At Motek 2014 Kistler will be presenting advanced versions of its proven maXYmos product family
Extending the maXYmos product range to control and monitor production processes and quality assurance
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in...
Users obtain a full range of force–displacement measurement systems from one source
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with...
Dr.-Ing. Oliver Schnerr, Head of Sales of the Industrial Process Control (IPC) division, hands over the...
From flexible torque sensors to complete test stands for highly-efficient electric drives
1 mm pressure sensor Type 6183C with a new design
Monitoring, open- and closed-loop control of RTM and SMC processes
New longitudinal measuring pin for non-contact cavity pressure measuring
Kistler Goes Beyond Limits: Acceleration sensors for heavy-duty applications at the SENSOR+TEST 2013
Kistler Goes Beyond Limits: High-tech sensors for heavy-duty applications at the SENSOR+TEST 2013
In 2012, the Kistler Group reached a record turnover of 279 million Swiss francs with an increase in turnover...
Kistler Group, a leading global provider of sensors for measuring pressure, force, torque and acceleration,...
Kistler präsentiert auf der Fachmesse SPS/IPC/DRIVES in Nürnberg (24. bis 26. November 2012) am Stand 4A-451...
At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012), Kistler will present a...
At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012) Kistler will present its...
The new firmware upgrade V2.4 for Kistler's CoMo Injection process monitoring system offers better...
Kistler Group continues to expand: revenues up 20 %, strengthening of customer-specific development capacities...
Kistler Gruppe weiterhin auf Expansionskurs: Umsatzsteigerung um 20 %, Stärkung der kundenspezifischen...
With the acquisition of the DTI Technology ("Digital Transducer Interface") from Hentschel System GmbH,...
Mit dem Erwerb der DTI-Technologie ("Digital Transducer Interface") von der Hentschel System GmbH, Hannover,...
At the Automatica Trade Fair, which will take place from 22 through 24 May, 2012 in Munich/Germany, Kistler...
Kistler sensors and systems deliver an impressive performance where products from other suppliers come to...
CIRP focuses on cutting because this method of machining components is one of the key production processes.
In-process quality assurance solutions made by Kistler Group have proven their high efficiency for...
Despite difficult conditions, with sales growth over 11 % Kistler still achieved a sound result in 2011.
On Stand 4A-451 in Hall 4A of the SPS/IPC/DRIVES exhibition from 22 to 24 November 2011 in Nuremberg, Kistler...
By designing a measuring unit and an evaluation unit as separate assemblies, and introducing modular...
This year's Fakuma sees Kistler showing a system for online prediction of the quality of injection molded...
Kistler brings the quality-minded injection molder another substantial step closer to zero-defect production.
As an XY monitor for process monitoring and product testing, the maXYmos BL Type 5867A… from Kistler has...
Telemetric transmission of the force signal without having to rely on a cable, and suitability for use in...
Kistler is expanding its selection of electromechanical NC joining modules NCFB Type 2160A… with versions...
The Kistler Group based in Winterthur, Switzerland, looks back on a successful 2010 financial year with sales...
Kistler, worldwide supplier of precision sensors, systems and instrumentation for the dynamic measurement of...
Kistler, worldwide supplier of precision sensors, systems and instrumentation for the dynamic measurement of...
Kistler's new generation of triaxial PiezoBeam® accelerometer Type 8688A(x) offers best-in-class sensitivity...
Swiss company Kistler Instrumente AG of Winterthur is the leading international supplier of sensors and...
The new press force sensor Type 9393A… extends the successful Press Force series of sensors to a measuring...
With the new combined pressure and temperature sensor Type 6188A… Kistler establishes another milestone in the...
Kistler has developed its new data acquisition (DAQ) system Type 5697A… for recording data in R&D laboratory...
Kistler has commissioned an additional calibration unit for torque sensors on its Lorch production site.
As a development partner of the automobile industry the Kistler Group aims to provide vehicle manufacturers...
The Kistler Group has been awarded the contract for instrumentation of three crash centers for the Indian...
In order to optimise processes inside an engine, it is extremely important to have a true picture of the...
New Type 4520A... Basic Line provides a cost-effective torque sensor based upon strain gage technology.
The well established Kistler press force sensors are based on the piezoelectric measuring principle.
Successful automation of joining processes where room is at a premium and joining stations closely spaced...
The Kistler Group acquired KT Automotive GmbH based in Munich, Germany, in an all-stock transaction on 22...
The curve of cavity pressure during injection molding is the critical process variable for evaluating part...
To allow direct incorporation of Kistler products into CAD designs, the Kistler CAD Download Service offers...
The Kistler Group has acquired Corrsys-Datron Sensorsysteme GmbH based in Wetzlar, Germany, in an all-stock...
The roll-out of the world's first measuring tram took place in Dresden, Germany, on 5 March with the handover...
The Kistler Group took over MSC Automotive GmbH based in Schwieberdingen, Germany, in an all-stock transaction...