最小的水冷式微型气缸压力传感器——奇石乐推出了升级版本

温特图尔,2022年1月 - 奇石乐推出最新的 M8微型气缸压力传感器(6041C)在卓越的测量领域取得了新的突破。该传感器采用了最先进的PiezoStar石英,并对其设计和制造工艺进行了改进,从而实现了卓越的性能。这种多功能、可靠的气缸压力传感器提供了无与伦比的测量精度——可视作发动机开发过程中热力学动态研究的首选方案,所有测量数据的精确度是最为重要的。

最近几十年来,内燃机的发展不断取得进展——由于测量技术的重大进步,在提高性能和降低排放方面发挥了至关重要的作用。内燃机将在之后的许多年里保持在未来动力传动概念中的地位,但新的替代燃料将对发动机开发者提出挑战。奇石乐的对策是:提供高度优化的传感器链,为发动机的开发过程提供最优的技术方案。

突出的测量特性

奇石乐是测量技术领域的领导者——尤其是在燃烧压力测量和分析方面。6041C微型气缸压力传感器——奇石乐最小的水冷式传感器(尺寸:M8)随着第三代产品的上市证实了这一定位。6041C将优化后的热力学表现与更好的稳定性和最小的传感器之间的误差结合起来。在与测量有关的技术参数方面,新传感器的主要特点是:

  • 最小的热灵敏度差异——能保持在整个工作范围内的稳定
  • 极小的线性偏差——在所有负荷下都能提供准确的测量数据
  • 极低的热冲击误差——在所有发动机工况下保证平均有效压力(MEP)的准确性
  • 长期稳定性——取决于测量元件周围优化过的冷却通道
  • 使用寿命长——不损失热力学精度

适用于各种应用的可靠传感器

与非水冷的传感器相比,水冷式传感器的优势在于,即使在承受高热负荷的工况下,它们也可以齐平安装,因此可以提供最高精度的测量结果。这是由于采用了最新的PiezoStar石英技术和先进的测量元件,再加上生产工艺的优化,这些优化改进使6041C微型气缸压力传感器工作在50±30°C的应用温度范围内具有更高的固有频率和出色的热稳定性,因此该传感器对换气分析可进行优化。

该传感器可安装在适配套中或直接安装在M8x0.75的孔中,可齐平安装或后缩安装。跟之前版本一样,6041C气缸压力传感器不需要过多的空间,可以安装在直径为12mm及以上的孔中。该传感器与其之前版本6041B和6041A,以及非冷却型6045A、6045B和6044A兼容安装。6041C与安装电缆一同交付,同时智能传感器可选。

为发动机开发商提供极高的精度

奇石乐压电式气缸压力传感器产品经理 Roger Leutwyler 评论道:"高灵敏度、高固有频率、低热冲击误差和突出的零点稳定性:这些优势使奇石乐新型6041C气缸压力传感器能够提供具有极高精度的测量结果。作为一个带有M8安装螺纹的微型传感器,它特别适用于空间有限的紧凑型多气门发动机——当然,测量精度和长期稳定性是传感器的关键因素。”
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.