Quattro Jump with Unique Performance Diagnostics Software

Winterthur, 15 September 2015 – The portable force measurement system Kistler Quattro Jump now supports the proprietary performance diagnostics software Kistler MARS. The software, which has been specially developed for Quattro Jump, enables the analysis and evaluation of performance and force for vertical jumps. The eight pre-defined analysis modules make it possible to evaluate measurements in just a few seconds and to display all relevant performance parameters at a glance. Kistler has thus expanded the tried and tested force plate into an integrated, attractively priced performance diagnostics system, making broad application in fitness clubs, performance centers and rehabilitation centers possible. Kistler Quattro Jump with MARS is available as from now.

Quattro Jump with Kistler MARS 2.1
In June, Kistler presented an extensive update of the proprietary Kistler MARS 2.1 Measurement, Analysis and Reporting Software for Kistler force plates. The software is now also supported by Kistler Quattro Jump. The portable force measurement system provides numerous innovations for performance diagnostics in sport and rehabilitation, for example, in the evaluation of drop jumps. ‘Our goal is to make piezoelectric measurement technology, which is outstanding because of its great robustness and accuracy, available to a broad group of users,’ says Florian Ullrich, manager of Kistler’s Biomechanics Business Field. ‘With Kistler MARS, Quattro Jump is now an integrated, attractively priced performance diagnostic system which can be used in many situations where, up until now, high-end technology was prohibitive simply because of the cost.’ 

Versatile Application in Performance Sports and Rehabilitation
Quattro Jump with Kistler MARS is targeted for performance coaches, team physiotherapists as well as fitness and rehab trainers who need to objectively determine the exact condition of their athletes. The portable force measurement system delivers a quick overview of all the relevant performance parameters of the legs. This makes it possible, for instance, to specifically control particular training or regeneration phases so that individual development phases can be reached more quickly. With a USB interface, which replaces the serial interface used up until now, Quattro Jump can be connected more easily than ever.

Eight Predefined Analysis Modules
The focus of the eight predefined analysis modules (i.e. Counter Movement Jump or Stamping) is on the analysis of force and endurance. The software delivers all relevant performance parameters within just a few seconds. This helps athletes train to their optimal level and avoid injury. Frequent and efficient performance tests give coaches and physiotherapists a good overview of the current performance capability of their athletes.

Easy Output of Desired Performance Parameters
The input parameters and data acquisition setup can be edited for each test separately. Data from projects, test persons and measurements are edited, structured and saved to a database using the management tool. Here, they are available for comparisons and reports. Extensive information and examples can be found in the Kistler MARS software help while online video trainings are available from the support website.

Collaboration with Leading Institutions in Biomechanics
The Windows-based software Kistler MARS has been developed in close collaboration with leading international institutions for biomechanics and extensively tested in practice using Quattro Jump. Kistler MARS for Quattro Jump is also available as a software upgrade for older Kistler Quattro Jump systems with USB (Type 9290BD).

You can find out more about the Kistler performance measurement solutions at www.kistler.com/biomechanics.

Download Press Release PDF

The following pictures can be downloaded in high resolution here.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.