奇石乐压电式加速度计更精确地测量微振动

温特图尔,2022年7月 - 奇石乐最成功的三轴加速度计8763B得到了进一步改进,其所有范围的噪声阈值都明显降低。得益于测试程序的优化,阈值降低了58%,这使得微振动监测的测量更加精确。工艺的改进带来更短的制造时间和更高的库存水平——从而缩短交货时间。

测量微振动在许多工程应用中是必不可缺的:准确的GPS数据取决于稳定的太空飞船和卫星,而汽车开发商需要NVH测试(噪声、振动和平顺性)来优化驾驶舒适度、车辆性能、耐久性和可靠性。因为微振动发生在微g范围内,所以这类应用需要一个具有极低噪声的高灵敏度测量链。

降低微振动测量的噪声阈值

IEPE(集成压电集成电路)三轴加速度计8763B是用于这些测量的最常用的奇石乐传感器,它允许在三个相互垂直的轴上进行振动监测。测量阈值决定了传感器能够可靠地拾取的最小可能的振动级。2021年,奇石乐已改善了50g范围内的噪音阈值。更有效的测试程序和对奇石乐设施的大量投资现在已带来进一步的优化。8763B现在的特点是所有范围的噪声阈值都大大降低:100g范围内的噪声阈值降低58%,250g内范围降低37%,500g范围内降低52%,1000g范围内降低54%,传感器的最高范围2000g内降低51%。得益于这些优化,8763B传感器变得更加适用于通用的应用,如模态分析、频率响应测量和电机测试。

三轴加速度计的可用性进一步优化

奇石乐进一步优化了程序和运行,大大缩短了8763B系列在中小规模订单上的生产周期,并减少了交货时间。在最佳条件下,生产时间已经大大减少。这也使安全库存水平提升。同时,配件的可用性也得到了改善。

8763B传感器在每个正交轴上都有很宽的频率响应,非常适合于动态振动测量,特别是在轻质结构上。其他特点包括传感器的轻质密封钛合金外壳,以及由于采用了剪切元件技术,对基础应变的高免疫力。一体化的硅胶电缆型号可用于高达10 bar的水下振动测试。8763B系列的传感器可以通过胶粘剂安装或灵活的螺柱安装在测试对象上,得益于三个5-40的螺纹孔,使其能够充分利用立方体设计的每个安装面,确保每个轴的校准的可靠安装。

媒体宣传资料

下载新闻稿 PDF,Word及高清图片素材: 奇石乐媒体资料.zip

27.09.2022
The new SlimLine Sensor 9132CD is nine times more sensitive than comparable SlimLine sensors.
16.09.2022
At K 2022, Kistler will showcase its solutions for injection molding that make plastics processing more intelligent and sustainable.
06.09.2022
奇石乐ComoScout过程监控系统简单易用、成本效益高,是优化注塑成型工艺的理想选择。
31.08.2022
High-end measurement systems for rolling stock – from brake testing to traffic monitoring.
22.08.2022
人工智能在冲压行业的应用:人工智能帮助制造商提高产品质量,加强质量保证。
28.07.2022
最成功的三轴加速度计8763B更精确地测量微振动。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.