Optical analysis of combustion processes in engines

Winterthur, November 2019 – Kistler, the Swiss measurement technology expert, is adding a new product to its portfolio: the innovative HIS high-speed camera system with optical probes for visualization of combustion processes in engines. The system comprises a control unit, a high-speed camera and a borescope with integrated LED illumination. HIS helps engine developers to optimize combustion processes, with the focus on emissions and consumption.

Electrified propulsion is set to gain ground in the coming years. Nevertheless, a large percentage of vehicles delivered by manufacturers will still be equipped with combustion engines, so developers are continuing to focus on optimizing their emission and consumption values. Demand for increasingly accurate measuring instruments is therefore growing – and Kistler has responded by expanding its range of products for the optical analysis of combustion processes.

High-resolution images of combustion processes

The new HIS system comprises a control unit, a high-speed camera and a borescope with integrated LED illumination. This innovative system allows detailed investigations of processes in engine cylinders, so users can examine phenomena such as the injection process, soot formation and flame propagation. The high-speed camera captures up to 40,000 high-resolution images per second and is equipped with an LED system for illumination. Thanks to these features, users can carry out precise investigations of gasoline direct injection and flame propagation. The high-speed camera images are captured synchronously with the combustion analysis pressure values in one control unit. All data is matched to ensure precise fine-tuning of the combustion process, resulting in optimal consumption values.

User-friendly integration of pressure sensor and light conductor

Another Kistler highlight: the cylinder pressure sensor and the optical waveguide are integrated in one spark plug. The plug is screwed directly into the engine, with no need for an additional mounting bore. The system is both user-friendly and rugged, making it ideal for modern engine applications aimed at developing high-performance compact engines with complex cylinder head geometries.

These new products from Kistler play a key part in the cost-effective development of engines with optimized consumption values and emission levels.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.