Nothing escapes sharpened senses

Stuttgart, 24 April 2018 – The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show. There will be a special focus on automatic testing and sorting machines from Vester. 

Quality assurance is a critical success factor in every industrial manufacturing process. Parts, sub-assemblies and components must be produced as planned: this requirement has to be guaranteed so that industrial enterprises can meet their customers' expectations. What's more, this goal must be achieved economically – which means efficiently in terms of costs and resources. The ultimate objective is a zero-defect culture, and the best way to achieve this is with process monitoring systems.

Automated testing for series, continuous, punched and hybrid parts

Vester Elektronik GmbH, which recently joined the Kistler Group, will have its own stand in hall 6 at Control 2018 where it will exhibit three of its highly integrated automatic testing and sorting ma-chines for punching and forming technology. High-performance image processing systems enable users to perform fully automated dimensional and surface tests with the additional options of gaging and hardness tests. The digital camera technology deployed for this purpose ensures 100% testing of mass-produced parts with very high throughput rates.

The Videocheck VVC-120 automatic testing and sorting machine ensures that mass-produced parts are fed into inclined quick-change test and transport rails, with positional stability maintained during handling. Telecentric illumination components and high-precision lenses guarantee efficient optical testing and high throughput rates. This fully encased, noise-damped automatic machine is operated via a 24-inch touchscreen; up to four cameras with different resolutions can be integrated for throughput of up to 250 parts per minute.

Videocheck VVC-620 is a test cell for parts manufactured continuously using processes such as punching and stamping, lamination and injection molding in particular. Various applications will be demonstrated on Vester's stand, including classical dimensional inspection, complete contour trac-ing and detection of surface defects. Users have a variety of test options at their disposal, and they themselves can define what should happen in case of an error: choices range from halting produc-tion to separating or marking bad parts.

Videocheck systems 821/C and 821/E were designed specifically for complex dimensional and surface inspections of mass-produced parts and they are equipped with a rotary plate with up to eight cameras. Depending on size and weight, parts for testing are fed in via an integrated (821/C) or separate (821/E) feeder system. In addition, blower nozzles ensure automatic sorting of good and bad parts including ejection control via light barrier.

Thanks to Vester, industrial image processing has now been add-ed to the Kistler Group's wide-ranging know-how. We are taking advantage of this opportunity to set up a Vision Center in Karlsruhe that will continue developing the related technologies. This means that more innovations in the industrial process monitoring segment can be expected from us in the future.”

Frank Kirgis, Head of Division Industrial Process Control (IPC) at Kistler

 

Come and see us!
Experience the products and services offered by Vester – a Kistler Group Company – on stand 6413 in hall 6 at the fair in Stuttgart from 24 to 27 April 2018. A warm welcome awaits you!  

 

媒体宣传资料

下载新闻稿 PDF,Word及高清图片素材: 奇石乐媒体资料.zip

28.07.2022
最成功的三轴加速度计8763B更精确地测量微振动。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.