Kistler's new cylinder pressure sensor: setting standards in engine development

Winterthur, November 2018 - Kistler's new M8 cylinder pressure sensor (Type 6044A) features an anti-strain design that makes it ideal for direct mounting in high-performance engines – with excellentthermodynamic precision, temperature stability and very low linearity deviation. A versatile, reliable sensor that delivers high-quality results – the optimum solution for the complete engine development cycle. 

Modern combustion engines deliver higher performance despite increasingly compact dimensions, setting new challenges for cylinder pressure measurement: users demand higher accuracy and greater stability under difficult conditions, but less and less space is available to accommodate the measurement technology. The new uncooled 6044A cylinder pressure sensor is Kistler's response to both of these challenges: significantly improved performance on one hand and a design that reduces sensitivity to external disturbance on the other.

Versatile range of applications

David Mauke, Product Manager Sensors, Engine R&D, explains: "The measuring element in our new sensor is decoupled from the sensor body – a design feature that ensures excellent stability under high loads, making this sensor highly rugged and insensitive to its mounting position. This is a versatile solution for engine development applications, from concept validation through to final calibration." Thanks to its lifetime-optimized piezo crystal, the 6044A also withstands high pressure peaks coming from pre-ignition.

Rugged and consistent – also when mounted directly

Kistler's latest innovation is fully compatible for installation with uncooled Type 6045 cylinder pressure sensors, as well as water-cooled Type 6041 sensors with an M8x0.75 through-hole thread. Key benefits include minimal sensitivity shift across the temperature range (thermal sensitivity shift), very low linearity deviation and high thermal shock resistance.

With an extended pressure range of up to 300 bar, the 6044A is the ideal replacement for earlier sensor versions. David Mauke's final comment: "Kistler's new cylinder pressure sensor gives engine developers more accurate measurement values combined with minimal cycle-to-cycle deviations especially when it is mounted directly."
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.