Kistler Unveils the Latest Functionalities for Automated, Reproducible Injection Molding Processes and Their Control

Düsseldorf, 19 October 2016 – Kistler is presenting the new versions of its ComoNeo and ComoDataCenter – both with innovative options for applications in injection molding production that vastly simplify the control, reproducibility and documentation of processes in this segment of industry. First and foremost among the new features: the Restart Assistant, which allows efficient reproduction of established processes when changing machines.

With quality requirements constantly on the increase, continuous control of the entire injection molding production chain is absolutely essential. The focus here is on improving product quality and boosting cost-efficiency. Kistler has now developed the successor versions of ComoNeo and ComoDataCenter, two system components that already have excellent track records. These new versions offer the best possible basis for achieving these goals – and they are ideal for novices as well as experienced users.

Automated Process Reproduction: ComoNeo Now with Restart Assistant and OPC Interface

Kistler has now integrated a Restart Assistant into ComoNeo, making it possible for users to transfer established processes from one machine to another with no problems at all. To ensure identical quality reproduction in the new machine, this intelligent tool suggests which parameters need specific changes. For this purpose, the Assistant detects deviations in the cavity pressure and compensates for them by adapting the machine parameters. This automated analysis generates a suggestion so that users can correct the process on the basis of the cavity pressure – and no previous specialist knowledge is required.

As the era of Industry 4.0 dawns, this support places users in the best possible position to conquer the challenges posed by digital networking. For example: the system now supports the OPC-UA interface, which is on the way to becoming the standard for injection molding production. By integrating OPC-UA into ComoNeo, Kistler has now made it possible to fully implement Multiflow control (automatic hot runner balancing) as a standalone solution. In other words, users no longer need a PC for control. The benefit: significantly less effort is required for the entire setup process. Another new feature in ComoNeo: online quality forecasting is now integrated directly into the system, so the complete range of cavity pressure monitoring methods is available. The EO Assistant (for automated setting of monitoring limits), online quality forecasting and the Restart Assistant: three aids that ensure novices as well as experts will be guided to the desired results.

Control with Industry 4.0 in Mind: New Features for Real-Time Control and Hot Runner Balancing

The first version of ComoNeo already set a new standard for monitoring of injection molding production processes. This was achieved with the help of the EO Assistant: for the first time, users with no specific knowledge of cavity pressure were given a simple option for monitoring. Kistler has now developed software that goes one step further in quality optimization. The new version of ComoNeo provides feedback to the operator and the machine so that the process can be optimized even further. This advance allows perfect timing for the switchover from speed control to pressure control in response to cavity pressure. ComoNeo also offers a sampling rate that cannot be matched by any comparable system. The result: yet again, real-time control has been made vastly more responsive in every respect.

Automatic switchover control can be used in two different ways. The first option is for manual setup: control behavior is only changed after the user intervenes. The second option is called SLP (Switching Level Processor): in this case, setup is fully automated and the control behavior is optimized independently from cycle to cycle. The main advantage of the manual option is that several dependencies can be set; with SLP, the key benefit is self-optimizing calculation of the switchover point. In these ways, ComoNeo 2.0 also covers a wide range of process control applications: for molds with multiple cavities, behavior during automatic changeover has been optimized for the specific purpose of compensating for different behavior patterns during the production sequence. When conditions are set manually, additional dependencies across multiple cavities are available as control criteria. On the other hand, automated changeover is mainly used for molds with small numbers of cavities. The benefit here: ease of handling. All that is needed is to activate the process – and everything else is controlled by the internal algorithm, virtually at the touch of a button. Both switchover options actively help prevent mold damage because safety functions respond if filling differences are excessive.

Multiflow control is a method used to control hot runner balancing. Its fundamental purpose is to use appropriate temperature control of the individual hot runner nozzles to ensure that all filling curves have an identical progression, so production quality is guaranteed. In the past, conventional production methods always required a manual fill study, but Multiflow control by ComoNeo now makes it possible to fill the individual cavities automatically – with increased speed and far greater precision. This advantage can be exploited during setup and also during the actual production operation. Thanks to the readjustment option that is newly integrated in ComoNeo, process fluctuations can now be compensated during the production phase as well.

ComoDataCenter: the Vital Link for Networked Injection Molding Production

The ComoDataCenter (CDC) is also enhanced with attractive new features that make it easier to network data and improve the traceability of part quality. For instance, the CDC is now available for ComoNeo as well. Thanks to this innovation, ComoNeo and CoMo Injection are linked via a com-mon database. Another new feature: mold management is integrated into the CDC. The settings can be stored centrally, so the ComoNeo and CoMo Injection mold settings can be transferred to other plants via CDC. For existing customers, this also ensures compatibility between CoMo Injection and ComoNeo – guaranteeing that CoMo Injection users can change over gradually to ComoNeo. There is also provision for integration into higher-level systems such as SAP or other MES systems. This means that the CDC acts as the single interface between the process and higher-level MES systems. The benefit: all data can easily be networked with other systems across the company. And, last but not least, the CDC's user interface is now standardized with the tried-and-tested ComoNeo interface – entirely in keeping with the universal operating philosophy advocated by Kistler.
By enhancing ComoNeo and the ComoDataCenter with these new features, Kistler is paving the way for yet more future improvements to product quality and cost-efficiency in injection molding production.

Kistler will be showcasing the latest technologies that we have developed for quality control at K Trade Fair in Düsseldorf.

User Contact
Daniel Fick
Business Development Manager
Phone: +41 52 2241 606
Email: daniel.fick@kistler.com
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.