Kistler showcases solutions for precise control and monitoring of production processes at The Assembly Show

Novi, MI, USA, 30 September 2014 – Kistler extends its maXYmos product family and presents the newly developed maXYmos NC for electromechanical joining modules at The Assembly Show 2014 in Rosemont, IL, USA. Visitors will also experience precise joining and testing demonstrations with the maXYmos BL, specifically designed for hand presses. Kistler’s full range of measurement systems facilitates end-users’ needs and acts as a single integrated source. This allows customers to operate a consistent systems approach for all applications in production – from the manual workstation to a fully controlled joining system. Intelligent sequence control – Enhancing precision With both manually operated and automatic pressing processes, product efficiency can only be assured in a zero-defect environment. The XY monitors from Kistler's maXYmos series enable customers to evaluate production processes, allowing them to operate with process-integration while enhancing consistency and maximizing quality assurance. Faulty parts are detected and removed early in the production process, thereby increasing product efficiency and avoiding unwanted downtime. Customers are able to conserve resources and increase quality assurance and product safety – saving substantial time and cost. A further development to the maXYmos family, the maXYmos NC (numeric control) enables manufacturers to monitor and control joining processes through system integration. The maXYmos NC evaluates and documents the XY curve progressions of joining and press-fitting processes in connection with the NC joining modules and the associated servo amplifier IndraDrive. Due to the shape of the measurement curves, each stage of the production and assembly line – and even the entire product – can be monitored and controlled via SERCOS III in real-time. As a result, optimum cycle times can be achieved with the highest degree of repeat accuracy, thereby reducing downtimes and allowing for increased machine availability in order to optimize the overall production process. For actuation of NC joining modules, Kistler has also developed an integrated and user-friendly sequence control system for the maXYmos NC. Programs for pressfitting parts can be created via the intuitive user interface of the color touch screen, which is connected to the control system. The integrated sequence control, or 'Sequencer Mode', enables versatile mapping of even the most complex processes easily and effectively. Visitors at the show have the opportunity to witness the intuitive operability and luminous display of the maXYmos systems. The uniform, operational interface in XY monitoring enables rapid integration into existing or newly planned systems. External measurement points – such as piezoelectric sensors for calibration or reference measurement – can also be connected at a later time thanks to the diversity of the interface. This ensures maximum flexibility, both during the installation process and for ongoing data analysis. Quality assurance for hand-press operations Kistler will also present an additional product from the maXYmos family at The Assembly Show in Rosemont – the maXYmos BL for hand presses. In non-automated operations, the maXYmos BL ensures that the processes are performed with reproducible quality using a sequence pre-programmed in the device – regardless of who is operating the system. Visitors at The Assembly Show will learn how the highly developed piezoelectric sensor and the intuitive monitoring enable rapid good/bad feedback and immediate correction or removal of faulty parts. With integrated or upgraded process control, zero-defect production of end-products is possible for each individual manufacturer, regardless of operating personnel. NC joining systems for reduced power consumption Kistler's NC joining systems support the automotive and automotive supplier industries by reducing power consumption within series production. This is achieved thanks to their higher level of efficiency when compared to pneumatic or hydraulic processes. The savings potential of the electrical process is up to 77 percent when compared with hydraulic systems, and up to 90 percent when compared with pneumatic process. Production costs decrease due to the low cost of system maintenance, which is less than an hour per system annually. The processes implemented with the NC joining systems in assembly and product inspection can be precisely controlled due to the integrated servo amplifier. Additionally, due to the dual measuring range of select NC joining systems and the simple program switchover, different components can be produced on the same machine. The NC joining systems can be installed quickly, are pre-tested by Kistler prior to installation, thereby enabling maximum in-process quality assurance while guaranteeing reliable results. Kistler will present its innovative products and customer service onsite at The Assembly Show in Rosemont, IL, USA from 28 – 30 October 2014 , Stand 1013. Download Press Release (PDF/EN)

Captions Image 1: The maXYmos product family: flexible solutions for the highest requirements Image 2: NC joining systems for riveting of lightweight brake disks

媒体宣传资料

下载新闻稿 PDF,Word及高清图片素材: 奇石乐媒体资料.zip

19.01.2022
The  latest M8 cylinder pressure sensor (6041C) from Kistler breaks new ground in measurement excellence.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.