奇石乐推出首款搭载压电式传感器的无线旋转切削测力仪(RCD)

奇石乐发布首款搭载压电式传感器的无线旋转切削测力仪 WL-RCD。该测力仪适用于多种加工工艺,能够实现高精度的切削力测量。其测量系统采用全新软件和硬件平台,可在测量时自动执行数据分析,帮助用户提高加工过程的效率。例如,通过预设测力仪各通道的配置参数,即可对系列测试开展自动分析。此外,用户可利用模拟信号和数字I/O输出,使该测力仪与机床、机器人等直接通讯,不仅可以实现过程监测,未来还会实现过程控制 

如今,RCD广受大学和研究中心的青睐,主要应用于刀具测量、机床研发,以及生产过程中的切削力监测,且尤其适用于铣削、钻削、磨削和超精加工等工艺。在加工过程中,工件加工质量、刀具寿命和生产时间均会受到多种因素的影响,而测力仪提供的数据能够帮助用户更好地了解磨损机制、材料特性、机床或工艺异常等宝贵信息。通过测量中获取的信息,用户可提高产品质量和切削过程的经济效益。

在生产监控中,客户尤其偏好无线解决方案,因为机床内部的空间有限,用线缆连接传感器的难度巨大,甚至难以实现。奇石乐无线旋转切削测力仪首次搭载压电传感器,通过无线技术连接数据采集设备。这款测力仪配备四通道压电石英晶体,可测量Fx、Fy和Fz三个方向的力和Mz的力矩。同时,采用低耗能无线技术,可连接五米内的信号接收器(最大连接距离视现场具体情况而定)。

压电测量技术,确保更高测量精度

压电式传感器具有宽量程(高达20kN)、高分辨率(< 1N)和高灵敏度的特点,使用户能够将同一款传感器应用于粗加工到精加工的多种应用场景。奇石乐无线旋转测力仪的采样率高达10 kHz,即使在转速高达16,000 RPM的应用中,也能够精准捕捉被测刀具的高速切削力变化。整体而言,压电式传感器的测量精度高于应变等技术,后者具有明显的局限性,尤其难以应对微小力和高动态过程的测量。对于研发工作和生产监控而言,测量精确度具有举足轻重的意义。压电测量技术能够捕捉极微小的变化和误差,避免生产缺陷对产品质量造成严重影响。

全新PTS软硬件平台,实现过程分析自动化

奇石乐无线旋转切削测力仪搭载全新PTS(压电式刀具系统)软件,可在机床运行的同时自动采集并分析加工数据。通过软件的信号趋势自动分析功能,用户可深入了解切削刀具的状态。未来,PTS平台还可与机床的控制单元直接通信,实现实时启动刀具自动更换等功能。这将有助于缩短机床停机时间,提高成本效益,减少维修时间。此外,PTS平台还能自动完成数据采集、分析和记录,显著提升实验室和研究中心的测试效率。

媒体宣传资料

下载新闻稿 PDF,Word及高清图片素材: 奇石乐媒体资料.zip

16.09.2022
At K 2022, Kistler will showcase its solutions for injection molding that make plastics processing more intelligent and sustainable.
06.09.2022
奇石乐ComoScout过程监控系统简单易用、成本效益高,是优化注塑成型工艺的理想选择。
31.08.2022
High-end measurement systems for rolling stock – from brake testing to traffic monitoring.
22.08.2022
人工智能在冲压行业的应用:人工智能帮助制造商提高产品质量,加强质量保证。
28.07.2022
最成功的三轴加速度计8763B更精确地测量微振动。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.