Kistler drives digitization ahead in test and assembly technology

Winterthur, 3 May 2018 – At Automatica 2018 in Munich (19 to 22 June 2018), the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and achieve gains in quality and efficiency. Center-stage at Kistler's fair stand will be joining systems and strain sensors as well as new components for enhanced digital system integration.

Sensors and systems from Kistler make sure that technology works as it is expected to. Haptics for smartphones and electronic switches, manufacturing processes for transmissions, and welding: in all these applications and more, intelligent monitoring and control of production processes generates added value based on data. The result: improved product quality. At Automatica 2018, visitors can experience the latest technology from Kistler live (in hall A6, at stand 425) with the opportunity to learn about the benefits in detail.

Offline parameterization reduces machine downtime

Thanks to process monitoring systems in the maXYmos product group, quasi-static and highly dynamic force processes on machinery and plant can be monitored and controlled with high precision, even when ambient conditions are difficult (limited installation space and small forces). For example, maXYmos visualizes and evaluates force-displacement profiles – making it possible for users to optimize their production processes simply and accurately with the help of the graphic presentation. And the integrated sequencer mode enables reliable control of sequences across multiple measurement programs, with no need for extra PLC programming.

The new version 1.6 – to be premiered at Automatica 2018 – gives users the option of configuring the system entirely offline from a PC. Thanks to this capability, the machine or plant only needs to be stopped briefly to upload or download the parameterization when changes to the production process are wanted. This new function cuts the total cost of ownership (TCO); it is available as of now for maXYmos TL and NC (joining systems).

Flexible joining with electromechanical technology

Customers who opt for electromechanical joining systems from Kistler benefit from major gains in flexibility and efficiency in the assembly process. The forces applied during press-fit processes can be monitored and controlled with precision; efficiency is many times higher than for hydraulic or even pneumatic technologies. The spectrum ranges from the highly economical NCFE to the NCFR for complex applications. NCFE is especially suitable for simple joining processes in the 10 to 80 kN force range. NCFR has the extra advantage of hollow-shaft motors so that a rotary movement can be performed in addition to the press-fit process.

Keeping large forces reliably in check

Piezoelectric (PE) strain sensors from Kistler offer a simple but effective way of protecting machines and tools against overload and damage. Thanks to their high natural frequency and sensitivity, they can capture even the smallest changes in the structure, so they act as an early warning system for critical process deviations in production and assembly – in applications such as press-fitting, punching and other forming process. Surface strain sensors are mounted directly on the machine structure with just one screw. Strain measuring pins can even be integrated directly into tools with the help of blind holes. Compared to strain gage technology, PE sensors score high on long-term stability, insensitivity to temperatures and overload protection.

Simple automation with the digital charge amplifier

From now on, not only PE strain sensors but also all Kistler's other piezoelectric sensors can be integrated directly into the machine control via Ethernet. What makes this possible? The only digital charge amplifier on the market – our Type 5074A. For the first time, plant and machinery manufacturers can now integrate any desired piezoelectric sensors directly into a real time-capable Ethernet system (PROFINET, EtherCAT or EtherNet/IP) so they can easily make settings on the measuring amplifier via the control. This is a quantum leap along the path to Smart Automation and Industry 4.0.

Kistler at Automatica 2018: hall A6, stand 425
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.