Kistler Breaks New Ground with Custom Monitoring System for Injection Molding

Orlando, FL. May 7, 2018 – At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding. Unlike ever before, system users can assemble their own package from the vast range of functions available in the system.

ComoNeo is the system of choice for plastics processing companies looking to boost product quality and cost efficiency by optimizing their injection molding processes. Kistler is constantly developing this process monitoring system – not only to accommodate new application cases but also to ensure comprehensive optimization in every respect coupled with maximum cost efficiency.

Based on the measurement of cavity pressure with tried-and-tested sensors from Kistler, users are provided with modular functions to support predictive control of the injection molding process leading to optimum results. Support, monitoring, control and prediction make Version 2.1.0 of Kistler's ComoNeo the leader in process transparency, which is essential for Industry 4.0.

ComoNeo: guiding users to desired results

A key benefit of this system is its ability to support users according to their individual levels of know-how. Kistler has integrated a practical prediction tool into ComoNeo: the Stasa QC software, which uses measured values and statistical analyses to calculate the quality of the manufactured components in advance, and to assess them within the tolerance bands. This special type of process monitoring is particularly useful for manufacturers of high-grade parts – in medical technology or other sectors where safety is critical, for instance.

To ensure optimal product quality and cost efficiency for their injection molding processes, customers can tailor their own ComoNeo with these functions:

  • ComoNeoPREDICT Allows model-based prediction of specified part quality based on the cavity pressure and temperature profiles – for optimum process parameters and transparent processes.
  • ComoNeoMERGE When multiple materials are used, process technology becomes more complex – but ComoNeo 2.1.0 can easily accommodate this challenge. The system monitors and evaluates up to four components with different mold technologies.
  • ComoNeoMULTIFLOW For molds with multiple cavities, this option allows hot runner balancing through individual adjustment of the nozzle temperature – to ensure identical injection conditions in all cavities and automatic correction of deviations.
  • ComoNeoSWITCH This function ensures automated switchover from the injection phase to the holding phase at the ideal time – for balanced injection behavior and optimum mold protection during the process.
  • ComoNeoCOMPOSITE Another new feature: injection molding with the RTM process can now be optimized. Special RTM sensors from Kistler create the conditions for controlled high-quality machining of long-fiber composites.
  • ComoNeoGUARD This function helps users to define monitoring windows that enable accurate separation of good and bad parts on a step-by-step basis. The benefits: guaranteed part quality and less pseudo scrap.
  • ComoNeoRECOVER This feature makes it possible to reproduce a proven injection molding process on a different machine. The user is guided through the adaptation step by step, deviations are identified and the assistant suggests corrective actions.

ComoDataCenter: transparent processes enhance quality and cut costs

As soon as ComoNeo has been specifically tailored to your individual application, everything quite literally comes together in the ComoDataCenter, a database that stores all the process data and establishes a seamless communication with overarching systems. Users benefit from the comprehensive overview of their entire injection molding production, which ultimately provides for a sound basis for ongoing analysis and optimization.

We're offering companies a complete modular and multifunctional package that fulfills all the requirements for intelligent and efficient injection molding. ComoNeo is Industry 4.0 put into practice. Mastery of new processes and greater levels of complexity shows the full extent of what injection molding can achieve in terms of quality – and the potential of process-integrated quality monitoring is far from being exhausted. Development is certainly set to continue."

Dr. Robert Vaculik, Head of Kistler's Strategic Business Field Plastics.

 

Kistler looks forward to welcoming you at NPE in Orlando from May 7 to 11, 2018. Visit Kistler at booth W7145. For more information and to watch a video on ComoNeo, go to: www.kistler.com/comoneo
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.