Kistler and BIG KAISER partner for precise measurement of cutting forces

Stuttgart, 18th September 2018 - At the International Exhibition for Metal Processing (AMB) in Stuttgart, Hall 1, Booth 1A61, Kistler and BIG KAISER are showcasing how their collaboration will help customers. The two companies are exhibiting a new system, where Kistler’s Type 9171A rotating dynamometer and BIG KAISER’s MEGA New Baby Chuck are combined to deliver high levels of accuracy in cutting force measurement.

The BIG KAISER MEGA New Baby Chuck offers higher precision than traditional ER clamping systems, delivering superior runout accuracy. BIG KAISER has specially adapted the interface on the MEGA New Baby Chuck to ensure it connects securely and accurately to the Type 9171A. As a result, Kistler’s customers can now achieve noticeably lower total radial runout errors by using this dynamometer. 

This means that they benefit from improved cutting force measurement accuracy, enabling them to increase the lifetime of cutting edges. For customers using the dynamometer in their own production processes, its high precision enables them to develop machining strategies that increase tool lifetimes and thereby reduce overall cost. In manufacturing, it enables tools to be replaced before they break, as increased forces at the cutting edge indicate that a failure is imminent.

The Type 9171A is a piezoelectric dynamometer for use in high-performance cutting applications. It measures forces and torques even under very high loads at speeds up to 12,000 rpm, allowing machining processes to be analyzed and optimized while obtaining information on tool wear. Compared to previous dynamometer models, the Type 9171A delivers a much wider range of spindle speeds with improved dynamic properties and a significant weight reduction. It is particularly suited to multi-component force and torque measurements on rotating tools during milling and drilling.

BIG KAISER's collet chucks offer high accuracy for any machine spindle, with a guaranteed runout of 0.001 mm at the collet nose and less than 0.003mm at 4xD. The MEGA New Baby Chuck is the company’s most popular collet chuck for diameters up to 25 mm. All MEGA collet chucks have a notch-free MEGA nut that prevents vibration and reduces noise levels. These chucks are tightened using a unique MEGA wrench that can safely and evenly apply force along the entire nut periphery.

Innovative design and high precision

Gunnar Keitzel, Head of Cutting Force, Kistler, said, “Tool holders from BIG Kaiser are characterized by an innovative design, which has been optimized for high-speed machining. Kistler is pleased to now also be able to offer rotating cutting force systems with these high-precision interfaces, including the innovative MEGA New Baby Chuck."

Stefan Appenzeller, Head of Product Marketing, BIG KAISER, said, “Kistler’s 9171A is a market-leading dynamometer that provides the highest levels of precision. Together, BIG KAISER and Kistler can now help customers develop and improve their cutting processes.”


The International Exhibition for Metal Processing (AMB) is held in Stuttgart, Germany from 18th to 22nd September 2018. 1,500 exhibitors from more than 30 countries will present the latest machine and precision tool developments as well as other machining solutions. In 2016, approximately 90,000 visitors attended the AMB, and this year an extra exhibition hall has been added.


The Type 9171A dynamometer and MEGA New Baby Chuck, with the adapted interface to fit the Type 9171A, are available from Kistler now.

Image material (please name the Kistler group as picture source)

媒体宣传资料

下载新闻稿 PDF,Word及高清图片素材: 奇石乐媒体资料.zip

19.01.2022
The  latest M8 cylinder pressure sensor (6041C) from Kistler breaks new ground in measurement excellence.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.