From time to condition-based train brake maintenance with Kistler

The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A. The innovative all-in-one system is to be unveiled at the upcoming InnoTrans in Berlin from 18 to 21 September in Hall 6.2, Booth 110.

The safety and availability of rolling stock is of key importance in railway operations. Reliable brakes are one of the main reasons why trains are still considered to be one of the safest means of transport. Regular inspection of brake pad force ensures the safety and availability of the rolling stock and helps save resources. 

Predictive, cost-effective operation

A very efficient way of optimizing vehicle maintenance is offered by switching from time-based preventive to condition-based predictive maintenance. The benefits of this method are twofold: measures to increase operational reliability can be adopted at an early stage, while cost savings of 15% to 20% can be achieved.

Precise measurement data as the basis for the switch

Kistler supports implementation of this future-focused maintenance concept with the appropriate measuring system that can be deployed by maintenance contractors, rail vehicle manufacturers and train operators. Switching from preventive to predictive maintenance calls for new methods of establishing changes in condition, like the performance of systematic brake pad force measurements. 

Brake system wear and tear can be checked with a brake pad force measuring system. Conditions and changes are recorded by a suitable data management system across several test cycles. Reliable conclusions can be drawn from their analysis about existing and anticipated wear and tear and the consequential (future) reduction in braking action. 

The same series of measurements helps to optimize maintenance planning and, along with other operational data, forms the basis for implementing the predictive maintenance concept. 

Compact, mobile and flexible solution

The Swiss sensor specialist presents it all-in-one solution in a practical case comprising braking force measuring system Type 2899A and all the necessary components, including brake force measuring elements, signal conditioning, data acquisition and application-specific software. The case comes on rollers and is battery-operated for mobile use. It can be used both for maintenance (factory floor) and permanent in-line condition monitoring. 

The Kistler brake force measuring system is designed for the diagnosis of shoe and disc brakes. Instead of brake shoes or pads, the measuring elements are mounted to permit direct, precision measurement of the respective parameters. The brake force measuring elements are compatible with various wheel diameters and cover a wide range of forces up to 60 kN. The system and related process comply with the proof of safety in line with CSM-RA (EU) 402/2013 and (EU) 352/2009 (Common Safety Methods – Risk Assessment). 

Long-serving, rugged sensors

The brake force measuring system can be equipped with up to eight force sensors and optional pressure and trigger sensors. The piezoelectric force sensors are based on Kistler's decades of experience in this field: they are particularly rugged in terms of mechanical design, UIC-compliant and factory calibrated. Thanks to the high-resistance amplifier inputs, the linear and absolute charge signals generated are insensitive to electromagnetic interference. A special focus was placed on the consistent separation of railway and workshop mass to avoid adverse equalizing currents.

The new brake force measuring system is available and will be presented at the InnoTrans 2018 (18 to 21 September in Berlin).

Visuals (Reproduction is free of charge provided that the Kistler Group is credited as the source of the image) 
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.