RoaDyn传感器首次应用于日本小型汽车道路测试中

温特图尔,2021年8月 – 近期,奇石乐获日本政府批准,有权使用旗下RoaDyn S635六分量车轮力传感器(WFT)开展公共道路测试。此前,RoaDyn顺利通过一系列综合测试,符合日本轻合金车轮认证(JWL)标准的规定。自上市以来,Kistler RoaDyn车轮力传感器首次搭载于日产小型汽车中,在当地公共道路测试中发挥其优异的测量性能。

奇石乐RoaDyn车轮力传感器适用于公共道路测试、封闭场地测试、越野测试以及测试台测试。用户可根据车辆类型,借助适用的转换器,将RoaDyn的每个测量单元连接至轮圈和轮毂上。测试过程中,三分力测力单元将直接放大测量信号,安装在轮毂上的车轮电子对信号进行过滤、数字化和编码处理。

随后,数据的传输将由内侧传输遥测系统完成(遥测系统的转子安装于车轮内侧,定子安装于制动总成上);最后,车载电子仪器将对数据进行处理,并将处理结果输出至数据采集设备。经过上述几个步骤,RoaDyn S635可向用户交付精确的测量结果,为车辆研发提供宝贵的数据依据。

搭载内部传动型遥测系统,无需安装外部组件

RoaDyn S635的遥测系统位于车轮内侧,能够最大限度减少对车轮轮廓产生的影响。因此,这款传感器是公共道路测试的理想选择。RoaDyn S635所有结构零件和轮圈均由奇石乐独家设计并生产。此外,奇石乐通过开展有限元(FEM)强度模拟分析,确保该六分量车轮力传感器能够测量数据表中标明的载荷。

RoaDyn S635车轮力传感器采用基于独立测力单元的模块化结构,能够灵活满足不同轮毂和轮圈形状、载荷及测量范围需求。同时,该传感器使用数字化信号,确保数据传输的完整性。

RoaDyn S635顺利通过严苛的JWL系列测试

日本轻量化合金车轮认证(JWL)标准由日本国土交通省制定发布,旨在提高轻看、量化合金车轮的安全性。轻量化合金车轮必须满足JWL标准,才能投入公共道路使用。近日,奇石乐RoaDyn S635车轮力传感器顺利通过三项严苛的测试,并最终取得JWL认证。.

认证程序的首要项目是旋转载荷测试,该测试重点关注车辆行驶过程中作用于车轮的旋转载荷和力矩:在测试中,奇石乐六分力设备的特制轮辋夹紧装置,将车轮力传感器(包括测力单元、结构元件和铝制轮圈)安装于被测设备上;随后,被测设备完成120,000次旋转,车轮力传感器则需承受作用于轮毂安装面的旋转力矩。第二个项目为径向载荷耐久测试,即借助配备转鼓的特殊机器,使传感器经受600,000余次旋转。最后的项目则是冲击测试:首先,测试人员将车轮以13度的倾斜固定于安装盘上;随后通过重物自由落体的方式,使轮辋凸缘受到冲击;最后,检查车轮的裂纹、形变和气漏情况。

每项测试结束后,测试人员均会通过探测试验,检查车轮内部是否存在裂纹。Kistler RoaDyn S635六分量车轮力传感器成功达到各项测试的严苛要求;此外,其遥测系统成功通过电磁兼容性检测,进一步证明了这款传感器的卓越性能。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.