高温环境中的振动测量

 瑞士温特图尔,202010——奇石乐全新推出8248A3三轴加速度计可承受260摄氏度高温。传感器采用全新专利技术,以卓越的稳定性脱颖而出,尤其适用于温度变化剧烈测量环境。与其他用于振动测量的压电式传感器相比,加速度计更小、更轻,可在空间、传感器重量受限,或高温、温度变化剧烈的环境中得到广泛应用。

不论火车还是汽车,业界对于交通载具驾乘舒适性的要求正不断提高。为此,工程师们正致力于减少由车辆内外部件振动造成的不良噪音。对车辆部件振动的监测,不仅要求传感器能够实现精准测量,测量车辆动力总成或排气系统的振动时,还要求传感器能够承受较高的环境温度。铁路工程测量或动力装置的振动监测同样如此。奇石乐全新推出的8248A3迷你加速度计,可在260摄氏度的高温环境中测量三个方向的振动,并提供可靠的测量结果。该传感器采用两种陶瓷材料,可在温度变化时产生不同反应,并实现相互抵消,从而大幅降低温度变化对传感器造成的影响。

体小量轻和压电效应,确保可靠测量结果

被测物体的固有频率可能受加速度计自身质量的影响,因此不利于准确测量结果的产生。为避免该等影响,奇石乐全新传感器的体积和重量显著小于其他同类型传感器。对于测量设备空间有限的应用场景而言,小型传感器也更具优势。

传感器自身的固有频率在振动测量中发挥着决定性的作用:力作用于被测物体时,不仅物体本身会发生振动,传感器也会随之振动。得益于晶体部件的刚性,压电式传感器(如8248A3加速度计)具有较高的固有频率;该频率可最大程度地减少传感器自身振动对测量结果的影响,因此适用于要求严苛的测量场景,例如,压电式传感器可在发动机研发的爆震监测中精准测量z轴上的力。8248A3加速度计具有+/- 2000 G的宽量程和高线性度,同时具备良好的温度稳定性和电荷输出功能,适用于多种测量场景。

媒体宣传资料

下载新闻稿 PDF,Word及高清图片素材: 奇石乐媒体资料.zip

19.01.2022
The  latest M8 cylinder pressure sensor (6041C) from Kistler breaks new ground in measurement excellence.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.