通向数字化的桥梁

瑞士温特图尔, 2020年4月15日 - 全新灵活电荷放大器适用于当今工业应用:奇石乐推出全新微型电荷放大器,支持IO-Link技术——可满足生产环境中的广泛应用,从而惠及机器人、包装、食品等行业,也是OEM厂商的理想选择。该电荷放大器融合模拟和数字技术,为业界迈向工业4.0保驾护航。

奇石乐推出5028A电荷放大器,是市场上同类产品中首款可通过集成IO-Link技术,将压电式传感器的模拟信号输出为数字测量数据。可以为用户带来高感度,动态压电测量技术,而且具备抗干扰和端到端通信等数字化优势。IO-Link技术为用户提供实时数据,帮助用户监测大至整个工厂、小至各个传感器或测量链的状态,为开展预见性维护提供依据。例如,工厂数据经常超出设定值范围时,用户即可提前启动设备维护安排。当IO-Link部件被替换,新参数也会自动传输。

5028A电荷放大器内部集成数字接口,标志着奇石乐向工业4.0智能联网工厂又迈进了一步。该产品可对原始模拟信号进行数字化处理,避免因电感应或电容耦合产生的干扰;同时,用户可轻松完成信号模拟及控制,无需进行复杂且成本高昂的单独布线工作。如有需要,5028A还可用作模拟电荷放大器,但需加装复位/操作输入端。模拟电荷放大器模式下,该产品可应用于低延迟、低抖动高速过程的控制。谈及5028A的潜力时,奇石乐生产监控部产品经理Stefan Affeltranger表示:“5028A是全球首款支持IO-Link通信协议、且适用于压电式传感器测量数据处理的电荷放大器。对于希望其工业应用组件轻量化、配置简单化的用户而言,5028A是理想的选择。”

标准接口实现灵活应用

除了有广泛的功能,5028A电荷放大器为客户带来决定性的好处:上游传感器的接口和下游客户的系统符合同一工业标准。这就意味着电荷放大器可集成与现有的支持IO-Link技术的网络,这一优势确保了简单,高性价比的安装——用户也可以确保传输的数据是可靠、安全的。奇石乐正朝着将专利接头与常用标准协同这一方向前行。这样,产品就能更方便使用。即使是奇石乐最小型放大器,客户都能将之适配于现有的设备。这一创新是奇石乐响应工业领域的大趋势:更灵活的零部件可适用于不同系统,这样的客户需求越来越多。

5028A单通道电荷放大器体小量轻,非常适用于机械臂、活动部件等高度自动化应用环境;同时,该产品采用标准化接口,可集成于几乎任何支持IO-Link技术的生产设备中。5028A可广泛应用于机械工程和厂房建设;此外,鉴于用户可以安全变更并随时验证设置,该产品也非常适合医疗技术等受到严格监管的产业应用。5028A价格实惠,加之IO-Link带来的附加价值(IO-Link联盟强调的技术优势之一),定能为准备踏足压电式传感技术领域的新用户提供诸多便利。

免费网络讲堂:2020年5月14日,集成IO-Link技术的电荷放大器

奇石乐产品经理 Dipl. Ing. FH Stefan Affeltranger 将带来关于集成IO-Link技术的电荷放大器免费网络讲堂,就在2020年5月14日,周四 10:00 (CET)。与会者将通过本课程了解IO-Link技术的产品和优势,了解电荷放大器最适用于哪些工业领域的应用,及其带给智能工厂的附加价值。

点击 这里 注册报名。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.