特殊用途专用传感器

温特图尔,2020年11月——经过彻底的改进,Kistler 9091B传感器现在比以往任何时候都更加精准和耐用。奇石乐产品组合中最大的力传感器可用于多种应用:例如,用于材料力学的塔式落锤试验或核电站研发与监测试验。

Kistler 9091B传感器确保在极端条件下进行高精度测量。在传感器生产过程中,保证同样的精度:如在组装过程中保证绝对干燥环境,否则经过一段时间后,湿气会在表面凝结并影响电气绝缘。为了排除传感器在制造过程中的任何潜在污染,Kistler将9091B传感器保证洁净室进行组装,并采用改进的烘烤和清洁工艺。总体而言,针对15个不同的影响因素,对传感器的性能和耐久性进行了优化。

多元化测量的精度

高刚度的传感器测量各种应用中的大小力。例如,在材料研发的塔式落锤冲击试验中,传感器用来确定力峰值以及力的持续时间和分布。安装卫星天线时,它们可确保精确并有助于防止天线表面变形。在测试反应堆中,传感器可提供有关放射性芯子的有价值的力学数据,放射性芯子是在堆芯熔化期间形成的粘性物质。与其他材料接触时,钙会释放出极高的能量和爆炸性物质,例如氢。基于这些结果,研究人员可以重新评估核电站的安全相关参数。最后,高精度力传感器在校准设备中发挥着重要作用,例如Kistler同样使用此类产品进行相关的校准。

当需要评估动态力时,传感器内部的石英晶体始终可以确保精确的结果。 通过优化的制造,用户现在可以更加依赖这些坚固耐用的传感器,来保证始终如一的高精度。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.