极端条件下的精准测量

瑞士温特图尔,2020年7月 – 奇石乐发布了一款用于船机和发电机组缸压监测的新型传感器6635A1。此传感器应用于船机和发电机组中的四冲程气体机、双燃料及柴油发动机,可在燃烧室的恶劣环境下实现高精度测量。

双燃料发动机可以使用传统燃油、天然气或其他可再生能源作为燃料,因此,使用双燃料发动机能够减少燃油消耗和二氧化碳排放量。为提升双燃料发动机的性能,必须对其燃烧过程进行持续的监测和控制,而这正是6635A1气缸压力传感器的主要用途。使用多个6635A1传感器同时监测发动机所有气缸,通过精确的压力测量,得到平均指示有效压力(IMEP)和爆震等信息。通过对气缸压力进行持续监测,可实现发动机的燃烧闭环控制,提升发动机性能、节省燃料。实验证明,通过燃烧闭环控制能够使每台发动机平均每年节省约2%的燃料,相当于减少200吨的二氧化碳排放。

燃烧室的连续监测

传感器在燃烧室要经受高冲击力、高振动、高温以及高压。因此,传感器必须坚固耐用。为确保传感器的可靠性,6635A1采用焊接接头取代了传统的插入式接头。这项改进使传感器能够承受高达2000G的机械冲击。通过使用优化的膜片设计,6635A1不仅能够测量高达350bar的最大压力,同时还能最大程度地减少热冲击误差。此外,6635A1还使用了奇石乐独有的PiezoStar®专利晶体,能够保证在恶劣环境中卓越的稳定性和最小的温度灵敏度漂移。在晶体温度高达350°C时,6635A1仍能可靠工作。

奇石乐船机和发电机组部门的主管Miika Jussila表示:“奇石乐在气缸压力测量方面拥有多年经验。凭借这些经验,奇石乐确保为客户提供可靠的测量数据,以便尽早发现问题,并对燃烧过程进行优化。此外,客户还可基于奇石乐传感器测得的数据,优化发动机维修间隔、规划停机时间。”

6635A1传感器可为主机厂提供高质量测量数据,帮助您优化发动机燃烧过程,显著节省燃料、减少二氧化碳排放。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.