智能配件范围的拓展推动压电传感器领先起步

温特图尔,2021年5月--奇石乐Kistler拓展其智能配件设备的范围,以确保压电传感器能够完美和安全在任何单独的测量系统中适用。三维图纸和分步说明使安装过程变得简单。适配器、连接器扩展器和特殊铰刀确保传感器紧密地安装在位置上并完美地传输信号。如果需要,它们可以被连接到螺钉安装的电缆线上,即使长期浸泡在水中也能提供保护。

在高要求的测量应用中,选择合适的传感器至关重要的——选择满足各自应用挑战的测量周边设备更是如此。奇石乐从规划文件开始,在每一步都为客户提供帮助。测试工程师可以从制造商的网页上下载任何传感器或适配器的3D CAD模型。这使他们能够决定如何最好地安装传感器及其外围设备。

如果使用安装适配器,安装过程可以简化,有不同格式的公制螺纹或经验螺纹。传感器可以简单地安装到适配器上,而不需要任何进一步的工作。在其他情况下,可能需要将传感器平齐地安装在机器上,这就要钻一个孔。特殊的铰刀有助于确保完美的配合。当机械结构不能有削减时,或如果倾向于使用BNC-或TNC-连接,奇石乐的工程师可以从庞大的产品组合中推荐连接器扩展器。

一旦设置到位,可能有必要进行测试。有些情况下,工程师不能确定压力是否会超出传感器的最大负荷。这就是传感器假人出现的地方。它们允许彻底的测试,而不会对昂贵的传感器造成潜在的损害。它们还有助于延长传感器的使用寿命,例如,当进行循环测试而不需要压力测量时。通过简单地用假人替换实际的传感器,传感器可以休息,并在之后重新用于额外的测试周期。

每个测试和测量环境都是不同的,所以不可能有一个放之四海而皆准的解决方案。我们的目标是通过提供他们需要的智能配件和简单易懂的说明来帮助客户进行自助服务。”

压力测试和测量业务部压力产品经理 Ricardo Rodrigo

 

特殊条件:防水设备

压电测量技术需要高度绝缘的电缆,以确保信号传输的低损耗。在一些测试环境中,例如在造船和航海的研究实验室,可能需要特殊的防水设备。奇石乐现在提供了更多的防水传感器附件,其螺旋式安装的电缆线符合IP68防护等级,即使长期浸泡在淡水中也能提供保护。这为用户提供了更多的灵活性并节省了成本。如果螺丝安装电缆线被不可修复地损坏,需要更换的只是电缆线而不是传感器。

"我们努力确保我们的客户找到适合他们特殊情况的测量解决方案,"奇石乐测试与测量业务部压力产品经理Ricardo Rodrigo说。"每个测试和测量环境都是不同的,所以不可能有一个放之四海而皆准的解决方案。我们的目标是通过提供客户所需的智能配件和简单易懂的说明来帮助客户进行自助服务。"
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.