奇石乐推出新一代数字电荷放大器,搭载更多优化功能

瑞士温特图尔,202011——电荷放大器是压电测量链的关键组件。奇石乐Kistler根据用户需求,打造定制型电荷放大器,提供与客户特殊要求及数字化程度相匹配的创新性解决方案。现在,奇石乐对5074A型数字电荷放大器进行了全新升级——5074B型电荷放大器灵活性更强,集成更加便捷,全方位保证客户利益。

2018年,奇石乐推出5074A型数字电荷放大器,在工业电荷放大器技术领域实现了全新突破。5074A型电荷放大器是全球市场上首个数字电荷放大器,是控制和监控工业压装、装配和连接等过程的理想解决方案。当时,该设备是市场上唯一基于工业以太网(IE)实现通信一致性的电荷放大器;有史以来,工厂和机器制造商首次能够将任何所需的压电传感器直接集成至实时以太网系统之中。通过部署5074A,用户可通过控制系统轻松完成测量电荷放大器设置,可谓一项前所未有的功能。同时,20到1,000,000 pC的超宽量程以及适用于多种应用的丰富测量功能,赋予了5074A型电荷放大器超高的灵活性,使无数种测量操作的实现成为可能。凭借该等优点,5074A型电荷放大器成为需要通过工业以太网开展的动态和准静态测量的完美选择。此外,5074A型电荷放大器单通道采集率高达50kSps,同时具备测量数据实时传输功能,传输周期低至100微秒,即使以今天的标准衡量,其性能也十分出色。

奇石乐生产监控产品经理Stefan Affeltranger表示:“刚上市不久的全新5074B型数字电荷放大器取代了以前的5074A型,但保留了后者久经验证的各项优势。”除继承前身的多个优点外,5074B型电荷放大器搭载两项全新功能,使其操作性能得到显著提升。首先,5074A型每次启动均需30秒,而5074B型仅需6秒即可准备就绪,为用户节省了宝贵时间。这项优化,使工厂——尤其是支持热插拔模块的工厂——也能够部署电荷放大器开展测量。其次,在5074B中,M8连接器的两条供能路径被分隔开,用户可任意连接符合行业标准的其他标准设备,同时还可关闭外围电源。Affeltranger解释道:“使用全新5074B型电荷放大器,用户能够在不限制放大器功能的情况下,轻松可靠地在机器上连接其他设备。”

高度便捷的低成本安装

与其前身5074A型一样,5074B型电荷放大器可实现便捷的低成本安装。用户无需使用任何额外软件,也无需部署复杂且昂贵的模拟信号和控制信号传输电缆,即可将5074B集成至现有的以太网中。5074B型电荷放大器通过控制系统进行配置,确保卓越的数据安全性,为工业过程提供保障。Affeltranger指出:“新上市的5074B型电荷放大器是奇石乐电荷放大器家族的重要成员,包括模拟信号型、数字型、以及支持IO-Link技术的微型电荷放大器。我们不断拓展产品构成,通过创新和领先技术满足客户的广泛需求。我们通过不懈努力,在多个领域突破了技术和经济制约,开启了测量链的数字化时代。”

媒体宣传资料

下载新闻稿 PDF,Word及高清图片素材: 奇石乐媒体资料.zip

19.01.2022
The  latest M8 cylinder pressure sensor (6041C) from Kistler breaks new ground in measurement excellence.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.