奇石乐推出全球首台陶瓷多分力测力仪,可测量更高频的微振动

瑞士温特图尔,2020年1月 - 奇石乐全新推出的9236A压电式多分力测力仪,专为测量卫星测试中的微振动而设计。9236A测力仪采用陶瓷顶板取代钢制顶板,拥有更加出色的固有频率,其微振动频率测量带宽较传统传感器提高了40%,能够捕捉到高频率小力中的极小动态力的变化。9236A测力仪的面世,标志对地观测领域向前迈出了重要一步。

人们早已对谷歌地图提供的高清图像司空见惯,但想要保证高清图像的质量,就必须消除或减少可能导致图像模糊的微振动。微振动由极小的加速度形成。压电式力传感器和测力仪由于固有频率较高,已被广泛用于与测量微振动和追踪微振动成因的理想测量工具。

微振动测量面临新挑战

人们对卫星拍摄地面图像的精度要求不断提高,因此,高分辨率摄像头的使用势在必行。但分辨率越高,摄像头就越容易受到微振动的影响。解决这一问题有两种途径:一是使用固有频率更高的测力仪,从而更轻松地分离高频率微振动;二是部署大型测力仪,对分系统和小型卫星进行完整测量。压电式测力仪支持静态预载,并能以高分辨率测量六向动态力和力矩。传统测力仪采用钢制顶板,测力仪越大,顶板越沉,质量越大。然而,质量越大意味着固有频率越低,不论多么精确的传感器都无法抵消其影响。因此,除非在顶板材料上另辟蹊径,否则传统测力仪的固有频率显然已达到极限。

突破压电式测力仪测量极限

针对这项挑战,奇石乐提出了全新的解决办法,即用陶瓷代替钢材料制作测力仪顶板。奇石乐开发人员克服了陶瓷材料的脆性问题,终于开发出一套具有显著优势的完美解决方案:新型测力仪刚性更强,重量更轻,固有频率达到2.6kHz(比传统钢制顶板测力仪高40%)。全新的陶瓷顶板测力仪尺寸不变,仍是260 x 260毫米。得益于上述诸多优势,新型测力仪的测量范围扩大到-500N~500N,突破了此前的极限。不仅如此,奇石乐还提供两种不同尺寸的测力仪型号供客户选择,大尺寸测力仪可应用于复杂系统或小型卫星的测量。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.