奇石乐微型模腔压力传感器引领行业新标准

体积小、精度高、顶级性能; 这是奇石乐发布的新型传感器(6178C,6182D和6183D)的技术特点。新型号传感器实现了统一灵敏度(UNISESS®)从而最大化地提升了测量精度,同时还增加了碳化钛涂层。10月16日至23日在杜塞尔多夫参观2019年K展的观众可以莅临10号大厅G81展台上了解多种微型传感器。

这些微型传感器具有令人信服的优点: Unisens®统一灵敏度,确保其精度仅为先前公差范围的一小部分。这样增加的精度增益消除了系统中传感器区分的需要。这些传感器的高灵敏度保持恒定,因此用户不再需要从每个传感器数据表中输入系统值。这也意味着更换传感器非常简单,尤其是涉及多腔模具时。对于复杂高精度零件(如电气插头)的制造商以及汽车和医疗行业的制造商来说,非常严格的公差范围和易于操作性显然将是该型传感器被选择的关键。

抗磨损,使用寿命更长

从现在起,新的微型传感器也可增加碳化钛涂层(而不是硬铬)。这种涂层在注塑领域多次证明了它的卓越性: 它提供了最佳的耐磨保护,确保了这些高灵敏度传感器更长的使用寿命。碳化钛涂层具有两个决定性的优点: 优异的耐磨性和耐化学品腐蚀性。由于这些优点,这种新型传感器非常适用于玻璃纤维增强塑料和阻燃塑料的成型过程监控。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.