奇石乐展示数字创新成果及扩展服务

20171012日温特图尔——在即将于20171128日至30日举办的德国纽伦堡工业自动化展会上,奇石乐集团将首次展示新一代最高至100 kNm的扭矩校准系统,以及其他具有里程碑意义的电气自动化创新成果,如KiTorq系列高性能(实时)扭矩传感器、全球首个数字电荷放大器等。

奇石乐的传感器和系统可以帮助客户最有效地使用现有机械和设备。例如,用它们协助检查传动装置和工具,监控并优化个别生产流程,分析并自动化整个生产工序。随着数字化时代的到来,工程师将面临若干重大挑战,其中之一便是开发有利于实现工业4.0目标的压电传感器等产品,以确保最大程度地连通自动化环境。奇石乐的最高目标是——为客户创造真正的附加值。

KiTorq实现对运动的实时控制

奇石乐再次增强了KiTorq系列高性能传感器的性能。传输速率现在达到了4 kHz,在采用Profinet或EtherCat接口连接情况下,该模块化系列的评估单元(定子)比以前快了3倍。采用Profinet时,使用IRT模式可以实现多个同步运动控制应用之间实时通信,使得在测试台上控制扭矩等成为可能。

在KiTorq系统(如2016年德国纽伦堡工业自动化展会上展示过的KiTorq 4550A等)中,我们可以为新一代的定子按需搭配各种转子,从而以最高8192的每转脉冲数提供超高分辨率的扭矩、速度、旋转角度测量值。

校准大挑战:高端测试系统成为一种服务

奇石乐集团下属洛尔希(Lorch)工厂面向传动技术领域客户推出了新一代具有卓越性能的校准系统。该系统支持1~100 kNm的扭矩量程,是该性能级别少数几种获得DAkkS(德国认证机构)认证的大型设备之一。有了该系统,重型机械、船用发动机和风力发电机组设计师以及特种机械制造商现在可以对自家解决方案进行密集测试与优化。该新设备(保证可追溯性)意味着奇石乐集团的校准服务范围再次显著扩大。

世界第一:新一代数字电荷放大器

奇石乐新一代5074A型数据采集器实现了工业传感器技术突破。5074A型电荷放大器是目前市场上唯一一款面向压电传感器且具备工业以太网通信能力的放大器。大型设备和机械制造商有史以来第一次可以直接将压电传感器集成到实时以太网系统内,从而轻松通过控制装置对测量放大器进行设置。

对于该新品,奇石乐生产监控部门产品经理Stefan Affeltranger热情表示:

5074A电荷放大器是世界上唯一一款面向准静态测量过程,且其压电传感器支持实时工业以太网通信的放大器。

奇石乐生产监控部门产品经理Stefan Affeltranger。

此外,该产品也非常安全,他补充道:“该设备没有适当的工业通信协议无法访问,要修改测量参数也必须通过主机。”

2017年德国纽伦堡工业自动化展会上发现新的可能

如果您想亲身体验一下奇石乐在测试台和校准方面的数字创新成果和扩展服务,我们热情邀请您参加今年11月28日至30日的德国纽伦堡工业自动化展会,我们的展台在4A大厅526号。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.