奇石乐定制传感器可应对各种测量挑战——无论多么极端的条件

瑞士温特图尔,2019年2月 - 奇石乐9397C型三分量力传感器具有独一无二的测量能力,Z方向量程上限为450kN, XY方向量程上限分别为100kN。作为世界上同类型传感器中最大的传感器,该传感器是碰撞测试中捕获冲击力等大型测量任务的绝佳选择。瑞士奇石乐公司是压电测量技术领域的先行者,专门提供可同时应对超大量程的即用型定制解决方案。

根据奇石乐产品经理Martin Betschart所述,“三分量力传感器在涉及以最高精度测量超高动态力的各个应用中占据核心地位。”他继续表示,“我们以客户为中心、以应用为导向的方案是以我们60余年的压电测量技术经验为支撑,因此我们可以非常准确地了解到不同部门和行业的要求。全新的9397C型三分量力传感器表明,我们可以完成的测量级别实际上不受任何限制。”

压电式三分量力传感器在工业中用于测量动态和准静态的拉力和压力。由于具有非常高的刚性和较高的固有频率,此种传感器能够同时在三个方向上,非常精确、极为可靠地测量超大力中非常小的动态力。此种传感器在交付时已经过校准和预加载,因此正确安装完毕后即可使用。

可靠地测量巨大冲击力

一个典型的应用领域是测量飞机着陆时起落架的冲击力。起落架落震试验模拟飞机着陆时作用在起落架上的各种力。进行试验时,整个起落架在落塔内被提升到一定高度,起落轮进行加速,然后降落到传感器设备上。1个测力计内安装4个传感器,可同时测量900kN Fz和400kN Fx/y的力。另一个应用是自2017年7月下旬以来一直在中国运行的世界首个具有开创性的用于高速列车的碰撞墙。在该应用中,传感器的量程比汽车行业碰撞测试中的常用量程大20倍。

航空火箭上的载荷试验

在航天器的飞行试验阶段,望远镜、电子仪器等设施有效载荷会承受强大的准静态力和机械动态力。为了使该结构件满足飞行要求,在加载测试中采用振动和冲击试验台进行振动模拟仿真。力限振动试验法用于限制所施加的力,并防止力过大对有效载荷造成损害。为了完成此项实验,在振动台和负载之间需要集成若干个三分量力传感器。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.