奇石乐在注塑制造中引入人工智能

温特图尔-2019年9月-奇石乐将于2019年10月16日至23日在杜塞尔多夫出席K展——全球最大的塑料加工行业贸易博览会。奇石乐的测量技术专家将在10号展厅的G81展台欢迎参观者到来,了解人工智能将如何为未来的智能工厂铺平道路。奇石乐——来自瑞士的解决方案供应商将展示从传感器到软件的整个测量链智能且专业的解决方案和产品。

智能生产、网络化和数据一致性

奇石乐的过程监控系统ComoNeoPREDICT为注塑过程添加了人工智能。该智能软件基于神经网络生成质量模型。这是精确和高效的注塑加工的起点,以满足汽车和医疗技术行业的高标准要求。这种提前计算塑料制件性能的方法可以使注塑产品满足最高质量标准。

奇石乐还专注于系统的端到端网络,以确保高水平数据可用性。与质量相关的过程数据通过OPC UA协议在独立平台的基础上提供,以便(例如)进行长期持续分析,并确定故障原因。该网络将显示来自运行ComoNeo设备的合作伙伴的实时数据,并将在2019年K Show展示。

ComoNeo: 您智能生产的起点

来自奇石乐的ComoNeo是注塑行业过程监控的领先系统。无论是在车间的水平流程层面,还是在总体系统的垂直层面,它是数字价值链中的核心模块。在工艺层面上,ComoNeo提供了基于模腔压力的工艺监控等功能,满足传统和多组分注射成型(ComoNeoMERGE)。该系统还实现了基于模腔压力的注塑机的自动V/P切换(comonoSwitch)以及热流道控制系统的自动平衡(comonoMultiflow)。ComoNeo生成的所有与质量相关的过程数据都可以传送到更高级别的系统,如MES或ERP。所有这些优势使ComoNeo成为您智能生产的起点。

满足最苛刻要求的模腔压力测量

奇石乐在此次K展上将展示包括创新步道,在这里,客户和参观者可以体验到腔压测量技术已经在帮助今天的注塑机了,并对我们未来的发展方向进行了一些展望。测量技术价值链始于传感器及其核心部件压电石英。了解模腔压力传感器的结构,了解压电效应的基础以及如何利用它。并找出一个重要问题的答案:为什么奇石乐要培育自己高度专业化的石英?

模腔压力传感器技术对智能注塑成型至关重要,因为它提供了关于工艺参数的数据,这是提高注塑件品质的关键。在奇石乐展台,参观者将会看到如何测量模腔压力,直接测量或间接测量,甚至是非接触测量。非接触测量要归功于超紧凑的9239A型测量探针,该产品是为高外观要求的注塑产品专门研制的。另外,奇石乐将展示温度压力一体传感器技术。

ComoNeo高效注塑成型:从再现性到预测

ComoNeo 是奇石乐开发的分析传感器监测数据的先进过程监控系统。该系统的七个模块化功能为用户优化注塑生产线提供了透明的指导:

  • ComoNeoGUARD 帮助用户设置监控窗口,对次品注塑件进行可靠的评估。 
  • ComoNeoMERGE 满足更复杂的注塑工艺控制,最多可以满足多达4种不同组分的注塑成型。
  • ComoNeoMULTIFLOW 通过控制热流道的独立浇口温度,使多腔模具达到注射平衡。 
  • ComoNeoSWITCH 保证注塑机在理想的时间进行保压切换。
  • ComoNeoCOMPOSITE 优化长纤维复合材料的RTM 工艺-通过奇石乐RTM特殊传感器。 
  • ComoNeoRECOVER 在不同注塑机上实现工艺复制,通过软件注塑辅助逐步实现。
  • ComoNeoPREDICT 基于模腔压力与温度,通过模型预测注塑件品质。

奇石乐的专家将很高兴地向您展示ComoNeo如何工作。他们将演示如何根据每个客户的要求设置和使用该系统,以提高产品质量、降低次品率并提高工厂整体效率。 

与奇石乐相约 2019 K展 10号大厅G81展台! 

我们的专家期待着10月16日至23日在杜塞尔多夫欢迎您。了解我们的塑料加工智能解决方案。了解奇石乐如何在整个测量链中为客户创造附加值。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.