奇石乐在欧洲太空科技博览会上推出新产品

2017927日,温特图尔——作为欧洲航天业代表企业的盛会,欧洲太空科技博览会将于1024日至26日在德国不来梅省举办。该国际博览会是奇石乐展会计划中的一项固定活动。届时,我们的专家将在5号展厅A51展台向观众展示奇石乐的测量技术实力,以及针对挑战性空间应用的解决方案。

传感器通过提供有价值的测量结果辅助实现空间系统和子系统的质量、安全性和可靠性,因此在空间有效载荷、推进力、子系统测试中发挥着关键作用。由于应用环境存在温差大、压力波动大、冲击和振动强度高等极端情况,行业产品必须满足非常苛刻的要求。同时,测量设备往往还必须具备轻巧、结实、耐用等特点,而奇石乐制造的力传感器、振动传感器及压力传感器几乎适合所有应用。

在此次欧洲太空科技博览会上,我们将重点向观众展示针对多个选定空间应用的产品解决方案。观众可以在我们的展台上看到内置压力、力、加速度传感器的火箭发动机测试台、以及新式9306A型压电式六分量力/转矩连杆等展品。

奇石乐战略业务现场测试与测量部主管Manuel Blattner

直接、精确测量,适用于任意方向

在振动试验过程中,卫星及其子系统会因超载会遭到严重损坏,我们采用力限振动试验来防止这种情况发生。该试验在振动器至有效载荷接口处使用3分量力传感器对外来力进行监控。奇石乐将在博览会上展示该应用的理想解决方案——与尖端的信号调节和数据采集系统相连的预载3分量压电式力传感器。这种预载传感器安装在两个安装法兰之间,可测量各个方向的压力和张力。而高刚性能够实现较高的自然频率和较低的串扰,从而保证测量结果的精确度。

信号的测定和调节采用奇石乐首款多通道准静态及动态电荷放大器LabAmp 5167A。该产品具备模拟输出和综合数据采集功能,具备多项优点,包括:信号调节器和数据采集系统可扩展、可配置、性能高,支持通道同步,信号过滤,虚拟通道,方便评估单个力信号等。此外,综合数据采集使测量链进一步简化并提高了适应力。

在极端压力下获得最佳结果

火箭会承受很大的压力,尤其是在发射过程中。为了防止工作期间出现故障,测试阶段需对火箭组件,尤其是火箭发动机进行多次测试和检查。奇石乐还将在欧洲太空科技博览会上展示6021A型高温压力传感器。这种非冷却型压力传感器可应用于高可达700℃的温度,为判断燃烧过程和相关不稳定性提供高分辨率的压力测量结果。为此,该压力传感器采用了与地面绝缘的设计,并与一个低噪声、免电磁干扰的差动电荷放大器相连,以此实现测量的精确性。

 奇石乐还将在博览会上展出符合高温测试环境要求的5181A型差动电荷放大器,观众届时将有机会一睹其优势。

可靠地测量小扭矩和力

奇石乐还将在欧洲太空科技博览会上重点展出首款9306A型压电式6分量力/转矩连杆。该传感器无需计算即可提供3种力与3种转矩的精确、直接测量结果,是风洞内部测量的完美选择。通过奇石乐电荷放大器,用户可以自行调节各轴线的转矩和力测量范围。得益于压电测量原理和9306A型传感器的产品性能,即使是微小的转矩和力,用户也能轻松获取高分辨率的测量结果。

了解更多欧洲太空科技博览会展品情况
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.