可靠的车辆碰撞测试测量方案——无惧测量中断

20206月——奇石乐推出了新型超级电池 KiBAT和新的静态KiDAU据采集系统,为高效、成功的车辆安全测试和碰撞测试提供更优质的解决方案。

随着汽车碰撞测试中,传感器使用数量的不断增加,为了保证数据采集系统可靠地采集数据。奇石乐推出新型超级电池系统KiBAT,大大补充了KiDAU数采和DTI内置假人数采地采集测量持续待机时间,给试验提供更可靠的供电保障。

特殊功能的备用电池

碰撞测试过程中,随着内置假人和传感器数量的增加,数据采集系统的耗电量不断增加,持久的待机时间和连续工作时间成为最新的需求。为奇石乐推出更强大的自动切换供电的电池 KiBAT K3885。这款具备特殊功能的电池将通过CrashLink2总线,为所有车载组件提供供电支持。KiBAT K3885可在十分钟内持续供电400瓦,有效避免测量中断,系统能够持续采集可靠的测量数据。此外,KiBAT内置LED灯,可显示电量状态,且会在电量过低时发出声音警示。

KiBAT可通过CrashLink2总线自动打开电池电源,也可选择手动开启,其灵活性确保用户可在不同应用情境中轻松完成试验配置。

KiBAT是车载数据采集链的有力补充,用户可通过该产品,确保碰撞测试准备和执行进程的顺利进行。奇石乐从广泛的车辆安全系统试验和测试中积累了丰富的经验,并充分利用此经验持续研发新产品,旨在进一步提高车辆和交通安全。

高效的车辆安全部件测量解决方案——适用于试验室测量

KiDAU K3880AS 静态数采,集成多种测量采集包括模拟量采集,数字量采集,DTI-Bus总线采集,该产品配备19英寸的测量机架,以及多种即插即用、可级联的测量模块。奇石乐专门开发的这款通用静态数据采集系统被用来进行碰撞测试用假人的标定试验,假人准备检测工作。同时K3880AS 静态数采可以被用来进行汽车零部件试验数据采集等应用。如今,即使是在试验室等静态测量应用环境中,用户也能体验到与车载数采同样卓越和可靠的品质。

基本单元集成多种接口,可连接功能各异的碰撞测试外接型设备。KiDAU K3880AS可通过4个CL2接口,与现有车载设备直接连接;其采用标准的19英寸设计,良好的低发热性能,使其无需风扇降温。同时,该设备采用模块化架构设计,能够容纳最多8个即插即用型I/O测量模块。KiDAU K3880AS配备具有16个数字通道采集模块,该模块在最高采样率100kHz的采样频率下可循环记录1800秒,可以在试验开始前提前启动数据记录功能。此外,KiDAU K3880AS可搭载8通道模拟信号采集模块,每个采集模块均配备可编程输入信号放大器、桥路激励电路、低通滤波器和16位模数转换器。系统配置过程中,用户可通过软件自动完成预设的所有设置,也可选择手动调试。丰富的功能使KiDAU K3880AS数据采集系统具备广泛的适用性,因此,这套简便易用、高度可靠的解决方案,是保证假人检查和零部件试验结果可靠的理想选择。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.