可靠的微型切削方案

温特图尔,2018年5月29日– 经过近两年的研发时间,Kistler 推出了世界上最小的量产切削测力仪 MicroDyn。从现在开始,生产企业和研究机构将获得在微型刀具开发时高精度切削力测量的解决方案。

微小型工件的加工对使用刀具提出了较高要求。为了能够在最狭小的空间内——例如在钟表制造中——测量切削力,需要非常紧凑和高灵敏度的测量仪器。通过9109AA型微型测力仪,Kistler 为其超细加工、微精密加工和超精密加工领域的客户提供了新的解决方案——尤其是在硬脆性材料加工研发和和加工工艺的优化方面。.

最小的测力仪上市

凭借 30x30 mm 的外观尺寸,MicroDyn 成为世界上最小的测力仪。得益于三向 15 kHZ 的高固有频率——与此前产品相比提高系数约为2.5——能够十分准确地测量最大 500 N 的高动态力及50 Nm 的计算扭矩。由此能够测量刀具120,000 转速下单个刀刃的切削力。压电石英测量环保证了高灵敏度和非常低的阈值。此外其结构能够基本抵消温度影响。

刀具研发中的精准测量

特别是在新刀具研发时,了解其表现至关重要:出现了哪些切削力?刀具在不同情况下的表现(工艺稳定性)如何?刀具如何设计以避免力的峰值(提高使用寿命)同时使加工过程保持快速而高效?研发过程中仅通过准确测量即可以确保实现加工过程的可靠性并避免故障。例如钟表制造商在铣削外壳时,必须确保即使在进给条件不断变化的情况下,过程也运行稳定并且刀具不过载。

灵活的固定方式和数据分析

新的9109AA型 微型测力仪具有多种固定方式,既可以垂直也可以水平地安装在机床工作台上,工件从而可以相应地进行夹持。这对测量精度有利。为了快速无误的采集数据和分析,推荐使用5080A型高端多通道电荷放大器与微型测力仪的组合。Kistler 提供包括 Dynoware 软件在内的完整解决方案实现简单无误的配置,其中已储存了用于力和扭矩计算的公式。原则上,MicroDyn微型测力仪 也可以结合其它采集分析系统使用。MicroDyn 现在即可供货。

更多信息,请访问 www.kistler.com/microdyn
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.