准确测量巨浪 — 实现有效的海啸灾害防护

2019 年 8 月,温特图尔 — 在外海出海的日本渔民未发现任何异常。一切风平浪静,海上的情况也一如往常。但是,当他们驶进港口时,等待他们的却是一番触目惊心的景象:海岸几乎成了废墟 — 一股巨浪猛烈地冲击着建筑物和船只,以毁灭性的力量卷向动物和人们。这种现象称之为海啸,在日语中的意思是“港口波浪”。奇石乐的力传感器在海啸研究中发挥着关键作用。 

防御型建筑物的有效设计需要了解海啸波在影响建筑物时所产生的力 — 但目前为止,关于这方面的研究少之又少。显然,海防机构需要基于可靠的数据来建设未来的设施。为了满足这一要求,英国独立水力研究协会 HR Wallingford 与伦敦南岸大学讲师、前伦敦大学学院助理研究员 David McGovern 博士展开了密切合作。欧洲最大的波流水道 Fast Flow Facility 位于英国沃林福德镇,该设施也是世界上唯一可以模拟海啸的地方。目前的测试按 1:50 的比例进行。Fast Flow Facility 设施大小为 70 米 x 4 米。只有研究海啸在三维空间中的形成方式才能理解引发海啸的复杂力量。

面对这一挑战,McGovern 博士找到了瑞士传感器技术方面的专家奇石乐,帮助他深入观察波浪形成时作用的力。作为压电测量领域的市场领导者,奇石乐致力于各类传感器研发,包括特殊培养的石英晶体。这种晶体可以将波浪和移动水团所产生的力转化为电荷,从而实现对这些力的测量。这种情况所需的特殊功能是:用于海啸研究的传感器可以测量三个维度的力。

凭借这项技术,研究团队可以精确测量波浪在空间和时间上的整体形成。研究团队还能确认模拟海浪的数据与真实海啸数据的吻合度,从而确定研究结果的意义和可靠性。现在,这些数据为未来的海防建设项目奠定了良好的基础,因为研究人员终于有可靠的方法来模拟和计算海啸对不同建筑物形状的影响。在瑞士测量技术专家的帮助下,英国团队发挥了重要作用,他们能帮助确保未来的防御措施在海啸袭来时能挽救更多人的生命。
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20.11.2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09.05.2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08.05.2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03.05.2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24.04.2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12.04.2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06.03.2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16.02.2018
在阿姆斯特丹国际交通展览会上,奇石乐集团展示全面的KiTraffic动态称重(WIM)解决方案,其在道路和交通监控、非现场执法以及计重收费等方面为道路业主和道路管理部门提供支持。新的扩展服务包为众多应用提供了更多便利,并确保动态称重设备在整个系统生命周期中保持出色性能。
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
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
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19.05.2014
Users obtain a full range of force–displacement measurement systems from one source
06.02.2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.