The Technical University (TU) Dortmund tests new MicroDyn dynamometer from Kistler

The Institute of Machining Technology (ISF) at Dortmund Technical University (TU) has spent more than four decades researching and teaching in the field of machining covering all relevant machining processes and related technical subjects. A team of research associates are currently working in the Collaborative Research Center (CRC) Transregio 73. As part of sub projects B2 and B3, research is being conducted into the manufacture and modification of forming machines on which very hard tool steels (> 60 HRC) have to be machined with micro tools. Kistler provided the ISF with the new MicroDyn 9109AA cutting force dynamometer for the project. Thanks to its very high natural frequency, the world's smallest dynamometer unlocks completely new possibilities for the institute in the development of its micromachining processes – with astounding results. 

The ISF currently numbers more than 80 research associates, technical and student supporting staff, who are engaged in three research departments: machining, grinding technology and simulation and process development. The departments are equipped with modern machine tools and machining centers to achieve machining processes of the highest standard. The scientists also have access to comprehensive measurement technology and a computer infrastructure with well-developed basic equipment. Suitable premises and laboratories enable tests to be performed in the right framework conditions and the results precisely evaluated.

New manufacturing technology to master economical and ecological challenges 

As part of the Collaborative Research Center (CRC) Transregio 73, the TU Dortmund is working with the Leibnitz University Hanover and Friedrich-Alexander University Erlangen-Nürnberg. Funded by the German Research Foundation (DFG), the Collaborative Research Center was initiated to develop a new manufacturing technology called sheet-bulk metal forming (SBMF). This technology is designed to unite the advantages of sheet and bulk metal forming processes and extend possibilities with regard to component complexity. Besides the development of forming processes, the manufacture of innovative forming tools with specific characteristics represents a major step towards technology transfer into practical industrial implementation. Micromachining offers significant benefits in respect to the required form, dimensional accuracy and surface integrity, while enhancing the efficient and economical manufacture of forming tools and prolonging tool life. 

“Scientists would be fumbling in the dark if it wasn't for measurement technology” 

Eugen Krebs has been a research associate at the ISF for several years and is responsible for the sub project B2 along with Alexander Meijer in the CRC Transregio. The two colleagues' work at the institute focuses on micromachining. Their duties include process and tool development for the respective machining tasks for which they need the right measurement technology. “Micromachining demands the highest standards from measuring equipment on account of the very fine dimensions. Machining involves mechanical processes in which highly dynamic forces can occur over a very wide measurement range. Reliable measurement and analysis of these forces is crucial for our process evaluation. Without measurement technology, we scientists would be left to fumble in the dark,” explains Krebs. Along with 22 other research associates, he has been doing research in the Transregio CRC since 2010. “The Collaborative Research Center Transregio 73 plays a significant role in the necessary development of forming technology, and thus also in the mastering of current economical and ecological challenges,” adds Krebs. “This project creates the scientific fundamentals that will enable us to satisfy growing demand for customized, flexible systems of increasing functional density.” The results achieved will improve the economic and resource efficiency of forming processes. 

Daunting process requirements 

Forming tools in sheet-bulk metal forming consist of very fine, complex forming elements, which at the same time have to withstand high stresses. “We had to discount a lot of materials for the forming tools in the project because they simply didn't match up to our requirements,” continues Krebs. In the end, they opted for a powder metallurgical high speed steel with high resistance to wear and tear and dimensional stability with case hardening of up to 65 HRC. “At the beginning of the Transregio, we doubted that materials of this nature could be reliably machined at all with micro tools (less than d = 1 mm in diameter). Sub project B2 focused on tackling this challenge.”

Machining involves mechanical processes in which highly dynamic forces can occur over a very wide measurement range. Reliable measurement and analysis of these forces is crucial for our process evaluation. Without measurement technology, we scientists would be left to fumble in the dark.”

Eugen Krebs, research assistant at the ISF

 

The solution: Rugged measurement technology with high natural frequency 

Developing micromachining processes for high-strength materials with tool diameters ranging from 0.2 to 1 millimeter involved in-depth machining tests in which both suitable process parameters were to be identified and tool concepts optimized. Reliable measurement technology was required for the job, capable of both responding very sensitively and clearly while precisely mapping forces of less than 1 N to more than 200 N in a single process run. Another key criterion required by the ISF of measurement technology was high natural frequency. “If the natural frequency range of the force measurement system is less than 4,000 Hz, the force measurement platform will be excessively excited during the micromachining process, so we might end up measuring platform vibration instead of cutting force signals,” admits Krebs. Rugged qualities were also important for measurement technology to ensure that external influences like temperature or cooling lubricant did not compromise the process. And finally, repeatability and measurement accuracy were prioritized by the research team. “We frequently repeat measurements up to five to ten times. So of course it is crucial to obtain comparable, reliable results for the same tests,” concludes Krebs. 

Exploring the impossible with Kistler 

The MicroDyn 9109AA cutting force dynamometer fulfills all the above ISF requirements, and also offers many other benefits. “The TU Dortmund and the Kistler Group can look back on a long, intensive partnership. In the past, we have frequently conducted research with different Kistler dynamometers, and so far we have been very happy with them all. When we were given the opportunity to test the prototype of the new MicroDyn 9109AA dynamometer to assess our analyses of tool modifications, we jumped at the chance,” Krebs remarks.

The ISF has been using the dynamometer since February 2018. What has changed since? Krebs: “Before using the new Kistler dynamometer, our problem was that the micromachining force measurements were always compromised by the measurement instrument's natural frequencies. We no longer have to contend with this obstacle. Thanks to the high natural frequency of 15 kHz on all three axes (x, y, z), we can measure highly dynamic forces at spindle speeds of up to 160 000 rpm. This increases dynamic properties by a factor 2.5 compared to the predecessor product.” The device is also suitably dimensioned for a measurement range of up to 500 N. “We have never achieved the likes of this with our measurement technology. The MicroDyn has played an important role in extending the bounds of the possible. Now we are able to analyze processes with cutting speeds of vc > 500 m/min using small tool diameters,” remarks Krebs. “This measurement technology development provides new insights into micromachining, which used to be beyond our reach due to technological limitations.”

Although the Transregio 73 research program will finish at the end of 2020, Krebs and Meijer firmly intend to continue using the Kistler dynamometer. “We would like to explore further tool modifications and stretch the process limits of micromachining even further. So we look forward to the continued support of Kistler's measurement technology experts in the development of our processes.”

17.07.2019
Turkey opts for weight enforcement with WIM technology from Kistler
24.06.2019
载人飞船再次登月,奇石乐以可靠的测量结果保障月球之旅
20.06.2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14.05.2019
为确保零部件和医疗部件的卓越品质,Tessy公司选择了奇石乐传感器和解决方案。
18.04.2019
德国某知名小家电制造商对奇石乐集团旗下公司Vester的自动测试和分拣系统非常信赖。
02.04.2019
奇石乐MARS测力台系统,美国国家橄榄球联盟(NFL)职业橄榄球队——杰克逊维尔美洲虎队(Jacksonville Jaguars)训练智能化的秘密武器
25.03.2019
Schurter AG采用奇石乐过程监控系统maXYmos,以满足汽车制造业对质量控制和可追溯性的严格要求。
18.03.2019
如何高效判断运动员体能状态?奇石乐Quattro Jump运动表现分析系统报告为您提供有效支持。
17.12.2018
奇石乐精准的动态称重(WIM)技术,可持续的保护匈牙利国内道路免受超载车辆损坏。
27.11.2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10.10.2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08.10.2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31.08.2018
采埃孚公司启用带有集成化振动装置的奇石乐软件控制式紧固件测试台。
14.08.2018
大昭和精机株式会 (BIG Daishowa), 总部位于日本大阪,是机械 加工业刀柄的主要生产商之一。公司每年生产50多万个弹簧夹头。 其产品是采用奇石乐(Kistler)的切削力测量设备以及其他资源研发 而成。
16.07.2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11.04.2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14.11.2017
在冷却润滑液产品研发过程中,巴索润滑液公司依靠了奇石乐的专业测量系统。
29.08.2017
Applus IDIADA依赖于奇石乐的内置假人测量技术。
04.01.2017
奇石乐能够检测到车辆碰撞试验中最喜欢的变化,帮助提高事故生存率
22.12.2016
奇石乐优化车辆综合测试
20.12.2016
奇石乐传感器在任何条件下都能最大程度的保证数据的准确度
07.11.2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
28.10.2016
漫步在训练场(已有三年历史)内,立即被一个长长的混凝土建筑所吸引。与办公室和更衣室相同的是,该建筑物有现代化的训练区域,该区域自2015年底以来使用了奇石乐的测力台。该技术产生的测量结果让培训主管深入了解他们球员的身体状况。
17.08.2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19.02.2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04.11.2015
Piezoelectric Measurements with CompactRIO™
15.06.2015
Measurement Solutions for Automotive Test Systems
08.05.2015
Quality Assurance in the Automotive Industry
02.03.2015
博泽如何提高双组份制品品质和自动分离缺陷制品
02.12.2014
奇石乐集团追求的是进取和可持续增长的策略– 战略收购是该策略的核心要素之一。这意味着,奇石乐考虑和选择一些企业合作,可以实现更高的目标。2006 年对 Dr. Staiger Mohilo& Co. GmbH 公司的收购就是这种价值观的体现。通过这次收购, 奇石乐和被收购公司得到了共同发展,达到了双赢的目的。
02.12.2014
在太阳系飞行了十年之后,Rosetta 航天器于 2014 年 11 月 12 日将探测器 Philae 发射到“Chury”彗星上。为了避免探测器在 40 亿英里的太空航行中耗尽燃料,使用了奇石乐集团的压力传感器对燃料消耗量进行全程监测。
23.08.2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15.02.2011
End-to-end process monitoring for critical medical moldings
07.02.2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
联系方式
Cara-Isabell Maercklin
Cara-Isabell Maercklin
Media Contact
联系方式
(max 25 Mb)