Ohio authorities rely on Weigh In Motion technology from Kistler

The US state of Ohio is stepping up its efforts to collect traffic data so that it can claim important Federal budget funding to conserve infrastructure. Kistler Lineas sensors achieved exceptionally convincing results in the state's tests on Weigh In Motion systems.

Although Ohio is one of the smaller US states in terms of area, it is a key center of industry and business. From Cleveland on the shore of Lake Erie in the north to Columbus and Cincinnati in the southwest, Ohio has the seventh largest gross domestic product (GDP) of all US states, and is second only to neighboring Michigan in automobile production. Ohio is known as the Buckeye State, after the native tree similar to a horse chestnut that has a characteristic tan-colored eye in the middle of its seed. In US Presidential elections, Ohio is traditionally regarded as a swing state and a bellwether that usually votes with the winning party.

In some ways, Ohio resembles the German Federal State of Baden-Württemberg: the two territories have similar populations (about 11 million), their GDPs are comparable (about EUR 500,000 million), and the enterprise structure of both Ohio and Baden-Württemberg is defined by the automotive industry and its supply sector. However, Ohio has three times the area of Baden-Württemberg: it is located centrally in the United States, within one day's drive for 60% of the North American population. Responsibility for developing and conserving the highway infrastructure is assigned to the Ohio Department of Transportation (ODOT): with a workforce of over 4,500, this state agency controls all aspects of construction, planning, traffic monitoring and transportation safety.

For installation, operation and durability – quality is the focus

Dave Gardner, Manager of ODOT's Traffic Monitoring Section, shares responsibility for traffic oversight throughout the state of Ohio with his colleague Sandie Mapel, Field Manager. “Acquiring precise traffic data is very important for us because allocation of Federal budget funds depends on those statistics,” Gardner explains. “Axle loads and overall truck weights are recorded and submitted for the Federal Data Plan.”

ODOT currently operates 22 Weigh In Motion (WIM) stations to monitor stress on Ohio's roads caused by trucks and heavy commercial vehicles. “We'll gradually be adding more installations in the coming years,” Mapel adds. “We believe it's very important to deploy the correct systems in terms of installation, operation and data quality.”

A practical, high-performance system: Kistler Lineas scores convincingly in field tests

To investigate its options, ODOT installed a WIM test section on US Route 23, which links the country's far north to Florida and crosses Ohio from north to south. The traffic monitoring experts at ODOT were impressed by the performance of quartz-based Lineas sensors from Kistler. “Their compact design makes them easy to install, especially in existing roads. The Lineas sensors combine long service lifetimes with data quality that leaves nothing to be desired,” Mapel comments. “For all these reasons, we'll be deploying more Kistler sensor technology to acquire traffic data in the future. We're also examining how much use we could make of the complete KiTraffic Statistics system,” she concludes. Another test section to assess this option is due to be set up in Ohio before long.

Progressive expansion with technology from Kistler on board

ODOT’s first Kistler Lineas sensor installation was back in 2007, and the agency has been increasing its use of Lineas sensors since 2016. The oldest Kistler installation still operating in the state today dates from 2011. 

When asked if more WIM applications could be implemented with Kistler – such as direct camera-based collection of fees for overloaded vehicles (“direct enforcement”) or protection of bridges against overloaded trucks – Gardner slows the pace: “We aren't there yet! Law enforcement carry out random checks on trucks, and we also send them traffic monitoring data for analysis purposes. But the data isn't forwarded to Law Enforcement in real time.”

On the other hand, the situation for bridges could be different. Ohio has the second largest number of bridges of all 50 US states and many of them were built after the second world war, so they require appropriate monitoring, protection and maintenance. Technology from Kistler can help prevent damage inflicted on bridges by overloaded vehicles. Such vehicles can be prevented from driving onto a bridge with the help of accurate WIM data that is available in real time – so bridge lifetimes become substantially longer. “However, a different department at ODOT is responsible for that,” Gardner notes. Including Ohio, 48 out of the 50 US states are now operating WIM technology from Kistler. With over 50,000 Lineas sensors already installed in more than 50 countries, WIM by Kistler is internationally recognized as the solution of choice to protect road infrastructure, improve traffic safety, and collect weight-based toll fees.

Lineas quartz sensors for Weigh In Motion (WIM)

Lineas quartz sensors (9195G) are used to measure wheel and axle loads, and they can also determine gross vehicle weights with no disruption to traffic flow. Installed in the road pavement, these sensors deliver highly accurate measurement signals.

Key product features and user benefits at a glance:

  • Quartz technology for high-precision measurements and long-term stability
  • Compliant with OIML R134 (accuracy class 2)
  • Long life expectancy thanks to rugged sensor design
  • Wide measuring range
  • Nonstop weighing at low to high speeds
  • Insensitive to temperature fluctuations
  • Installation in the road pavement is fast and easy
05.10.2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18.09.2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20.08.2020
精度是高性能的关键:了解奇石乐测量技术如何助力埃莫克法兰肯(EMUGE FRANKEN)公司研发团队。
22.07.2020
奇石乐ComoNeo满足上海天泽精密模具精密生产要求。
09.06.2020
奇石乐助力森拉天时(Ceratizit)开发高动态车削(HDT)系统,用户仅需一把刀具,即可完成复杂几何结构的加工。
15.11.2019
奇石乐过程监控系统及模腔压力传感器帮助大幅降低注塑成型零件故障率。
23.10.2019
奇石乐测量技术如何助力提升顶级电动工具质量
15.08.2019
奇石乐分析系统如何提高紧固技术的安全性和透明度。
17.07.2019
土耳其选择搭载有奇石乐动态称重系统(WIM)的车辆超载执法管理
24.06.2019
载人飞船再次登月,奇石乐以可靠的测量结果保障月球之旅
20.06.2019
瞬间自动分离良品和次品,每个周期只有短短1.5秒:奇石乐过程监控系统保证年产量达500万件产品的高质量
14.05.2019
为确保零部件和医疗部件的卓越品质,Tessy公司选择了奇石乐传感器和解决方案。
18.04.2019
德国某知名小家电制造商对奇石乐集团旗下公司Vester的自动测试和分拣系统非常信赖。
02.04.2019
奇石乐MARS测力台系统,美国国家橄榄球联盟(NFL)职业橄榄球队——杰克逊维尔美洲虎队(Jacksonville Jaguars)训练智能化的秘密武器
25.03.2019
Schurter AG采用奇石乐过程监控系统maXYmos,以满足汽车制造业对质量控制和可追溯性的严格要求。
18.03.2019
如何高效判断运动员体能状态?奇石乐Quattro Jump运动表现分析系统报告为您提供有效支持。
17.12.2018
奇石乐精准的动态称重(WIM)技术,可持续的保护匈牙利国内道路免受超载车辆损坏。
27.11.2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10.10.2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08.10.2018
多特蒙德工业大学(TU)机械加工技术研究所(ISF)测试奇石乐新型MicroDyn 9109AA型切削力测力仪,为该研究所在开发微加工工艺方面打开全新的局面,
31.08.2018
采埃孚公司启用带有集成化振动装置的奇石乐软件控制式紧固件测试台。
14.08.2018
大昭和精机株式会 (BIG Daishowa), 总部位于日本大阪,是机械 加工业刀柄的主要生产商之一。公司每年生产50多万个弹簧夹头。 其产品是采用奇石乐(Kistler)的切削力测量设备以及其他资源研发 而成。
16.07.2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11.04.2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14.11.2017
在冷却润滑液产品研发过程中,巴索润滑液公司依靠了奇石乐的专业测量系统。
29.08.2017
Applus IDIADA依赖于奇石乐的内置假人测量技术。
04.01.2017
奇石乐能够检测到车辆碰撞试验中最喜欢的变化,帮助提高事故生存率
22.12.2016
奇石乐优化车辆综合测试
20.12.2016
奇石乐传感器在任何条件下都能最大程度的保证数据的准确度
07.11.2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
28.10.2016
漫步在训练场(已有三年历史)内,立即被一个长长的混凝土建筑所吸引。与办公室和更衣室相同的是,该建筑物有现代化的训练区域,该区域自2015年底以来使用了奇石乐的测力台。该技术产生的测量结果让培训主管深入了解他们球员的身体状况。
17.08.2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19.02.2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04.11.2015
Piezoelectric Measurements with CompactRIO™
15.06.2015
Measurement Solutions for Automotive Test Systems
08.05.2015
Quality Assurance in the Automotive Industry
02.03.2015
博泽如何提高双组份制品品质和自动分离缺陷制品
02.12.2014
奇石乐集团追求的是进取和可持续增长的策略– 战略收购是该策略的核心要素之一。这意味着,奇石乐考虑和选择一些企业合作,可以实现更高的目标。2006 年对 Dr. Staiger Mohilo& Co. GmbH 公司的收购就是这种价值观的体现。通过这次收购, 奇石乐和被收购公司得到了共同发展,达到了双赢的目的。
02.12.2014
在太阳系飞行了十年之后,Rosetta 航天器于 2014 年 11 月 12 日将探测器 Philae 发射到“Chury”彗星上。为了避免探测器在 40 亿英里的太空航行中耗尽燃料,使用了奇石乐集团的压力传感器对燃料消耗量进行全程监测。
23.08.2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15.02.2011
End-to-end process monitoring for critical medical moldings
联系方式
(max 25 Mb)