Kistler’s Performance Analysis System Prepares Swimmers for the Rio Olympics

For competitive swimmers, performance at starts and turns is a key factor in achieving better results. Just a few hundredths of a second decide whether the race is won or lost. This is why Kistler developed its Performance Analysis System for Starts, Turns and Relay Changeovers: the ideal tool to optimize each individual athlete's performance. 

Continuous Optimization as Challenge

All over the world, swimmers are driven on by the vision of being crowned as an Olympic Champion before cheering crowds. But to attain elite level and perfect their technique, swimmers have to put in endless hours of training. And when the moment of truth finally arrives, only a few hundredths of a second separate the Olympic champion from the rest – so coaches and performance analysts depend on reliable, objective data to work towards achieving the narrow margin that makes all the difference.

Success Factor Reliable Data

Objective and reliable data is the key to improving the performance of elite athletes. Leading experts in both swimming and biomechanics work together to define critical performance parameters. Then, these parameters are analyzed with the help of various measurement systems: for example, the equipment integrated into the biomechanical analysis process includes instrumented starting blocks, turning plates, high-speed video cameras and timing devices.

Kistler's Solution

The Kistler Performance Analysis System for Swimming delivers kinetic and kinematic information about starts, turns and relay changeovers. Drawing on over 50 years' experience of measuring infinitesimal differences in movements, Kistler has developed products that fully meet the requirements of modern performance analysis in sport. The instrumented starting block measures the forces that act as the swimmer starts off; then, cameras focus on his or her individual movements in the underwater phases. Finally, analytical software displays the video with biomechanical analysis − in a clear format that's easy to understand.

Achieving success with Kistler

Kistler’s Performance Analysis System for Swimming offers two key advantages: it can deliver immediate feedback, and it can compare two different trials on one screen. This detailed information gives coaches and athletes the basis to adapt performance directly and make minor changes in the next trial. The results: progress towards the goal, and increased benefit from training sessions. So: take the lead – right from the start!

Please find more information about the advantages of our Performance Analysis System for Swimming.

Our highly qualified employees push the limits of what is possible and deliver answers with our customers – and for our customers – to the great questions posed by a connected world around the megatrends mobility, emission reduction, quality control and lightweight construction.

Do you want to play a part in shaping the future? If so, become part of our team. 

26.06.2022
Heavy-duty application on the test track: S6XT delivers high-precision load measurements in Japan
04.05.2022
奇石乐MaDaM和jBEAM软件助力戴姆勒客车全电动城市公交车进一步研发
11.04.2022
ISTAR研究飞机在地面和空中都使用了IEPE和MEMS加速度计,助力研究的成功之路。
18.11.2021
使用奇石乐ANALYSE系统开展先进的紧固件测试,为汽车和风机制造业的锌片涂层工艺提供保障
12.10.2021
玉柴如何在符合国六标准的发动机生产中实现更高的精度、透明度和资源使用效率。
14.09.2021
配备测力仪、实验室电荷放大器和软件的高精度测量链可以进行客观的对比测试。
09.09.2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03.09.2021
Estudio de la Pisada足科诊所位于西班牙瓦伦西亚,其足科专家使用奇石乐3D测力台为患者和运动员制定治疗方案、制作矫形器。
02.07.2021
两个IEPE加速度计为推进器验证和优化飞行特性提供了关键数据,即使在平流层也是如此。
22.06.2021
使用测力台捕捉微振动,优化卫星技术。
02.06.2021
尽管产量大,仍实现零缺陷:使用Kistler测试自动化系统对锌压铸件进行质量保证。
26.04.2021
数字驱动的制动力测量系统使维修技术人员的列车维修更加轻松。
13.04.2021
荷兰海洋研究所MARIN的“大气”测试系统中安装了100个Kistler压力传感器,用于捕获不同环境条件下的波浪冲击力。
22.03.2021
MAN Energy Solutions使用奇石乐传感器,研发顺应未来趋势的燃气轮机
08.02.2021
针对撑杆跳运动训练和生物力学的测量技术助力更好表现。
05.10.2020
配备压电传感器的数字化测量链如何集成于复杂的车辆试验台中?
18.09.2020
令人信服的测试结果:俄亥俄州运输部将进一步增加奇石乐Kistler Lineas传感器的使用,进行交通监测。
20.08.2020
精度是高性能的关键:了解奇石乐测量技术如何助力埃莫克法兰肯(EMUGE FRANKEN)公司研发团队。
22.07.2020
奇石乐ComoNeo满足上海天泽精密模具精密生产要求。
09.06.2020
奇石乐助力森拉天时(Ceratizit)开发高动态车削(HDT)系统,用户仅需一把刀具,即可完成复杂几何结构的加工。
15.11.2019
奇石乐过程监控系统及模腔压力传感器帮助大幅降低注塑成型零件故障率。
23.10.2019
奇石乐测量技术如何助力提升顶级电动工具质量
15.08.2019
奇石乐分析系统如何提高紧固技术的安全性和透明度。
17.07.2019
土耳其选择搭载有奇石乐动态称重系统(WIM)的车辆超载执法管理
24.06.2019
载人飞船再次登月,奇石乐以可靠的测量结果保障月球之旅
20.06.2019
瞬间自动分离良品和次品,每个周期只有短短1.5秒:奇石乐过程监控系统保证年产量达500万件产品的高质量
14.05.2019
为确保零部件和医疗部件的卓越品质,Tessy公司选择了奇石乐传感器和解决方案。
18.04.2019
德国某知名小家电制造商对奇石乐集团旗下公司Vester的自动测试和分拣系统非常信赖。
02.04.2019
奇石乐MARS测力台系统,美国国家橄榄球联盟(NFL)职业橄榄球队——杰克逊维尔美洲虎队(Jacksonville Jaguars)训练智能化的秘密武器
25.03.2019
Schurter AG采用奇石乐过程监控系统maXYmos,以满足汽车制造业对质量控制和可追溯性的严格要求。
18.03.2019
如何高效判断运动员体能状态?奇石乐Quattro Jump运动表现分析系统报告为您提供有效支持。
17.12.2018
奇石乐精准的动态称重(WIM)技术,可持续的保护匈牙利国内道路免受超载车辆损坏。
27.11.2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10.10.2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08.10.2018
多特蒙德工业大学(TU)机械加工技术研究所(ISF)测试奇石乐新型MicroDyn 9109AA型切削力测力仪,为该研究所在开发微加工工艺方面打开全新的局面,
31.08.2018
采埃孚公司启用带有集成化振动装置的奇石乐软件控制式紧固件测试台。
14.08.2018
大昭和精机株式会 (BIG Daishowa), 总部位于日本大阪,是机械 加工业刀柄的主要生产商之一。公司每年生产50多万个弹簧夹头。 其产品是采用奇石乐(Kistler)的切削力测量设备以及其他资源研发 而成。
16.07.2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11.04.2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14.11.2017
在冷却润滑液产品研发过程中,巴索润滑液公司依靠了奇石乐的专业测量系统。
29.08.2017
Applus IDIADA依赖于奇石乐的内置假人测量技术。
04.01.2017
奇石乐能够检测到车辆碰撞试验中最喜欢的变化,帮助提高事故生存率
22.12.2016
奇石乐优化车辆综合测试
20.12.2016
奇石乐传感器在任何条件下都能最大程度的保证数据的准确度
07.11.2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
28.10.2016
漫步在训练场(已有三年历史)内,立即被一个长长的混凝土建筑所吸引。与办公室和更衣室相同的是,该建筑物有现代化的训练区域,该区域自2015年底以来使用了奇石乐的测力台。该技术产生的测量结果让培训主管深入了解他们球员的身体状况。
17.08.2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19.02.2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04.11.2015
Piezoelectric Measurements with CompactRIO™
15.06.2015
Measurement Solutions for Automotive Test Systems
08.05.2015
Quality Assurance in the Automotive Industry
02.03.2015
博泽如何提高双组份制品品质和自动分离缺陷制品
02.12.2014
奇石乐集团追求的是进取和可持续增长的策略– 战略收购是该策略的核心要素之一。这意味着,奇石乐考虑和选择一些企业合作,可以实现更高的目标。2006 年对 Dr. Staiger Mohilo& Co. GmbH 公司的收购就是这种价值观的体现。通过这次收购, 奇石乐和被收购公司得到了共同发展,达到了双赢的目的。
02.12.2014
在太阳系飞行了十年之后,Rosetta 航天器于 2014 年 11 月 12 日将探测器 Philae 发射到“Chury”彗星上。为了避免探测器在 40 亿英里的太空航行中耗尽燃料,使用了奇石乐集团的压力传感器对燃料消耗量进行全程监测。
23.08.2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15.02.2011
End-to-end process monitoring for critical medical moldings
联系方式
文件大小不超过 25 MB