Kistler’s Performance Analysis System Prepares Swimmers for the Rio Olympics

For competitive swimmers, performance at starts and turns is a key factor in achieving better results. Just a few hundredths of a second decide whether the race is won or lost. This is why Kistler developed its Performance Analysis System for Starts, Turns and Relay Changeovers: the ideal tool to optimize each individual athlete's performance. 

Continuous Optimization as Challenge

All over the world, swimmers are driven on by the vision of being crowned as an Olympic Champion before cheering crowds. But to attain elite level and perfect their technique, swimmers have to put in endless hours of training. And when the moment of truth finally arrives, only a few hundredths of a second separate the Olympic champion from the rest – so coaches and performance analysts depend on reliable, objective data to work towards achieving the narrow margin that makes all the difference.

Success Factor Reliable Data

Objective and reliable data is the key to improving the performance of elite athletes. Leading experts in both swimming and biomechanics work together to define critical performance parameters. Then, these parameters are analyzed with the help of various measurement systems: for example, the equipment integrated into the biomechanical analysis process includes instrumented starting blocks, turning plates, high-speed video cameras and timing devices.

Kistler's Solution

The Kistler Performance Analysis System for Swimming delivers kinetic and kinematic information about starts, turns and relay changeovers. Drawing on over 50 years' experience of measuring infinitesimal differences in movements, Kistler has developed products that fully meet the requirements of modern performance analysis in sport. The instrumented starting block measures the forces that act as the swimmer starts off; then, cameras focus on his or her individual movements in the underwater phases. Finally, analytical software displays the video with biomechanical analysis − in a clear format that's easy to understand.

Achieving success with Kistler

Kistler’s Performance Analysis System for Swimming offers two key advantages: it can deliver immediate feedback, and it can compare two different trials on one screen. This detailed information gives coaches and athletes the basis to adapt performance directly and make minor changes in the next trial. The results: progress towards the goal, and increased benefit from training sessions. So: take the lead – right from the start!

Please find more information about the advantages of our Performance Analysis System for Swimming.

Our highly qualified employees push the limits of what is possible and deliver answers with our customers – and for our customers – to the great questions posed by a connected world around the megatrends mobility, emission reduction, quality control and lightweight construction.

Do you want to play a part in shaping the future? If so, become part of our team. 

11.04.2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks...
14.11.2017
在冷却润滑液产品研发过程中,巴索润滑液公司依靠了奇石乐的专业测量系统。
29.08.2017
Applus IDIADA依赖于奇石乐的内置假人测量技术。
17.01.2017
三分量测量系统推进冷却润滑液产品的研发。
04.01.2017
奇石乐能够检测到车辆碰撞试验中最喜欢的变化,帮助提高事故生存率
22.12.2016
奇石乐优化车辆综合测试
20.12.2016
奇石乐传感器在任何条件下都能最大程度的保证数据的准确度
07.11.2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
28.10.2016
漫步在训练场(已有三年历史)内,立即被一个长长的混凝土建筑所吸引。与办公室和更衣室相同的是,该建筑物有现代化的训练区域,该区域自2015年底以来使用了奇石乐的测力台。该技术产生的测量结果让培训主管深入了解他们球员的身体状...
17.08.2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19.02.2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
15.06.2015
Measurement Solutions for Automotive Test Systems
08.05.2015
Quality Assurance in the Automotive Industry
02.03.2015
博泽如何提高双组份制品品质和自动分离缺陷制品
02.12.2014
奇石乐集团追求的是进取和可持续增长的策略– 战略收购是该策略的核心要素之一。这意味着,奇石乐考虑和选择一些企业合作,可以实现更高的目标。2006 年对 Dr. Staiger Mohilo& Co. GmbH...
02.12.2014
在太阳系飞行了十年之后,Rosetta 航天器于 2014 年 11 月 12 日将探测器 Philae 发射到“Chury”彗星上。为了避免探测器在 40...
23.08.2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15.02.2011
End-to-end process monitoring for critical medical moldings
07.02.2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany