Kistler enables digital measuring chains for advanced vehicle test stands

Faced with the challenge of modernizing its kinematics and compliance test machine for automotive engineering, AB Dynamics implemented the new digital charge amplifier 5074A from Kistler. It enables a fully digital measuring chain including a set of load cells to measure tire forces and moments in real time, no matter how complex the requirements might be.

Today's cars are high-powered technology hubs, packed with mechatronic components that deliver ever-increasing levels of driver assistance; they can even perform some maneuvers autonomously. However, impressive features and functions such as these need to be supported by comprehensive testing with specialized equipment, backed by specific know-how. One leading provider of these resources is Anthony Best Dynamics Limited, a British company based in the picturesque town of Bradford on Avon in south-western England. It is a member of the international AB Dynamics Group, which offers a portfolio of solutions for measurement and analysis systems, simulation, and proving ground automation.

“We went through a period of rapid growth in recent years, so our new headquarters here in Bradford on Avon has already become too small,” says Joanna Maddams, Marketing Manager at AB Dynamics. “That's why we're currently adding another new building opposite our head office. Our worldwide headcount has increased from about 70 back in 2015 to more than 200 today. We also have a network of offices in Europe, Japan and the USA that handle the distribution of our validation and durability solutions to many automotive OEMs, suppliers and vehicle test centers across the globe.”

Seamless integration into a state-of-the-art machine design

Matthew Dustan, Product Manager for Laboratory Test Systems at AB Dynamics, singles out some current trends in automotive testing: “Progress in testing Advanced Driver Assistance Systems (ADAS) has triggered higher demand for complex track test solutions and is generating some exciting opportunities for proving ground automation. There is also a move towards simulation in vehicle development and modeling ‒ this is particularly apparent with new electric vehicle manufacturers.”

Many vehicle developers throughout the world operate one of AB Dynamics' leading solutions: the Suspension Parameter Measuring Machine (SPMM), a complex test stand that can simulate a car's behavior by applying combined roll, pitch, bounce, and yaw motions on a moving platform. Under each of the four wheel stations, a multicomponent force link set of piezoelectric load cells ensures accurate measurement of all forces and moments: the 9366CC series from Kistler is a customizable kit with four sensing elements that deliver maximum accuracy thanks to their high rigidity and natural frequency. “Load cells from Kistler have always played a key part in the success of this product, and they are highly integrated into the overall system. They deliver zero values at high resolution when the vehicle is mounted on the test stand, and they also provide very precise measurements of all the specific high-load forces applied during kinematics and compliance testing. And by no means least, they help to prevent overloading and potential damage,” Dustan explains.

Faced with the growing complexity of automotive testing, the engineers at AB Dynamics wanted to digitize the entire SPMM system to provide higher bandwidth for advanced testing requirements in the future. “Our goal was to create an updated SPMM with a fully digital measuring chain and a closed-loop force control system,” Dustan continues.

It took us about two years to complete this development project, and the digital charge amplifier from Kistler was crucial to its success.”

Matthew Dustan, Product Manager Laboratory Test Systems at AB Dynamics

 

In the new SPMM 5000e, the signals from every wheel station are digitized by two 5074A digital charge amplifiers (each with four channels); they form part of a distributed EtherCAT topology that delivers live force readings at high frequencies.

“We're currently running a 2 kHz cycle on our machine, but the Kistler amplifier is capable of doing even more ‒ the bottleneck is elsewhere,” Dustan explains. “We plan to go to 4 kHz in the near future. We've also reduced the size of the electrical cabinet by about 40 percent; the machine now requires much less cabling and wiring, and far less installation effort. It comes with advantages such as high bandwidth, low latency and resilience to drift even in humid environments ‒ to mention only a few.” AB Dynamics has already delivered its new state-of-the-art solution to several customers in Europe and Asia.

Real-time force and moment measurements: precise, robust and high-resolution

One outstanding advantage of the 5074A digital amplifier from Kistler is its switchable measuring range. This allows precise measurements covering almost five decades of amplitude, providing greater flexibility for many applications. It is also a practical instrument for optimizing the measuring chain: “The measurement range setting can be used to individually adapt the optimal load capability and resolution. Using the 16-bit signals, we can start out by estimating the load and then make adjustments based on the first measurement data,” Dustan explains. This process results in high data quality ‒ a critical factor for AB Dynamics' customers, who use the data to inform their design decisions throughout the entire vehicle development process.

Dustan sums up the collaboration between the two companies: “We couldn't have completed the new machine without the digital charge amplifier from Kistler. It allowed us to run a closed-loop force control at high frequencies and also ‒ thanks to the amplifier's form factor ‒ we were able to package the complete measuring chain locally into sections of the machine. What's more, Kistler customized the load cells to ensure smooth integration into the new setup. In short, they provided exactly what you'd expect from a market leader: innovative products and custom solutions.”

Innovative, customized solutions that push the limits of automotive testing

How will the automotive testing market evolve over the next decade? According to Matthew Dustan: “Vehicles are generally becoming more complex and computerized ‒ and for testing, that presents challenges as well as opportunities. We're seeing a strong push towards simulation and electrification to improve vehicle behavior and ADAS support. Simulation, in particular, is data-driven ‒ so good measuring equipment is more critical than ever before as a factor in generating added-value data sets. After 25 years of working with Kistler solutions, we're now developing a new type of test stand for axle suspension NVH analysis that will also include accelerometers specifically designed by Kistler to accomplish these measurement tasks.”

05.10.2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18.09.2020
令人信服的测试结果:俄亥俄州运输部将进一步增加奇石乐Kistler Lineas传感器的使用,进行交通监测。
20.08.2020
精度是高性能的关键:了解奇石乐测量技术如何助力埃莫克法兰肯(EMUGE FRANKEN)公司研发团队。
22.07.2020
奇石乐ComoNeo满足上海天泽精密模具精密生产要求。
09.06.2020
奇石乐助力森拉天时(Ceratizit)开发高动态车削(HDT)系统,用户仅需一把刀具,即可完成复杂几何结构的加工。
15.11.2019
奇石乐过程监控系统及模腔压力传感器帮助大幅降低注塑成型零件故障率。
23.10.2019
奇石乐测量技术如何助力提升顶级电动工具质量
15.08.2019
奇石乐分析系统如何提高紧固技术的安全性和透明度。
17.07.2019
土耳其选择搭载有奇石乐动态称重系统(WIM)的车辆超载执法管理
24.06.2019
载人飞船再次登月,奇石乐以可靠的测量结果保障月球之旅
20.06.2019
瞬间自动分离良品和次品,每个周期只有短短1.5秒:奇石乐过程监控系统保证年产量达500万件产品的高质量
14.05.2019
为确保零部件和医疗部件的卓越品质,Tessy公司选择了奇石乐传感器和解决方案。
18.04.2019
德国某知名小家电制造商对奇石乐集团旗下公司Vester的自动测试和分拣系统非常信赖。
02.04.2019
奇石乐MARS测力台系统,美国国家橄榄球联盟(NFL)职业橄榄球队——杰克逊维尔美洲虎队(Jacksonville Jaguars)训练智能化的秘密武器
25.03.2019
Schurter AG采用奇石乐过程监控系统maXYmos,以满足汽车制造业对质量控制和可追溯性的严格要求。
18.03.2019
如何高效判断运动员体能状态?奇石乐Quattro Jump运动表现分析系统报告为您提供有效支持。
17.12.2018
奇石乐精准的动态称重(WIM)技术,可持续的保护匈牙利国内道路免受超载车辆损坏。
27.11.2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10.10.2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08.10.2018
多特蒙德工业大学(TU)机械加工技术研究所(ISF)测试奇石乐新型MicroDyn 9109AA型切削力测力仪,为该研究所在开发微加工工艺方面打开全新的局面,
31.08.2018
采埃孚公司启用带有集成化振动装置的奇石乐软件控制式紧固件测试台。
14.08.2018
大昭和精机株式会 (BIG Daishowa), 总部位于日本大阪,是机械 加工业刀柄的主要生产商之一。公司每年生产50多万个弹簧夹头。 其产品是采用奇石乐(Kistler)的切削力测量设备以及其他资源研发 而成。
16.07.2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11.04.2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14.11.2017
在冷却润滑液产品研发过程中,巴索润滑液公司依靠了奇石乐的专业测量系统。
29.08.2017
Applus IDIADA依赖于奇石乐的内置假人测量技术。
04.01.2017
奇石乐能够检测到车辆碰撞试验中最喜欢的变化,帮助提高事故生存率
22.12.2016
奇石乐优化车辆综合测试
20.12.2016
奇石乐传感器在任何条件下都能最大程度的保证数据的准确度
07.11.2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
28.10.2016
漫步在训练场(已有三年历史)内,立即被一个长长的混凝土建筑所吸引。与办公室和更衣室相同的是,该建筑物有现代化的训练区域,该区域自2015年底以来使用了奇石乐的测力台。该技术产生的测量结果让培训主管深入了解他们球员的身体状况。
17.08.2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19.02.2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04.11.2015
Piezoelectric Measurements with CompactRIO™
15.06.2015
Measurement Solutions for Automotive Test Systems
08.05.2015
Quality Assurance in the Automotive Industry
02.03.2015
博泽如何提高双组份制品品质和自动分离缺陷制品
02.12.2014
奇石乐集团追求的是进取和可持续增长的策略– 战略收购是该策略的核心要素之一。这意味着,奇石乐考虑和选择一些企业合作,可以实现更高的目标。2006 年对 Dr. Staiger Mohilo& Co. GmbH 公司的收购就是这种价值观的体现。通过这次收购, 奇石乐和被收购公司得到了共同发展,达到了双赢的目的。
02.12.2014
在太阳系飞行了十年之后,Rosetta 航天器于 2014 年 11 月 12 日将探测器 Philae 发射到“Chury”彗星上。为了避免探测器在 40 亿英里的太空航行中耗尽燃料,使用了奇石乐集团的压力传感器对燃料消耗量进行全程监测。
23.08.2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15.02.2011
End-to-end process monitoring for critical medical moldings
联系方式
(max 25 Mb)