How Polyfab trims its injection molding production to the highest quality

Polyfab uses process monitoring systems from Kistler based on cavity pressure measurement to sustainably optimize the high-volume production of plastic parts for various industries. Thanks to them, it was possible to reduce the number of faulty parts in injection molding to a record-breaking 1 PPM (parts per million).

Since 1971, Polyfab Corp. has been a custom thermoplastic injection molder. The American company supports the plastics molding industry needs of four major markets: medical, packaging, industrial, and commercial. In order to remain competitive in the ever-changing plastic molding industry, they must continuously adapt their monitoring processes with the ultimate goal of producing zero-defect quality assured parts.

Brian Burhop is a Project Engineer with over 16 years of experience at Polyfab Corp. located in Sheboygan, Wisconsin. He takes the quality of their molded parts seriously. Monitoring the molding process for suspect parts prior to packaging or assembly easily with guaranteed results is key. For nine years now, cavity pressure technology with sensors and systems of Kistler have provided a highly effective, reliable basis for automated inspection.

Integrated quality assurance increases customer satisfaction

Burhop says, “Our partnership with Kistler came about because Polyfab Corp. is very much a molder based on scientific principles which we employ to establish and monitor our molding processes. Process monitoring and containment is very important for our high-volume jobs. Our decision was based on very important factors, such as how user-friendly the monitoring equipment is, how easy it is to acquire and interpret the data, how easily configurable it is with our machinery, and how easy it is to incorporate Kistler's sensors into the mold itself. Kistler's products were really hands down the best choice for us in all those categories. Approximately 66% of Polyfab Corp. machinery is now equipped with Kistler monitoring and sensor technology.”

The first challenge Burhop and his team faced was to greatly improve the accuracy of short-shot monitoring for a dispenser lid with a living hinge. To reduce non-fills during the injection molding process, the pressure at end of fill was monitored with a flush mounted sensor directly in the cavity. This allows for more accurate setting of the required minimum pressure which is affected by process variables including injection speed, and melt temperature.

The installation of Kistler’s monitoring systems with our molding machines couldn’t be any easier. We can pick up just one signal and that’s really all we need because it is so streamlined, and we are able to start collecting data quickly."

Brian Burhop, Project Engineer at Polyfab Corp. in Sheboygan, Wisconsin

 

Burhop states, “Polyfab's customer return score prior to implementing Kistler in 2009 was above 10,000 PPM (parts per million). In 2017, we molded approximately 200 million parts and our rate for customer returns was 98 PPM, which is `world class' performance. Our 2018 year-to-date PPM customer return rate is now `1 PPM'. This represents a drastic improvement after implementing Kistler's process monitoring systems (ComoNeo/ CoMo Injection), as well as Kistler's direct and indirect cavity pressure sensors into our machinery.”

Automated assembly thanks to cavity pressure sensors

Polyfab Corp. has also integrated Kistler's sensors into their automated assembly process, producing very positive results. Burhop explains, “For automated assembly in terms of parts which have a lot of value added as they step through the assembly process, Kistler's sensors ensure that we are not assembling parts with suspect (defective) plastic components. For example, we have a commercial inkjet cartridge that we have completely automated the assembly.

The cell incorporates two molding machines, six robots, and two 4-cavity molds. We have placed a Kistler sensor in each one of those cavities so if there is a suspect or questionable shot, it segregates it so that those parts don't enter the assembly process. This has proven very beneficial and valuable to our automated assembly application needs.”

Process monitoring systems of Kistler save valuable time, reduce costs, and increase ROI

Kistler's process monitoring systems have been saving time, reducing costs, and increasing the Return on Investment (ROI). Burhop says, “From my perspective: reducing re-validations was key. For instance, if we need to validate a tool in another press, either for capacity reasons or for risk mitigation for a customer, Kistler's technology has made the process of duplicating a process much more straightforward and scientific in terms of the acquisition of data and the actual pressure curve data from the cavity.”

Bob Hendricks, Product Sales Manager with Kistler, who worked closely with Burhop, further explains this time-saving benefit of incorporating Kistler's process monitoring systems and sensors: “When you have a reference curve that represents the part quality, and you need to move it from one machine to another, the benefit is you no longer have to revalidate the whole process every time because that reference curve remains valid on any machine.”

Shorter set-up times ensure optimized production

According to Burhop, the set-up was quick and easy to learn and use. Kistler's contact elements for injection molds have also proven to be highly beneficial. Burhop says, “The use of Kistler's contact elements have greatly simplified our mold disassembly and maintenance process. At Polyfab Corp., we focus on lean production, set-up reduction and quick-change. By utilizing Kistler's multi-channel connectors, it's just one quick connection.” This allows Burhop and his team to save a lot of time and reduce costs by greatly decreasing the molding defect rate.

“Kistler's piezoelectric sensor technology, in my opinion, is much more straightforward and easier to use than a lot of the other sensors currently on the market. The installation of Kistler's monitoring systems with our molding machines couldn't be any easier. We can pick up just one signal and that's really all we need because it is so streamlined, and we are able to start collecting data quickly,” Burhop adds.

Customer satisfaction is key at Kistler

Hendricks is also enthusiastic about the long, successful cooperation and emphasizes: “At Kistler, we are focused on fulfilling our customer's needs with the goal of ensuring that they are completely satisfied. Our aim is to help our customers achieve zero-defect in series production, offering specialized, expert advice and onsite technical support including calibration services no matter where you are in the world.”

“We are very satisfied with Kistler's services and support,” Burhop elates. “If an issue does arise, which is not often, Kistler's support team responds very quickly and their services are fantastic. With regard to the implementation and installation of Kistler's piezoelectric sensors, our tool shops have had no issues installing the sensors in the molds. The implementation is very streamlined and almost transparent.”

15.11.2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23.10.2019
奇石乐测量技术如何助力提升顶级电动工具质量
15.08.2019
奇石乐分析系统如何提高紧固技术的安全性和透明度。
17.07.2019
土耳其选择搭载有奇石乐动态称重系统(WIM)的车辆超载执法管理
24.06.2019
载人飞船再次登月,奇石乐以可靠的测量结果保障月球之旅
20.06.2019
瞬间自动分离良品和次品,每个周期只有短短1.5秒:奇石乐过程监控系统保证年产量达500万件产品的高质量
14.05.2019
为确保零部件和医疗部件的卓越品质,Tessy公司选择了奇石乐传感器和解决方案。
18.04.2019
德国某知名小家电制造商对奇石乐集团旗下公司Vester的自动测试和分拣系统非常信赖。
02.04.2019
奇石乐MARS测力台系统,美国国家橄榄球联盟(NFL)职业橄榄球队——杰克逊维尔美洲虎队(Jacksonville Jaguars)训练智能化的秘密武器
25.03.2019
Schurter AG采用奇石乐过程监控系统maXYmos,以满足汽车制造业对质量控制和可追溯性的严格要求。
18.03.2019
如何高效判断运动员体能状态?奇石乐Quattro Jump运动表现分析系统报告为您提供有效支持。
17.12.2018
奇石乐精准的动态称重(WIM)技术,可持续的保护匈牙利国内道路免受超载车辆损坏。
27.11.2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10.10.2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08.10.2018
多特蒙德工业大学(TU)机械加工技术研究所(ISF)测试奇石乐新型MicroDyn 9109AA型切削力测力仪,为该研究所在开发微加工工艺方面打开全新的局面,
31.08.2018
采埃孚公司启用带有集成化振动装置的奇石乐软件控制式紧固件测试台。
14.08.2018
大昭和精机株式会 (BIG Daishowa), 总部位于日本大阪,是机械 加工业刀柄的主要生产商之一。公司每年生产50多万个弹簧夹头。 其产品是采用奇石乐(Kistler)的切削力测量设备以及其他资源研发 而成。
16.07.2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11.04.2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14.11.2017
在冷却润滑液产品研发过程中,巴索润滑液公司依靠了奇石乐的专业测量系统。
29.08.2017
Applus IDIADA依赖于奇石乐的内置假人测量技术。
04.01.2017
奇石乐能够检测到车辆碰撞试验中最喜欢的变化,帮助提高事故生存率
22.12.2016
奇石乐优化车辆综合测试
20.12.2016
奇石乐传感器在任何条件下都能最大程度的保证数据的准确度
07.11.2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
28.10.2016
漫步在训练场(已有三年历史)内,立即被一个长长的混凝土建筑所吸引。与办公室和更衣室相同的是,该建筑物有现代化的训练区域,该区域自2015年底以来使用了奇石乐的测力台。该技术产生的测量结果让培训主管深入了解他们球员的身体状况。
17.08.2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19.02.2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04.11.2015
Piezoelectric Measurements with CompactRIO™
15.06.2015
Measurement Solutions for Automotive Test Systems
08.05.2015
Quality Assurance in the Automotive Industry
02.03.2015
博泽如何提高双组份制品品质和自动分离缺陷制品
02.12.2014
奇石乐集团追求的是进取和可持续增长的策略– 战略收购是该策略的核心要素之一。这意味着,奇石乐考虑和选择一些企业合作,可以实现更高的目标。2006 年对 Dr. Staiger Mohilo& Co. GmbH 公司的收购就是这种价值观的体现。通过这次收购, 奇石乐和被收购公司得到了共同发展,达到了双赢的目的。
02.12.2014
在太阳系飞行了十年之后,Rosetta 航天器于 2014 年 11 月 12 日将探测器 Philae 发射到“Chury”彗星上。为了避免探测器在 40 亿英里的太空航行中耗尽燃料,使用了奇石乐集团的压力传感器对燃料消耗量进行全程监测。
23.08.2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15.02.2011
End-to-end process monitoring for critical medical moldings
联系方式
(max 25 Mb)