2019年夏,位于奥地利罗伊特的森拉天时公司(Ceratizit Austria GmbH)创新中心开展了多项测试,其首要目标是获得HDT系统的最高性能。为此,测试人员选择不同进给量和切削深度开展测试。随后,测试人员还逐渐增加FreeTurn刀具接近角的陡度。奇石乐测力计为测试过程中产生的各种力提供了详细而可靠的测量值。测试人员将这些数据与使用PCLNL 2525 M12型传统车刀的测试结果进行比较,并做出进一步分析。
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.