Fakuma News: New Cavity Pressure Sensor for RTM Makes Composite Production More Transparent

At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012) Kistler will present its new cavity pressure sensor for the production of advanced lightweight construction components at booth 3104 in hall A3. The production of these composite components is a special challenge for process monitoring and quality assurance systems. With its new sensor for Resin Transfer Molding (RTM), Kistler provides the key to process optimization and monitoring during processing of crosslinking molding compounds for lightweight plastic constructions for automotive and aerospace engineering.

 

Sensor Type 6161AA… measures cavity pressure levels of up to 200 bar. It is suitable for industrial application, particularly for monitoring, open and closed-loop control of RTM processes, high pressure RTM (HP-RTM) and SMC processes (Sheet Molding Compound) with pressure levels of up to 150 bar. The sensor offers a range of function such as the detection of filling errors or controlling cascade filling via several gates. In addition to pressure measuring, the sensor can also be used for measuring the vacuum of the evacuated cavity. In short, the sensor is able to record all relevant process data.

Kistler at Fakuma 2012: Hall A3, Booth 3104