The NCFR Joining Module from Kistler

Stuttgart, 5 October 2015 – At the Motek 2015, Kistler will present its new NCFR Joining Module: as well as the classical linear joining process, this system can now perform a rotary movement of the ram, either sequentially or even simultaneously. These movements are monitored and controlled by integrated sensors on the NC joining module.

Kistler's electromechanical NC joining systems are coordinated systems with integrated force sensors and high-performance force-displacement evaluation. They provide end-to-end process monitoring and documentation for all measurements and process values. The measurement range covered
is wide – from 50 N to 600 kN – and the scope for potential applications is enormous. The launch of the new NCFR Joining Module marks the completion of Kistler's family of joining modules: with this innovative new module, joining processes can now be performed in combination with rotary movements.

Dynamic Drive Technology and High-Precision Sensors
The new NCFR Joining Module reflects the state of the art in joining process technology: with its integrated hollow-shaft servo motors, the module features compact dimensions and extremely low weight. This design offers excellent dynamic characteristics, creating the basis for dramatically reduced
cycle times. Integrated sensors continuously capture and evaluate force and displacement − as well as rotation angle and torque − with maximum precision, so 100% quality and control are ensured. The piezoelectric force sensor has two predefined measuring ranges to deliver high resolution; it also offers high overload capacity, especially in the small measuring range.

The joining process is monitored by maXYmos NC: activated via fieldbus, this monitoring system evaluates and documents XY profiles for joining and press-fit processes, together with the NCFR Joining Module and the IndraDrive servo amplifier that is included in the system. The patterns of measurement curves can be used to monitor and control the quality of a single production step, a sub-assembly or an entire product. The benefits: optimal cycle times can be achieved with maximum repeat accuracy, downtime is minimized and machine availability is increased – adding up to a remarkable boost in productivity for the manufacturing process.

NC joining systems with NCFR are fully tested systems that greatly simplify installation and handling: sequence programming is child's play, with parameterization on the PC or the touch panel. Even complex joining processes are simple to display thanks to sequencer mode. Depending on
requirements, practical sequence elements (e.g. various motions) can be used for the movements. The result: both linear and rotary movements can be programmed and controlled via events – flexibly, rapidly and easily, without intermediate stops.

One Module – Multiple Benefits
Like the entire family of NC joining modules, the NCFR Joining Module delivers a host of additional benefits for its users: thanks to the servo amplifiers used in the module, for instance, all traverse movements performed in assembly and product testing can be controlled with high precision. Another example: completely different components can be manufactured on one and the same machine, because all NC joining systems allow measuring ranges to be changed over, with easy switching between measuring programs.

And there are even more advantages: the system offers substantially higher efficiency than pneumatic or hydraulic processes. The savings potential of the electrical process is up to 77 % when compared to hydraulic systems and up to 90 % when compared with pneumatic process. Maintenance outlay for these systems is low – so users can save even more on their already low production
costs. Last but not least, the consistently simple operating philosophy of the maXYmos family makes setup fast and comfortable, and adjustments after commissioning are easy to perform.

Focusing on Cost-Efficient Operation
Alexander Müller, Product Manager for NC Joining Systems at Kistler, is utterly convinced by this innovative new development: "Maximum flexibility and excellent dynamics combined with simple operation mean that complex joining processes are mapped quickly and efficiently. Capacity utilization rates for plant are increased, and the commissioning and set-up phase is reduced to the minimum. And with its low energy consumption, the new NCFR Joining Module will help the automobile industry and the automotive supply sector to cut energy costs in series production. There's enormous market demand for both factors. Together, they create the basis for sustainable optimization
of resources, paving the way for cost-efficient operation in the long term."

Download Press Release PDF

Media Contact
Simone Koch
Divisional Marketing Manager IPC
Phone +41 52 2241 802
Email: simone.koch@kistler.com

User Contact
Alexander Müller
Product Manager, NC Joining Systems
Phone +49 7172 184 176
Email: alexander.mueller@kistler.com

媒体宣传资料

奇石乐公司简介及标志:Kistler Press Kit.zip

12.10.2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
09.10.2017
Kistler's Type 5074A industrial charge amplifier breaks new ground in industrial charge amplifier technology
06.10.2017
Whether hybrid drives or electric vehicles: anyone who wants to make a change needs to measure and understand
27.09.2017
Our experts will present you Kistler measuring technologies for demanding space applications.
05.09.2017
At Fakuma 2017, we will demonstrate how you can benefit from new ComoNeo functionalities
31.08.2017
Kistler Group showcases the entire spectrum of its integrated quality assurance solutions
28.08.2017
可用于要求严苛的车辆测试的测量装备
28.08.2017
2017 AHTE 上展示全新的NCFR 压装模块,以及新一代 maXYmos 监测系统
11.08.2017
Jaguar Land Rover uses Kistler RoaDyn® Wheel Force Transducers for accurate tyre modelling
11.07.2017
奇石乐集团并购位于亚琛的MES(制造执行系统)软件和硬件系统供应商IOS GmbH
06.07.2017
奇石乐集团于 7 月 5 日成功收购位于德国泰特南的 eso GmbH(德国)
20.06.2017
MES 系统集成助您实现生产数据完美同步
25.04.2017
第二届国际模塑博览会将于 2017 年 5 月 30 日至 6 月 2 日在斯图加特举行。在本次展会上,奇石乐集团将展示确保注塑模具质量所需测量技术的安装的便捷性。
12.04.2017
奇石乐将在世界著名的国际质量控制及仪器仪表展览会上展示
12.04.2017
Advanced features for LabAmp family maximize flexibility for cutting force users.
11.04.2017
满足复杂精细测试测量需求的奇石乐产品
01.02.2017
奇石乐集团持续增长,并在全球范围内招聘专业人才。
12.12.2016
奥运冠军安东尼.埃尔文和奇石乐仪器创造成功故事
02.12.2016
Kistler seeks more than 40 specialists in what is likely Switzerland's largest job advertisement.
29.11.2016
德国纽伦堡举办的SPS IPC Drives大会上,奇石乐首次展示了分析螺栓装配的实验室系统、扭矩工具的校准设备和测试系统,以及随机抽样测试的测量系统。
23.11.2016
奇石乐集团收购Schatz GmbH,从而为我们的客户提供更广泛的应用.
21.10.2016
奇石乐通过对燃烧过程的监测和控制提高了大型船机和发电机组的效率及可靠性。
19.10.2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
14.10.2016
所有的行业参与者与企业都必须在持续开发现有技术和扩大专业知识方面发挥积极的作用。这是协调全球互联经济发展需要与保持环境不受破坏的唯一方法。
12.07.2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12.05.2016
Screw technology complements the range of applications.
27.04.2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...
02.02.2016
奇石乐集团尽管受到汇率的不利影响仍获得持续增长。
26.11.2015
Increased Flexibility for High-Speed Combustion Analysis
02.11.2015
New Piezoresistive Sensor with Temperature Probe and Integrated Signal Conditioning.
27.10.2015
Kistler Provides Maximum Flexibility for Product Testing and Development
16.10.2015
Kistler's NCFR Joining Module honored in the handling and assembly category
05.10.2015
Setting the Standard for 100% Control of Linear Joining Processes with Partial Rotation
18.09.2015
Kistler Group: safeguarding the firm's competitive edge.
15.09.2015
Quick evaluation of performance and force with Kistler MARS 2.1.
03.09.2015
Major update for Kistler’s mobile engine indication system.
01.09.2015
Setting New Standards in Automated Process Monitoring for Injection Molding.
25.08.2015
Kistler Showcases Three Latest Product Innovations at Motek 2015
29.06.2015
Kistler Automotive GmbH honored as one of Germany's most innovative companies
26.06.2015
Kistler honored with ASCO Award Gold for best corporate transformation in Switzerland.
26.06.2015
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...