Quattro Jump with Unique Performance Diagnostics Software

Winterthur, 15 September 2015 – The portable force measurement system Kistler Quattro Jump now supports the proprietary performance diagnostics software Kistler MARS. The software, which has been specially developed for Quattro Jump, enables the analysis and evaluation of performance and force for vertical jumps. The eight pre-defined analysis modules make it possible to evaluate measurements in just a few seconds and to display all relevant performance parameters at a glance. Kistler has thus expanded the tried and tested force plate into an integrated, attractively priced performance diagnostics system, making broad application in fitness clubs, performance centers and rehabilitation centers possible. Kistler Quattro Jump with MARS is available as from now.

Quattro Jump with Kistler MARS 2.1
In June, Kistler presented an extensive update of the proprietary Kistler MARS 2.1 Measurement, Analysis and Reporting Software for Kistler force plates. The software is now also supported by Kistler Quattro Jump. The portable force measurement system provides numerous innovations for performance diagnostics in sport and rehabilitation, for example, in the evaluation of drop jumps. ‘Our goal is to make piezoelectric measurement technology, which is outstanding because of its great robustness and accuracy, available to a broad group of users,’ says Florian Ullrich, manager of Kistler’s Biomechanics Business Field. ‘With Kistler MARS, Quattro Jump is now an integrated, attractively priced performance diagnostic system which can be used in many situations where, up until now, high-end technology was prohibitive simply because of the cost.’ 

Versatile Application in Performance Sports and Rehabilitation
Quattro Jump with Kistler MARS is targeted for performance coaches, team physiotherapists as well as fitness and rehab trainers who need to objectively determine the exact condition of their athletes. The portable force measurement system delivers a quick overview of all the relevant performance parameters of the legs. This makes it possible, for instance, to specifically control particular training or regeneration phases so that individual development phases can be reached more quickly. With a USB interface, which replaces the serial interface used up until now, Quattro Jump can be connected more easily than ever.

Eight Predefined Analysis Modules
The focus of the eight predefined analysis modules (i.e. Counter Movement Jump or Stamping) is on the analysis of force and endurance. The software delivers all relevant performance parameters within just a few seconds. This helps athletes train to their optimal level and avoid injury. Frequent and efficient performance tests give coaches and physiotherapists a good overview of the current performance capability of their athletes.

Easy Output of Desired Performance Parameters
The input parameters and data acquisition setup can be edited for each test separately. Data from projects, test persons and measurements are edited, structured and saved to a database using the management tool. Here, they are available for comparisons and reports. Extensive information and examples can be found in the Kistler MARS software help while online video trainings are available from the support website.

Collaboration with Leading Institutions in Biomechanics
The Windows-based software Kistler MARS has been developed in close collaboration with leading international institutions for biomechanics and extensively tested in practice using Quattro Jump. Kistler MARS for Quattro Jump is also available as a software upgrade for older Kistler Quattro Jump systems with USB (Type 9290BD).

You can find out more about the Kistler performance measurement solutions at www.kistler.com/biomechanics.

Download Press Release PDF

The following pictures can be downloaded in high resolution here.

User Contact
Florian Ullrich
Head of Business Field Biomechanics
Phone +41 52 2241 520
Email: florian.ullrich(at)kistler.com

Press Contact
Tabea Zuberbühler
Media Coordination
Phone +41 52 224 12 74
Email: tabea.zuberbuehler(at)kistler.com

媒体宣传资料

奇石乐公司简介及标志:Kistler Press Kit.zip

12.10.2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
09.10.2017
Kistler's Type 5074A industrial charge amplifier breaks new ground in industrial charge amplifier technology
06.10.2017
Whether hybrid drives or electric vehicles: anyone who wants to make a change needs to measure and understand
27.09.2017
Our experts will present you Kistler measuring technologies for demanding space applications.
05.09.2017
At Fakuma 2017, we will demonstrate how you can benefit from new ComoNeo functionalities
31.08.2017
Kistler Group showcases the entire spectrum of its integrated quality assurance solutions
28.08.2017
可用于要求严苛的车辆测试的测量装备
28.08.2017
2017 AHTE 上展示全新的NCFR 压装模块,以及新一代 maXYmos 监测系统
11.08.2017
Jaguar Land Rover uses Kistler RoaDyn® Wheel Force Transducers for accurate tyre modelling
11.07.2017
奇石乐集团并购位于亚琛的MES(制造执行系统)软件和硬件系统供应商IOS GmbH
06.07.2017
奇石乐集团于 7 月 5 日成功收购位于德国泰特南的 eso GmbH(德国)
20.06.2017
MES 系统集成助您实现生产数据完美同步
25.04.2017
第二届国际模塑博览会将于 2017 年 5 月 30 日至 6 月 2 日在斯图加特举行。在本次展会上,奇石乐集团将展示确保注塑模具质量所需测量技术的安装的便捷性。
12.04.2017
奇石乐将在世界著名的国际质量控制及仪器仪表展览会上展示
12.04.2017
Advanced features for LabAmp family maximize flexibility for cutting force users.
11.04.2017
满足复杂精细测试测量需求的奇石乐产品
01.02.2017
奇石乐集团持续增长,并在全球范围内招聘专业人才。
12.12.2016
奥运冠军安东尼.埃尔文和奇石乐仪器创造成功故事
02.12.2016
Kistler seeks more than 40 specialists in what is likely Switzerland's largest job advertisement.
29.11.2016
德国纽伦堡举办的SPS IPC Drives大会上,奇石乐首次展示了分析螺栓装配的实验室系统、扭矩工具的校准设备和测试系统,以及随机抽样测试的测量系统。
23.11.2016
奇石乐集团收购Schatz GmbH,从而为我们的客户提供更广泛的应用.
21.10.2016
奇石乐通过对燃烧过程的监测和控制提高了大型船机和发电机组的效率及可靠性。
19.10.2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
14.10.2016
所有的行业参与者与企业都必须在持续开发现有技术和扩大专业知识方面发挥积极的作用。这是协调全球互联经济发展需要与保持环境不受破坏的唯一方法。
12.07.2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12.05.2016
Screw technology complements the range of applications.
27.04.2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...
02.02.2016
奇石乐集团尽管受到汇率的不利影响仍获得持续增长。
26.11.2015
Increased Flexibility for High-Speed Combustion Analysis
02.11.2015
New Piezoresistive Sensor with Temperature Probe and Integrated Signal Conditioning.
27.10.2015
Kistler Provides Maximum Flexibility for Product Testing and Development
16.10.2015
Kistler's NCFR Joining Module honored in the handling and assembly category
05.10.2015
Setting the Standard for 100% Control of Linear Joining Processes with Partial Rotation
18.09.2015
Kistler Group: safeguarding the firm's competitive edge.
15.09.2015
Quick evaluation of performance and force with Kistler MARS 2.1.
03.09.2015
Major update for Kistler’s mobile engine indication system.
01.09.2015
Setting New Standards in Automated Process Monitoring for Injection Molding.
25.08.2015
Kistler Showcases Three Latest Product Innovations at Motek 2015
29.06.2015
Kistler Automotive GmbH honored as one of Germany's most innovative companies
26.06.2015
Kistler honored with ASCO Award Gold for best corporate transformation in Switzerland.
26.06.2015
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...