Kistler Unveils the Latest Functionalities for Automated, Reproducible Injection Molding Processes and Their Control

Düsseldorf, 19 October 2016 – Kistler is presenting the new versions of its ComoNeo and ComoDataCenter – both with innovative options for applications in injection molding production that vastly simplify the control, reproducibility and documentation of processes in this segment of industry. First and foremost among the new features: the Restart Assistant, which allows efficient reproduction of established processes when changing machines.

With quality requirements constantly on the increase, continuous control of the entire injection molding production chain is absolutely essential. The focus here is on improving product quality and boosting cost-efficiency. Kistler has now developed the successor versions of ComoNeo and ComoDataCenter, two system components that already have excellent track records. These new versions offer the best possible basis for achieving these goals – and they are ideal for novices as well as experienced users.

Automated Process Reproduction: ComoNeo Now with Restart Assistant and OPC Interface

Kistler has now integrated a Restart Assistant into ComoNeo, making it possible for users to transfer established processes from one machine to another with no problems at all. To ensure identical quality reproduction in the new machine, this intelligent tool suggests which parameters need specific changes. For this purpose, the Assistant detects deviations in the cavity pressure and compensates for them by adapting the machine parameters. This automated analysis generates a suggestion so that users can correct the process on the basis of the cavity pressure – and no previous specialist knowledge is required.

As the era of Industry 4.0 dawns, this support places users in the best possible position to conquer the challenges posed by digital networking. For example: the system now supports the OPC-UA interface, which is on the way to becoming the standard for injection molding production. By integrating OPC-UA into ComoNeo, Kistler has now made it possible to fully implement Multiflow control (automatic hot runner balancing) as a standalone solution. In other words, users no longer need a PC for control. The benefit: significantly less effort is required for the entire setup process. Another new feature in ComoNeo: online quality forecasting is now integrated directly into the system, so the complete range of cavity pressure monitoring methods is available. The EO Assistant (for automated setting of monitoring limits), online quality forecasting and the Restart Assistant: three aids that ensure novices as well as experts will be guided to the desired results.

Control with Industry 4.0 in Mind: New Features for Real-Time Control and Hot Runner Balancing

The first version of ComoNeo already set a new standard for monitoring of injection molding production processes. This was achieved with the help of the EO Assistant: for the first time, users with no specific knowledge of cavity pressure were given a simple option for monitoring. Kistler has now developed software that goes one step further in quality optimization. The new version of ComoNeo provides feedback to the operator and the machine so that the process can be optimized even further. This advance allows perfect timing for the switchover from speed control to pressure control in response to cavity pressure. ComoNeo also offers a sampling rate that cannot be matched by any comparable system. The result: yet again, real-time control has been made vastly more responsive in every respect.

Automatic switchover control can be used in two different ways. The first option is for manual setup: control behavior is only changed after the user intervenes. The second option is called SLP (Switching Level Processor): in this case, setup is fully automated and the control behavior is optimized independently from cycle to cycle. The main advantage of the manual option is that several dependencies can be set; with SLP, the key benefit is self-optimizing calculation of the switchover point. In these ways, ComoNeo 2.0 also covers a wide range of process control applications: for molds with multiple cavities, behavior during automatic changeover has been optimized for the specific purpose of compensating for different behavior patterns during the production sequence. When conditions are set manually, additional dependencies across multiple cavities are available as control criteria. On the other hand, automated changeover is mainly used for molds with small numbers of cavities. The benefit here: ease of handling. All that is needed is to activate the process – and everything else is controlled by the internal algorithm, virtually at the touch of a button. Both switchover options actively help prevent mold damage because safety functions respond if filling differences are excessive.

Multiflow control is a method used to control hot runner balancing. Its fundamental purpose is to use appropriate temperature control of the individual hot runner nozzles to ensure that all filling curves have an identical progression, so production quality is guaranteed. In the past, conventional production methods always required a manual fill study, but Multiflow control by ComoNeo now makes it possible to fill the individual cavities automatically – with increased speed and far greater precision. This advantage can be exploited during setup and also during the actual production operation. Thanks to the readjustment option that is newly integrated in ComoNeo, process fluctuations can now be compensated during the production phase as well.

ComoDataCenter: the Vital Link for Networked Injection Molding Production

The ComoDataCenter (CDC) is also enhanced with attractive new features that make it easier to network data and improve the traceability of part quality. For instance, the CDC is now available for ComoNeo as well. Thanks to this innovation, ComoNeo and CoMo Injection are linked via a com-mon database. Another new feature: mold management is integrated into the CDC. The settings can be stored centrally, so the ComoNeo and CoMo Injection mold settings can be transferred to other plants via CDC. For existing customers, this also ensures compatibility between CoMo Injection and ComoNeo – guaranteeing that CoMo Injection users can change over gradually to ComoNeo. There is also provision for integration into higher-level systems such as SAP or other MES systems. This means that the CDC acts as the single interface between the process and higher-level MES systems. The benefit: all data can easily be networked with other systems across the company. And, last but not least, the CDC's user interface is now standardized with the tried-and-tested ComoNeo interface – entirely in keeping with the universal operating philosophy advocated by Kistler.
By enhancing ComoNeo and the ComoDataCenter with these new features, Kistler is paving the way for yet more future improvements to product quality and cost-efficiency in injection molding production.

Kistler will be showcasing the latest technologies that we have developed for quality control at K Trade Fair in Düsseldorf.

Download Press Release (PDF)

User Contact
Daniel Fick
Business Development Manager
Phone: +41 52 2241 606
Email: daniel.fick@kistler.com

Media Contact
Simone Koch
Divisional Marketing Manager IPC
Phone +41 52 2241 802
Email: simone.koch@kistler.com

媒体宣传资料

奇石乐公司简介及标志:Kistler Press Kit.zip

09.10.2017
Kistler's Type 5074A industrial charge amplifier breaks new ground in industrial charge amplifier technology
06.10.2017
Whether hybrid drives or electric vehicles: anyone who wants to make a change needs to measure and understand
27.09.2017
Our experts will present you Kistler measuring technologies for demanding space applications.
05.09.2017
At Fakuma 2017, we will demonstrate how you can benefit from new ComoNeo functionalities
31.08.2017
Kistler Group showcases the entire spectrum of its integrated quality assurance solutions
28.08.2017
可用于要求严苛的车辆测试的测量装备
28.08.2017
2017 AHTE 上展示全新的NCFR 压装模块,以及新一代 maXYmos 监测系统
11.08.2017
Jaguar Land Rover uses Kistler RoaDyn® Wheel Force Transducers for accurate tyre modelling
11.07.2017
奇石乐集团并购位于亚琛的MES(制造执行系统)软件和硬件系统供应商IOS GmbH
06.07.2017
奇石乐集团于 7 月 5 日成功收购位于德国泰特南的 eso GmbH(德国)
20.06.2017
MES 系统集成助您实现生产数据完美同步
25.04.2017
第二届国际模塑博览会将于 2017 年 5 月 30 日至 6 月 2 日在斯图加特举行。在本次展会上,奇石乐集团将展示确保注塑模具质量所需测量技术的安装的便捷性。
12.04.2017
奇石乐将在世界著名的国际质量控制及仪器仪表展览会上展示
12.04.2017
Advanced features for LabAmp family maximize flexibility for cutting force users.
11.04.2017
满足复杂精细测试测量需求的奇石乐产品
01.02.2017
奇石乐集团持续增长,并在全球范围内招聘专业人才。
12.12.2016
奥运冠军安东尼.埃尔文和奇石乐仪器创造成功故事
02.12.2016
Kistler seeks more than 40 specialists in what is likely Switzerland's largest job advertisement.
29.11.2016
德国纽伦堡举办的SPS IPC Drives大会上,奇石乐首次展示了分析螺栓装配的实验室系统、扭矩工具的校准设备和测试系统,以及随机抽样测试的测量系统。
23.11.2016
奇石乐集团收购Schatz GmbH,从而为我们的客户提供更广泛的应用.
21.10.2016
奇石乐通过对燃烧过程的监测和控制提高了大型船机和发电机组的效率及可靠性。
19.10.2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
14.10.2016
所有的行业参与者与企业都必须在持续开发现有技术和扩大专业知识方面发挥积极的作用。这是协调全球互联经济发展需要与保持环境不受破坏的唯一方法。
12.07.2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12.05.2016
Screw technology complements the range of applications.
27.04.2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...
02.02.2016
奇石乐集团尽管受到汇率的不利影响仍获得持续增长。
26.11.2015
Increased Flexibility for High-Speed Combustion Analysis
02.11.2015
New Piezoresistive Sensor with Temperature Probe and Integrated Signal Conditioning.
27.10.2015
Kistler Provides Maximum Flexibility for Product Testing and Development
16.10.2015
Kistler's NCFR Joining Module honored in the handling and assembly category
05.10.2015
Setting the Standard for 100% Control of Linear Joining Processes with Partial Rotation
18.09.2015
Kistler Group: safeguarding the firm's competitive edge.
15.09.2015
Quick evaluation of performance and force with Kistler MARS 2.1.
03.09.2015
Major update for Kistler’s mobile engine indication system.
01.09.2015
Setting New Standards in Automated Process Monitoring for Injection Molding.
25.08.2015
Kistler Showcases Three Latest Product Innovations at Motek 2015
29.06.2015
Kistler Automotive GmbH honored as one of Germany's most innovative companies
26.06.2015
Kistler honored with ASCO Award Gold for best corporate transformation in Switzerland.
26.06.2015
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...