Kistler showcases solutions for precise control and monitoring of production processes at The Assembly Show

Novi, MI, USA, 30 September 2014 – Kistler extends its maXYmos product family and presents the newly developed maXYmos NC for electromechanical joining modules at The Assembly Show 2014 in Rosemont, IL, USA. Visitors will also experience precise joining and testing demonstrations with the maXYmos BL, specifically designed for hand presses. Kistler’s full range of measurement systems facilitates end-users’ needs and acts as a single integrated source. This allows customers to operate a consistent systems approach for all applications in production – from the manual workstation to a fully controlled joining system.

 

Intelligent sequence control – Enhancing precision

With both manually operated and automatic pressing processes, product efficiency can only be assured in a zero-defect environment. The XY monitors from Kistler's maXYmos series enable customers to evaluate production processes, allowing them to operate with process-integration while enhancing consistency and maximizing quality assurance. Faulty parts are detected and removed early in the production process, thereby increasing product efficiency and avoiding unwanted downtime. Customers are able to conserve resources and increase quality assurance and product safety – saving substantial time and cost.

A further development to the maXYmos family, the maXYmos NC (numeric control) enables manufacturers to monitor and control joining processes through system integration. The maXYmos NC evaluates and documents the XY curve progressions of joining and press-fitting processes in connection with the NC joining modules and the associated servo amplifier IndraDrive. Due to the shape of the measurement curves, each stage of the production and assembly line – and even the entire product – can be monitored and controlled via SERCOS III in real-time. As a result, optimum cycle times can be achieved with the highest degree of repeat accuracy, thereby reducing downtimes and allowing for increased machine availability in order to optimize the overall production process. For actuation of NC joining modules, Kistler has also developed an integrated and user-friendly sequence control system for the maXYmos NC. Programs for pressfitting parts can be created via the intuitive user interface of the color touch screen, which is connected to the control system. The integrated sequence control, or 'Sequencer Mode', enables versatile mapping of even the most complex processes easily and effectively.

Visitors at the show have the opportunity to witness the intuitive operability and luminous display of the maXYmos systems. The uniform, operational interface in XY monitoring enables rapid integration into existing or newly planned systems. External measurement points – such as piezoelectric sensors for calibration or reference measurement – can also be connected at a later time thanks to the diversity of the interface. This ensures maximum flexibility, both during the installation process and for ongoing data analysis.

Quality assurance for hand-press operations

Kistler will also present an additional product from the maXYmos family at The Assembly Show in Rosemont – the maXYmos BL for hand presses. In non-automated operations, the maXYmos BL ensures that the processes are performed with reproducible quality using a sequence pre-programmed in the device – regardless of who is operating the system. Visitors at The Assembly Show will learn how the highly developed piezoelectric sensor and the intuitive monitoring enable rapid good/bad feedback and immediate correction or removal of faulty parts. With integrated or upgraded process control, zero-defect production of end-products is possible for each individual manufacturer, regardless of operating personnel.

NC joining systems for reduced power consumption

Kistler's NC joining systems support the automotive and automotive supplier industries by reducing power consumption within series production. This is achieved thanks to their higher level of efficiency when compared to pneumatic or hydraulic processes. The savings potential of the electrical process is up to 77 percent when compared with hydraulic systems, and up to 90 percent when compared with pneumatic process. Production costs decrease due to the low cost of system maintenance, which is less than an hour per system annually. The processes implemented with the NC joining systems in assembly and product inspection can be precisely controlled due to the integrated servo amplifier.

Additionally, due to the dual measuring range of select NC joining systems and the simple program switchover, different components can be produced on the same machine. The NC joining systems can be installed quickly, are pre-tested by Kistler prior to installation, thereby enabling maximum in-process quality assurance while guaranteeing reliable results.

Kistler will present its innovative products and customer service onsite at The Assembly Show in Rosemont, IL, USA from 28 – 30 October 2014 , Stand 1013.

 

Download Press Release (PDF/EN)

 

Media Contact


Simone Koch
Divisional Marketing Manager IPC
Phone +41 52 2241 802
E-Mail: simone.koch(at)kistler.com

 

 

Captions

Image 1: The maXYmos product family: flexible solutions for the highest requirements

Image 2: NC joining systems for riveting of lightweight brake disks

媒体宣传资料

奇石乐公司简介及标志:Kistler Press Kit.zip

12.10.2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
09.10.2017
Kistler's Type 5074A industrial charge amplifier breaks new ground in industrial charge amplifier technology
06.10.2017
Whether hybrid drives or electric vehicles: anyone who wants to make a change needs to measure and understand
27.09.2017
Our experts will present you Kistler measuring technologies for demanding space applications.
05.09.2017
At Fakuma 2017, we will demonstrate how you can benefit from new ComoNeo functionalities
31.08.2017
Kistler Group showcases the entire spectrum of its integrated quality assurance solutions
28.08.2017
可用于要求严苛的车辆测试的测量装备
28.08.2017
2017 AHTE 上展示全新的NCFR 压装模块,以及新一代 maXYmos 监测系统
11.08.2017
Jaguar Land Rover uses Kistler RoaDyn® Wheel Force Transducers for accurate tyre modelling
11.07.2017
奇石乐集团并购位于亚琛的MES(制造执行系统)软件和硬件系统供应商IOS GmbH
06.07.2017
奇石乐集团于 7 月 5 日成功收购位于德国泰特南的 eso GmbH(德国)
20.06.2017
MES 系统集成助您实现生产数据完美同步
25.04.2017
第二届国际模塑博览会将于 2017 年 5 月 30 日至 6 月 2 日在斯图加特举行。在本次展会上,奇石乐集团将展示确保注塑模具质量所需测量技术的安装的便捷性。
12.04.2017
奇石乐将在世界著名的国际质量控制及仪器仪表展览会上展示
12.04.2017
Advanced features for LabAmp family maximize flexibility for cutting force users.
11.04.2017
满足复杂精细测试测量需求的奇石乐产品
01.02.2017
奇石乐集团持续增长,并在全球范围内招聘专业人才。
12.12.2016
奥运冠军安东尼.埃尔文和奇石乐仪器创造成功故事
02.12.2016
Kistler seeks more than 40 specialists in what is likely Switzerland's largest job advertisement.
29.11.2016
德国纽伦堡举办的SPS IPC Drives大会上,奇石乐首次展示了分析螺栓装配的实验室系统、扭矩工具的校准设备和测试系统,以及随机抽样测试的测量系统。
23.11.2016
奇石乐集团收购Schatz GmbH,从而为我们的客户提供更广泛的应用.
21.10.2016
奇石乐通过对燃烧过程的监测和控制提高了大型船机和发电机组的效率及可靠性。
19.10.2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
14.10.2016
所有的行业参与者与企业都必须在持续开发现有技术和扩大专业知识方面发挥积极的作用。这是协调全球互联经济发展需要与保持环境不受破坏的唯一方法。
12.07.2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12.05.2016
Screw technology complements the range of applications.
27.04.2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...
02.02.2016
奇石乐集团尽管受到汇率的不利影响仍获得持续增长。
26.11.2015
Increased Flexibility for High-Speed Combustion Analysis
02.11.2015
New Piezoresistive Sensor with Temperature Probe and Integrated Signal Conditioning.
27.10.2015
Kistler Provides Maximum Flexibility for Product Testing and Development
16.10.2015
Kistler's NCFR Joining Module honored in the handling and assembly category
05.10.2015
Setting the Standard for 100% Control of Linear Joining Processes with Partial Rotation
18.09.2015
Kistler Group: safeguarding the firm's competitive edge.
15.09.2015
Quick evaluation of performance and force with Kistler MARS 2.1.
03.09.2015
Major update for Kistler’s mobile engine indication system.
01.09.2015
Setting New Standards in Automated Process Monitoring for Injection Molding.
25.08.2015
Kistler Showcases Three Latest Product Innovations at Motek 2015
29.06.2015
Kistler Automotive GmbH honored as one of Germany's most innovative companies
26.06.2015
Kistler honored with ASCO Award Gold for best corporate transformation in Switzerland.
26.06.2015
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...