Reyher reliably controls threaded joints thanks to an universal fastener test stand

REYHER aims to maintain its long tradition of professionalism in supplying and advising customers across many different industrial sectors – and to achieve its goal, this Hamburg-based company puts its trust in an ANALYSE system by Kistler. One particular benefit of the system: it can perform standard-compliant friction coefficient tests on fasteners of sizes up to M48, such as those often used in wind turbines.

If fasteners are what you need, you go to REYHER. For over 70 years, this company has supplied fasteners and fixing elements for threaded joints of all types from its base in Hamburg, North Germany. REYHER (or F. REYHER Nchfg. GmbH & Co. KG, to use the company's full name) operates as a wholesaler to supply over 11 000 customers across the globe from a range comprising 130 000 different articles.

Sound advice depends on analysis of friction coefficients

Frank Poggensee has been with REYHER for the last 14 years. As Head of Quality Technology, it is his responsibility to make sure that the characteristics of the company's fasteners are correct. "My personal background is in the automotive industry, which is traditionally the main driver of quality requirements. But wind power has also become an increasingly critical factor for REYHER in recent years," he explains. It is a fact that up to 11 tonnes of fasteners can be built into one single wind turbine plant. "This is an environment where exceptionally demanding requirements have to be met. Of course, safety is a critical priority in wind turbines – there's no telling what would happen if fasteners were to fail in one of these plants," Poggensee continues.

Since Poggensee joined REYHER, the Product and Quality Management (PQM) department has grown from eight people to a team of 40. This is partly because the threaded joints segment has become far more complex than ever before. "More and more surfaces and coatings are available, and the service component is also growing: that involves offering recommendations and advice, providing support for our own products, and training the customers. And then, of course, we shouldn't overlook the issues of traceability and transparency," Poggensee points out. "It's increasingly desirable and necessary for customers to know how each fastener is designed, which tools are used, and which standards have to be observed." Wind turbine installations, for example, make use of high-strength preloadable bolt fittings. For these components, the relevant quality requirements have to be met with the help of special material inspections, testing procedures and production processes – and end-to-end traceability of the production history is generally required as well.

REYHER's intention is to position itself appropriately in this segment so that it can reliably meet its customers' ever-increasing quality requirements. To achieve this objective, REYHER began operating an ANALYSE system from Kistler early in 2018. Friction coefficient tests can now be carried out far more efficiently in house – for fasteners up to class M48 such as threaded bolts, hexagon and hexagon socket bolts and screws, as well as high-strength preloadable (HV) fittings. "In the past, all we had was a mobile two-channel test system for fasteners up to M24. We were gradually reaching the limits in terms of capacity as well as quality," Poggensee recalls. 

Thanks to the ANALYSE system from Kistler, we have improved our ability to meet our customers' requirements, so we can guarantee a higher level of quality."

Frank Poggensee, Head of Quality Technology at REYHER

 

An investment that pays dividends

For example, REYHER can now carry out in-house testing of M48 bolts for the wind energy sector to ISO 16047, which was previously impossible. The result: important customers rely on REYHER to a very large extent. "In the past, these fasteners had to be sent out of house for testing. That involves using various service providers, to avoid being entirely dependent on just one. And this was how we first came into contact with Kistler," Poggensee remembers. "However, a cost-effectiveness analysis showed that an investment in our own Kistler ANALYSE system would be worthwhile to cope with the continuously increasing scope and growing requirements."

Olaf Schuhknecht, Sales Engineer with Kistler, gives this explanation of the structure and characteristics of the new solution: "Every ANALYSE system is a three-channel measuring instrument that precisely determines the tightening torque, thread torque and preloading force of a threaded joint. Each system is individually designed to meet the customer's requirements. For instance, we can align the test stand either horizontally or vertically, so either very small or very large fasteners can be tested. This approach creates a customized solution precisely tailored to the specific requirements." Performance scope is expanded with add-on modules such as ultrasonic measurement or vibration units to allow even more accurate analyses as well as simulations of real loads.

Higher quality despite greater complexity

The Kistler ANALYSE system used at REYHER offers maximum torque of 8 000 Nm. Screws, bolts and nuts from M5 to M48 can be tested thanks to the extensive range of sensors deployed for torque/rotation angle, preloading force and thread torque. "Our torque/rotation angle sensors measure directly on the test object, so they are not subject to any falsification due to drive shaft torsion," Schuhknecht adds. 

How satisfied is REYHER with the test stand? Poggensee has no doubts: "This system fully meets our expectations in every respect, and it helps us to reliably fulfill our customers' quality requirements  - which are increasing all the time." He continues: "We looked at several offers, but many factors persuaded us to opt for Kistler: they provided the range of sizes we needed up to M48, and their reputation with suppliers is good (as we know from the audits we regularly conduct for our customers). Our existing business relationship and the availability of service were also key advantages."

11.04.2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14.01.2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18.11.2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12.10.2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14.09.2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09.09.2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03.09.2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02.07.2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22.06.2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02.06.2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26.04.2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13.04.2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22.03.2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08.02.2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05.10.2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18.09.2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20.08.2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22.07.2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09.06.2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15.11.2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23.10.2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15.08.2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17.07.2019
Turkey opts for weight enforcement with WIM technology from Kistler
24.06.2019
For the next manned flight to the moon: safety that can be measured
20.06.2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14.05.2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18.04.2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02.04.2019
NFL's Jaguars boost their fitness levels with Kistler.
25.03.2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18.03.2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17.12.2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27.11.2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10.10.2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08.10.2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31.08.2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14.08.2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16.07.2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11.04.2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14.11.2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11.08.2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04.01.2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22.12.2016
Kistler makes progress in vehicle development possible
22.12.2016
Kistler Sensor Correvit® SFII measures world record
20.12.2016
Kistler sensors deliver a maximum in data quality under any conditions.
07.11.2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05.10.2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17.08.2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19.02.2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04.11.2015
Piezoelectric Measurements with CompactRIO™
15.06.2015
Measurement Solutions for Automotive Test Systems
08.05.2015
Quality Assurance in the Automotive Industry
02.03.2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02.12.2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02.12.2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23.08.2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15.02.2011
End-to-end process monitoring for critical medical moldings
07.02.2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Контакты
Max 25 MB