Process automation for industrial production and testing with Smart Single Stations

Turnkey solutions from Kistler for assembly and testing processes: integrated measurement technology know-how for industrial production, tailored to each user's individual requirements. These manufacturing or testing cells are designed exactly in line with customers' specifications. Depending on how complex the requirements are, they can be operated as simple single cells, semi-automated single cells or fully integrable automated cells.

Industrial production processes in sectors such as automotive, electronics or medtech often have to comply with the highest quality standards. Manufacturers must also conform to additional requirements for sustainability, traceability and efficiency that can only be met with advanced production technologies. Components and systems equipped with measurement technology are the key to improving production processes such as part joining and press-fitting, or end-of-line quality testing – and they also make these processes more transparent.

Kistler offers these solutions not only as single products or modules, but also as customized turnkey solutions – known as Smart Single Stations (SSTs). They are used in any situation where precise, quality-assured and traceable production processes play a critical part. Smart Single Stations can be used to perform a vast range of assignments – and in many cases, flexible and energy-efficient electromechanical joining systems from Kistler are integrated into the solution. Here are three examples of SST applications:

  • Manual workstation in a test line for electric motor production
  • Complex circuit board assembly for an electric pickup vehicle
  • Complete line production of valve islands for an active brake system

Highly individualized manual workstation for prototype production

A major European manufacturer of utility vehicles commissioned Kistler to supply a high-caliber customized manual workstation for its electric motor production. Its function: press-fitting of various rotor stacks onto a shaft. This application uses a special angled version of the NCFN NC joining system from Kistler with a high nominal joining force of 400 kN. To ensure ergonomic loading and unloading of the cell, the solution integrates a motorized precision-movable table that can accommodate components weighing up to 75 kg. "We also had to come up with solutions for a whole series of challenges in response to the safety and design specifications requested by our customer," says Wadim Weber, Sales Engineer for Smart Single Stations at Kistler. "An additional force transducer was integrated to cope with small forces and also to act as a reference sensor. What's more, the system features a handheld electronic scanner – so the measurement programs for the different rotor stacks can be called up directly from the maXYmos NC process monitoring system."

Once the shaft has been assembled successfully, the measurement results and production data are transmitted from Kistler maXYmos to the customer's MES. The system includes a customer-specified industrial PC that not only visualizes the process data from maXYmos, but also handles direct analysis of measurement data and can be used for other applications as well. Weber adds: "Due to factors such as the level of detail and the demanding safety and quality requirements for this project, a period of around one year was needed from receipt of the order to commissioning in the manufacturer's prototype production department."

Complex semi-automated circuit board assembly

In this case, the customer was a U.S. company that is driving ahead the electrification of the pickup trucks that are so popular in America. Kistler supplied a complex semi-automatic system to assemble semiconductor elements (insulated-gate bipolar transistors, or IGBTs). A process known as cold welding is used to permanently join a total of seven components of different types to the circuit board. "Following manual insertion, the individual positions are approached automatically so the joining processes can be performed with high precision and reliability," according to Klaus Hoffmann, SST Product Manager at Kistler. He continues: "The joining module had to be movable in the X and Y directions, and the tool had to be rotatable through 90 degrees. We implemented both these requirements exactly according to the customer's specifications. The operator simply has to remove the automatically assembled board at the end of the process."

To maximize the system's operating efficiency, an open design was chosen for the work area and two light barriers were installed for protection. The work surface is equipped with appropriate fixtures, and it can be retracted and extended with a handle to make assembly easier. "Thanks to this combination of a manual workstation with sophisticated process automation, we did a very successful job of meeting the customer's requirements for repeatability, precision and efficiency," Hoffmann adds.

Fully automated in-line system production

Multiple SSTs can be combined to form a complex line whenever required: this approach means that several assembly steps can be executed consecutively and simultaneously, so short cycle times are achieved. On behalf of the plant engineer of a major Chinese car manufacturer, Kistler is currently working to design combined assembly and testing cells for a fully automated production line. Comprising a total of six Smart Single Stations, this line to produce components of a braking and assistance system in electric cars should be able to assemble 450,000 systems per year with a cycle time of 30 seconds.

Cao Yue, Engineering Manager at Kistler in China, explains: "All in all, 12 electromechanical joining systems are used to assemble a complete valve island. Five stations with identical structures are used to press-fit and rivet 36 balls into each of six different valve bodies. Finally, at the sixth station, three more balls are joined at a different angle, and these are also riveted." As additional features, each Smart Single Station includes robot handling, automatic tool changing and air-sprung work surfaces. At the start of the line is a laser marking cell from Kistler with fully automated (robotic) loading; this cell also assigns a data matrix code to the valves being manufactured so as to ensure traceability. Chaining of the test cells and integration of the robotics are handled by the plant engineer in close collaboration with Kistler.

Flexible production technology – exactly as customers want it

Kistler's Smart Single Station concept is not limited to joining processes such as press-fitting, clinching, riveting or similar operations. In particular, optical testing technology can also be integrated flexibly into these systems to perform quality assurance: in this case, parts are inspected with the help of high-resolution cameras and the KiVision software from Kistler to ensure compliance with the highest quality standards – up to and including zero-defect production. Other technologies can also be integrated on request to create turnkey systems that meet customers' individual requirements: examples include automated fastener testing, e-motor testing and industry-specific process monitoring solutions for semiconductor production or medtech applications – to name only a few.

30.09.2022
Process automation in industrial production: Smart Single Stations for assembly and testing according to customers' specifications.
04.05.2022
Daimler Buses relies on MaDaM and jBEAM to further develop of its electric city buses.
11.04.2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14.01.2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18.11.2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12.10.2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14.09.2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09.09.2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03.09.2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02.07.2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22.06.2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02.06.2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26.04.2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13.04.2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22.03.2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08.02.2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05.10.2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18.09.2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20.08.2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22.07.2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09.06.2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15.11.2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23.10.2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15.08.2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17.07.2019
Turkey opts for weight enforcement with WIM technology from Kistler
24.06.2019
For the next manned flight to the moon: safety that can be measured
20.06.2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14.05.2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18.04.2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02.04.2019
NFL's Jaguars boost their fitness levels with Kistler.
25.03.2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18.03.2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17.12.2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27.11.2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10.10.2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08.10.2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31.08.2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14.08.2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16.07.2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11.04.2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14.11.2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11.08.2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04.01.2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22.12.2016
Kistler makes progress in vehicle development possible
22.12.2016
Kistler Sensor Correvit® SFII measures world record
20.12.2016
Kistler sensors deliver a maximum in data quality under any conditions.
07.11.2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05.10.2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17.08.2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19.02.2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04.11.2015
Piezoelectric Measurements with CompactRIO™
15.06.2015
Measurement Solutions for Automotive Test Systems
08.05.2015
Quality Assurance in the Automotive Industry
02.03.2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02.12.2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02.12.2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23.08.2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15.02.2011
End-to-end process monitoring for critical medical moldings
07.02.2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Контакты
Max 25 MB