Extremely robust miniature sensors for lunar missions

Temperatures above boiling point in the sunlight and in the shock-freezing range in the shade – these are normal, everyday conditions on the moon. Space is the environment that presents the most challenging possible conditions for technical equipment. In order for spacecraft to withstand these extremes and safely transport their crews, simulation tests are performed to guarantee reliability before the launch. And Kistler sensors, which are just a few millimeters in size and can brave even the harshest conditions, are the main focus of these tests.

Aerospace engineers are constantly walking a tightrope: extreme temperature ranges, major pressure fluctuations and high levels of vibration require durable materials that can make it through missions lasting several months without maintenance. Astronauts need enough room to live and carry out their research. At the same time, every additional gram of weight means more fuel is needed. Designing rockets is challenging – particularly because it is impossible to test them under real conditions: once the first engine ignites, there’s no turning back. This is why realistic simulations are used to guarantee safety on board. Testing equipment plays a decisive role in these simulations and must meet the strictest requirements both in terms of accuracy and reliability.

Crucial tests under extreme conditions

The main sources of stress on the materials are constant micro-vibrations and temperatures of up to 1,000°C around the engines. To sound out the limits, numerous aerospace research centers around the world rely on measurement technology from Kistler. Kistler sensors provide highly accurate measurements despite challenging conditions. They contain a quartz crystal that releases an electrical charge when a force is applied – and the charge is proportional to the force. Charge amplifiers make it possible to measure the pressure.

Let’s take, for example, a lunar mission: in this case, the European Space Agency (ESA) has been contracted by NASA to construct a propulsion module. When it comes to the most critical components, even minor deviations could result in major catastrophe. The focus is on the fuel valves in particular: the faster they open or close, the stronger the pressure surges will be. If the pressure rises above a specific limit, it could damage the fuel lines or relevant components – or, in the worst-case scenario, result in a fatal explosion.

The ESA’s test model for the simulations is equipped with numerous sensors from Kistler that measure the pressure in the fuel lines. This makes it possible to determine the optimal closing speed for the valves. So that these highly accurate sensors fit into the limited space inside the engines, they measure only five-and-a-half millimeters – and yet, despite their minuscule size, they guarantee the survival of the astronauts on board.

Razor-sharp images

Challenges in spacecraft design are not always immediately life-threatening, but even seemingly mundane issues can jeopardize the success of a mission. For example: unlike photos intended for personal use, blurred images on space expeditions can put the entire research project at risk. In the early years of space exploration, constant vibrations repeatedly caused cartographic imaging instruments to fail.

Given the long exposure times required for these images, even minimal vibrations can result in blurry photographs. These kinds of vibrations are barely perceptible by humans. They only become evident when photos are of low quality or cannot be used at all. In order to discover which instruments are permanently vibrating before the start of a mission, force sensors from Kistler are used to detect these types of micro-vibrations. This allows engineers to cushion the components in a targeted manner – so razor-sharp images are guaranteed despite challenging external conditions.

You might be interested also in:

Solutions from Kistler:
Singling out potentially overloaded vehicles is now a thing of the past. Today, these traffic offenders can be identified using automatic cameras.
“Everyone makes mistakes” – except in the field of medical technology. In the worst-case scenario, defects in the production of insulin pens could put patients’ safety at risk.
Stunned pigs, self-experimentation with showers of glass splinters – these were just some of the ways that vehicles were crash-tested in the first half of the 20th century. Today, crash testing involves high-tech crash dummies.
Preventing ligament tears with advanced technology: tailoring training and physiotherapy precisely to the athlete or patient using highly sophisticated measurement technology is becoming increasingly popular.
Turn, press or tilt: control elements such as hand brakes are put to the test before being installed in vehicles.
If the fasteners that secure the swiveling arm of a crane were to fail, people could be injured – or even lose their lives. Our inspection systems make sure that this could never happen.
Space is the environment that presents the most challenging possible conditions for technical equipment. In order for spacecraft to withstand these extremes and safely transport their crews, our sensors guarantee reliability before the launch.
While container ships, tankers and freighters are essential for the international transport of goods, they are also responsible for around 3 percent of global CO2 emissions. However, our sensors can significantly reduce this.
Контакты
Max 25 MB