Kistler showcases practical sensor integration for injection molds

Winterthur, 25 April 2017 – At the second international Moulding Expo in Stuttgart (from 30 May until 2 June 2017), the Kistler Group will show how easy it is to install the measurement technology needed for quality assurance in injection molds. As well as offering visitors the chance to try out a realistic example of this technology, Kistler's stand at the international trade fair will focus on two product groups that feature new developments: sensors that are insensitive to their installation position and multichannel connectors.

Sensor technology has to be integrated into molds in order to optimize the injection molding process. Growing numbers of injection molders see this as an essential requirement to prepare them for the 'digital revolution' – and to raise their product and process quality to new levels. Kistler identified this need at an early stage and at the Moulding Expo, the Group will showcase its solutions and tools designed specifically so that moldmakers can meet the requirements for integrated quality testing in the injection molding process.

Hands-on! Sensor installation in six steps

At Kistler's stand E61 in hall 5, customers and visitors can try this technology out for themselves and learn how easy it is to integrate Kistler's sensors into injection molds. In six steps, we'll show you how sensors are positioned, installed, cabled and function-tested. Kistler is constantly working to make it as simple as possible for moldmakers to integrate measurement technology into their processes. As well as special tools and an extensive range of accessories, the Swiss specialist offers practical support through worldwide service and training units on installation, commissioning and maintenance.

Multi-channel connector – with added new features

With the new Type 1722 multi-channel connectors, up to eight sensors can easily be linked up via single-wire plug connections – so there's no need for screwed joints, and the connector is more robust. The new, completely redesigned connecting elements ensure simple, error-tolerant installation and what's more, they are backwards-compatible with the predecessor version as regards con-nections and space requirements. Whether the four-channel or eight-channel version is used, changing the connection elements is a straightforward operation. This technology also enables combined pressure/temperature measurements (with the help of an additional thermocouple amplifier).

Installation made simple – because the sensor is insensitive to its installation position

Cavity pressure is one of the key factors in the injection molding process. Piezoelectric sensors from Kistler allow you to capture long-term measurements of this variable with high linearity, independently of temperature: a critical contribution to quality assurance. Depending on the installation conditions, part geometries and plastic materials, Kistler offers a wide choice of variants for direct in-cavity measurements, indirect and contact-free measurements, or combinations for contact tem-perature measurement.

At the Moulding Expo 2017, Kistler will unveil its new Type 6185 sensor, which is insensitive to its installation position. This product has been systematically adapted to confined installation conditions – its frontal diameter is a mere 2 mm – and its design ensures that measurement results cannot be falsified by lateral forces (such as those caused by difficult installation conditions). The results: maximum precision with simplified installation. With this sensor too, signal transmission can be implemented with a conductive spacer sleeve instead of via cables.

Piezoelectric sensor technology: the basis for process monitoring

To be sure that their machines will meet the requirements of the future, more and more manufacturers are turning to integrated quality assurance in the injection molding process. Kistler's ComoNeo monitoring system offers a reliable solution for monitoring cavity pressure and forecasting part quality. However, there is one key requirement for the sought-after goal of zero-defect production: sensor technology must be suitably integrated at mold level. The Kistler Group will demonstrate the wide-ranging options for achieving this goal – and will highlight some points to note during installation – at the trade fair in Stuttgart from 30 May until 2 June. Anyone interested is warmly invited to visit stand E61 in hall 5 at the fair.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Overcoming the complexities of RTM – with Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.