Dörken opts for test stands from Kistler to determine friction coefficients

Corrosion-proof fasteners are essential in the automotive industry, and they perform an equally critical function in wind turbines. Thanks to its choice of four ANALYSE systems from Kistler as test stands to determine friction coefficients, Dörken can meet ever-stricter test requirements and ensure compliance with uniform standards throughout the world – especially for its zinc flake coatings.

How is it that a fastener testing laboratory is located on the site of a chemical company that generates most of its sales (totaling around EUR 300 million) from paints, varnishes and laminated sheets for roofs? Founded back in 1892, Ewald Dörken AG has its headquarters in the German town of Herdecke (State of North Rhine-Westphalia). As well as construction finishing and coatings of all types, the company's expertise also includes corrosion protection – with a special focus on fasteners. Virtually all the fasteners in a car are coated, and what are known as zinc flake coatings are used for this purpose in most cases: Small steel components are cleaned and dipped in an immersion bath containing the coating; the excess is then spun off, and the final stage of the process is baking. As zinc is less noble, it protects the coated metals – and the same process is also used for large M24 anchor bolts in wind turbines.

However, this process is not carried out on Dörken's own site – instead, it is performed by coating service providers. These independent companies and licensees are supplied and audited by Dörken (some of them also use different fastener test stands). Its worldwide network includes over 200 of these “coaters” who ensure that the right corrosion protection is applied to fasteners, nuts and other parts for the automotive industry, the wind power and mechanical engineering sectors, and many other special-purpose applications. As well as zinc flake coatings, there are other technologies such as coil coating and galvanic coating – but these methods are not so important in terms of volume.

The easy way to determine the friction coefficient

It is also essential to ensure that the fasteners can still be processed after they have been coated: for this purpose, friction coefficient tests are carried out continuously in the Herdecke laboratory and at three other facilities in China, Korea and the USA. An ANALYSE system from Kistler is operated in each of these Dörken Tech Centers. These test stands can perform large numbers of friction coefficient tests that meet the specifications required by the automotive industry and many other sectors. Michael Stähler, Lead Technologist Fasteners, has been with the company for 15 years and is responsible for laboratory equipment, training, sales and advice for customers. He explains:

Thanks to the test stands from Kistler, we can accurately and reliably determine the friction coefficient – the link between torque and preloading force. One point to note here is that different customers or countries prefer different friction coefficient windows. These are influenced by lubrication, which makes the overall picture somewhat complex. Increasingly efficient processes in the automotive industry are presenting quite a few challenges for measurement technology – but with the ANALYSE system from Kistler, we have no problems in meeting customers’ standards that require pre-tightening at up to 700 rpm.”

Michael Stähler, Lead Technologist Fasteners at Dörken

 

Different test methods have to be applied depending on the fastener and the specification: faster or slower tightening, and fastening in relation to specific reference parts with steel, aluminum or CDC (cathodic dip-coated) surfaces. This calls for a system that can be used with some degree of flexibility, as well as software that reduces the user's workload to the minimum and makes the process easier. Oliver Jakob, Channel Manager Fastening Technology EMEA at Kistler, outlines the benefits of ANALYSE systems: “Our test stands for determining the friction coefficients of detachable fasteners can be assembled flexibly from a variety of modules and components – also, for example, they can be equipped with different drives. Our testXpert software includes both predefined and freely configurable test procedures, and it's designed to be user-friendly."

Kistler's global presence and reputation persuaded Dörken to opt for ANALYSE systems at an early stage. The test stand at the company's German headquarters was expanded in 2015 and then in 2019, the USA became the fourth location for friction coefficient determination. “That means we can now carry out uniform testing in all our Tech Centers: the testing regulations we develop here at headquarters can be rolled out globally via Kistler software, with guaranteed process reliability,” Stähler adds. Another advantage: regular calibration ensures reliable compliance with customer standards that specify certain reference parts down to the last detail, for example. Organizations such as the German Fastener Association (DSV) – where Stähler chairs the “Surfaces” working group – also conduct round-robin tests to assess the comparability of test stands with different measurement principles.

The ANALYSE system: uniform, efficient and modular

“Our four ANALYSE systems from Kistler also give us excellent international positioning. They stand us in good stead with our customers. High measurement frequency, excellent resolution and direct evaluation – this is a combination that leaves almost nothing to be desired. What's more, all the data and measured values – even from previous software versions – are stored and traceable. That's quite reassuring not only for us, but also for the coaters and end customers – and into the bargain, there's the good service that Kistler provides, available everywhere in the world." 

Which trends are shaping the future of fastening technology, and how is the market likely to develop in the coming years? Stähler points to increasing test requirements imposed by the automotive industry, such as faster tightening and multiple fastening; he also foresees other developments that will depend on factors such as the availability of certain materials. He quotes a specific example: "Ultrasonic control of tightening during the fastening process is an interesting technology, even though it's not all that relevant for us in the corrosion protection segment. With this technique, the preloading force is determined continuously from the change in runtime on the fastener, which is measured ultrasonically. At present, however, this process is tied to general conditions such as plane-parallel areas on the fastener heads and ends.” Oliver Jakob adds a final comment: “We can already feed ultrasonic signals into our ANALYSE systems, and we can use suitable calculation functions to establish a direct relationship between the preloading force measured by the force sensor and the elongation of the fastener measured via ultrasound.”

14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
15/06/2015
Measurement Solutions for Automotive Test Systems
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contacto
Max 25 MB