Marine engines: efficiency down to the last detail

While container ships, tankers and freighters are essential for the international transport of goods, they are also responsible for around 3 percent of global CO2 emissions. Sensors from Kistler can be installed in marine engines to reduce these emissions: by monitoring the engines, they save significant amounts of fuel and CO2, thereby reducing the ecological impact on the environment and relieving the financial burden on shipping companies. 

90 percent of all goods are transported by ship across the world’s oceans every day. Large marine engines are used to propel these vessels and provide the necessary power on board. Depending on the size of the ship, these large engines can be up to 16 meters high and consume up to 300,000 liters of heavy fuel oil per container ship per day when operating around the clock under full load. But where there are high levels of consumption, there is also savings potential. In fact, it is possible to cut the total annual fuel consumption by around 2 percent simply by monitoring the ships’ large engines with special cylinder pressure sensors. In the largest marine engines, these sensors make it possible to reduce harmful CO2 emissions by up to 20 tonnes per engine per day, which is equivalent to the annual carbon footprint of 2.5 residents of Germany.

Internal and external regulation

The sensors are installed in the cylinder – this is the location of the piston, which is connected to the crankshaft and which drives the engine with its upward and downward movements. These upward and downward movements are powered by the explosive combustion of the fuel mixture, which generates pressure in the cylinder. The sensor’s task is to monitor the pressure in real time during this process so the engine control system can compensate for pressure differences between the cylinders. The more even this pressure is, the less fuel is required to drive the engine – and the volume of CO2 emissions is also reduced. 

While marine engines traditionally burn heavy fuel oil (HFO) or marine diesel oil (MDO), the importance of liquefied natural gas (LNG) is increasing steadily due to ever-stricter environmental regulations. A current example of this shift is what are known as dual-fuel engines. Engines of this type can be converted from standard liquid fuels to liquefied natural gas (LNG), therefore helping to reduce emissions. To ensure that dual-fuel engines can provide maximum efficiency and optimal power, their internal combustion processes must be continually monitored and regulated. And this is where extremely robust cylinder pressure sensors from Kistler in Winterthur come into play once again. 

While experts cannot say for sure which environment-friendly alternatives will be used to power the marine engines on our oceans ten years from now, one thing is already certain today – the smallest parts can have the biggest impact. Sensors from Kistler will remain an essential component of the marine engines of the future, regardless of whether they run on methanol, ammonia or biodiesel.

You might be interested also in:

Solutions from Kistler:
Singling out potentially overloaded vehicles is now a thing of the past. Today, these traffic offenders can be identified using automatic cameras.
“Everyone makes mistakes” – except in the field of medical technology. In the worst-case scenario, defects in the production of insulin pens could put patients’ safety at risk.
Stunned pigs, self-experimentation with showers of glass splinters – these were just some of the ways that vehicles were crash-tested in the first half of the 20th century. Today, crash testing involves high-tech crash dummies.
Preventing ligament tears with advanced technology: tailoring training and physiotherapy precisely to the athlete or patient using highly sophisticated measurement technology is becoming increasingly popular.
Turn, press or tilt: control elements such as hand brakes are put to the test before being installed in vehicles.
If the fasteners that secure the swiveling arm of a crane were to fail, people could be injured – or even lose their lives. Our inspection systems make sure that this could never happen.
Space is the environment that presents the most challenging possible conditions for technical equipment. In order for spacecraft to withstand these extremes and safely transport their crews, our sensors guarantee reliability before the launch.
While container ships, tankers and freighters are essential for the international transport of goods, they are also responsible for around 3 percent of global CO2 emissions. However, our sensors can significantly reduce this.
연락처
Max 25 MB