Guinea pigs – made of plastic!

Stunned pigs and self-experimentation with showers of glass splinters – life in the early days of vehicle occupant testing was certainly an adventure! But nowadays, all that has changed thanks to crash test dummies: high-tech models of human beings that provide critical input for modern vehicle safety. Inside these plastic research assistants, hundreds of sensors capture the accelerations and forces that occur during collisions. Kistler, the measurement technology specialist, is building the latest generation of frontal dummies that can even reproduce the facial injuries caused when a vehicle occupant is hurled into an airbag.

Until the middle of the 20th century, it was taken for granted that the human body was no match for the forces generated during car accidents. There was general acceptance that road accidents would inevitably cause deaths – and back then, there was no shortage of reasons for this assumption: hard, sharp-edged metal fittings and the general absence of safety belts, to name but two. Then in the early 1950s, this widely-held belief prompted researchers to carry out the first accident tests. They had no hesitation in strapping human corpses into cockpits to study typical injuries, both internal and external. These experiments were followed by tests where volunteers were exposed to emergency braking, or even showers of glass splinters. But the pain threshold was soon reached – quite literally! – so the engineers went on to place stunned pigs, bears or monkeys behind the wheel for the more brutal tests.

Sensors to the rescue

Humans and animals were eventually spared from these perils by the arrival of Sierra Sam, the world's first crash test dummy. Developed for the United States Air Force back in 1949, Sierra Sam was the prototype for subsequent dummy models that were put to use for road crash tests just a few years later. To replicate reality as closely as possible, dummies came in all shapes and sizes: male and female, short and tall, young and old. However, what really revolutionized crash testing was not so much the variety of versions that were available, but the integration of technology into the dummies.

This trend began in the early 1970s when the Hybrid I to III series of models from General Motors were fitted with the first sensors to measure force and acceleration in their heads, torsos and thighs. As technology improved, engineers equipped the models with additional sensors in parts of the body where injuries could prove fatal, such as the neck or the spinal column. Angular rate sensors also made it possible to measure bending of the limbs due to a collision.

Dummies get smart

For many years, the Hybrid III was regarded as the universal standard in the industry – until THOR pushed it out of the driver's seat. THOR – the Test Device for Human Occupant Restraint – differs from its predecessor in many ways: with the help of extra facial sensors, for example, it achieves better resolution of the distributed forces that are generated when an occupant is flung into an airbag. THOR represents an average adult male, weighing in at 77 kilograms and with a height of 1.76 meters.

To prepare this latest-generation crash dummy for real use, the measurement experts at Kistler equipped it with data acquisition capacity for up to 288 measuring channels. Data is speedily exported from the wreck via one single Ethernet cable in the dummy's thorax. By contrast, THOR's forerunners with their tangle of wires looked more like puppets on many strings. Since 2018, Kistler has carried out the complete production process for THOR dummies at its Heidelberg site.

Despite this impressive progress, dummy development has certainly not reached the end of the road yet: these "accident dolls" will become even smarter as time goes on, and further improvements such as more realistic replication of injuries to internal organs will become possible. Long ago, people believed that a car accident meant certain death – but thanks to crash dummies, that era is now well and truly over.

You might be interested also in:

Solutions from Kistler:
Singling out potentially overloaded vehicles is now a thing of the past. Today, these traffic offenders can be identified using automatic cameras.
“Everyone makes mistakes” – except in the field of medical technology. In the worst-case scenario, defects in the production of insulin pens could put patients’ safety at risk.
Stunned pigs, self-experimentation with showers of glass splinters – these were just some of the ways that vehicles were crash-tested in the first half of the 20th century. Today, crash testing involves high-tech crash dummies.
Preventing ligament tears with advanced technology: tailoring training and physiotherapy precisely to the athlete or patient using highly sophisticated measurement technology is becoming increasingly popular.
Turn, press or tilt: control elements such as hand brakes are put to the test before being installed in vehicles.
If the fasteners that secure the swiveling arm of a crane were to fail, people could be injured – or even lose their lives. Our inspection systems make sure that this could never happen.
Space is the environment that presents the most challenging possible conditions for technical equipment. In order for spacecraft to withstand these extremes and safely transport their crews, our sensors guarantee reliability before the launch.
연락처
Max 25 MB