Two-stage process monitoring for excellent plastics from Tessy

Zero-defect production with 100% quality assurance is the ultimate goal of every plastics processing operation. Reliable process control is the key to achieving this goal. The solution? Piezoelectric sensors and systems from Kistler. They measure and analyze the cavity pressure during the injection molding process while monitoring the process directly in the cavity mold and separating rejects.

Tessy Plastics, founded in 1973 with several facilities located in Central New York, is one of the largest custom medical device and consumer component contract manufacturing suppliers in the Northeast (U.S.). They engineer, manufacture, assemble and distribute a very wide range of products. Intensely committed to quality, Tessy embraces Scientific Injection Molding (SIM) to allow them to define and optimize their molding process from start to finish.

Ben Passetti, Research & Development Engineer with 15 years of experience at Tessy Plastics, takes the quality of their molding parts very seriously. Eliminating defects in the assembly monitoring process easily with guaranteed results is key. This means that reliable, efficient measurement equipment is an absolute, essential factor in order to provide their customers who take delivery of millions of their products, with excellent quality assurance. Passetti says, “Our product portfolio is split 50/50 medical/consumer. We focus primarily on value-added, high dollar items with very complex manufacturing tight tolerances - everything from 720 tons down to micro molding so our molding portfolio is pretty large from a versatility standpoint. We have a focus on micro molding in the medical sector because it is challenging and difficult - we can accomplish tight tolerances with the tooling partners we have put in place.”

Overcoming the complexities of injection molding with Kistler

Continuous process monitoring and control of the entire production measuring chain is essential to meeting today's demanding industry requirements. By combining Kistler process monitoring systems and sensors, one can not only achieve optimized process efficiency and quality assurance, but also gain a competitive edge that raises the bar. This has proven true for Tessy. Passetti points out, “There has been a visible shift in the plastic molding market within the past five years. Customers are more educated and understand a lot more about the injection molding process than in the past and they are actively searching for more technological savvy solutions. 

After reviewing Kistler's extensive product portfolio, Tessy decided to implement and combine several Kistler products in order to achieve a competitive edge. Jay Sklenka, Field Sales Engineer at Kistler, explains “Tessy has been using several Kistler products over the past five years; not just for injection molding but for assembly as well. This includes the Kistler ComoNeo, maXYmos, load cells, and pressure sensors. They are also using our amplifiers mounted on the injection molding machines to bring the pressure signals back into the machine controller.”

From an assembly standpoint, we liked that Kistler pressure sensors allow us to detect the force that drives the components back and forth so we can make any necessary adjustments with reliable, visible, sustainable results."

Ben Passetti, Research & Development Engineer at Tessy Plastics

 

“We added ComoNeo from Kistler to give us a better understanding of how the component actually looks like to ensure they are fully formed and are able to move into the production stage with 100% zero-defect results. We also chose to implement the process monitoring system ComoNeo because prior to its implementation, we were struggling to understand what was happening in the mold itself to achieve accuracy and repeatability.” The result: control of the outcome throughout different stages of the value chain.

Quality assurance with reliable, repeatable, controllable results

Passetti describes how Kistler pressure sensors are utilized in their injection molding process: “In one of the first stages of the molding process for our medical components, the parts are inserted with the automation directly into the medical component. Here, we are monitoring the cavity pressure to ensure that parts are fully formed and to ensure that we do not overpack the mold using a visible envelope/reference curve over the injection profile so that we can monitor the fill. 

When asked if he feels Kistler solutions have provided Tessy with useful tools to achieve success, Passetti exclaims, “Absolutely! We are using Kistler process monitoring systems and sensors for our documentation and providing invaluable information to our processes. Without it, we would likely struggle to meet the demands of today's market from a quality, efficiency, and cost-effectiveness standpoint. Kistler is probably the most advanced sensor company.” 

Shaping the future with process monitoring systems and sensors of Kistler

Working together with Kistler has proven beneficial by drastically reducing scrap and improving Tessy's overall success rate. Looking back at the resulting reduced rate of return and increased ROI over the years, Passetti happily notes, “We are definitely satisfied with Kistler solutions. We at Tessy have been pushing the boundaries of facility size limitations for our machinery. We know that Kistler is continuously working to provide smaller systems and sensors to fit this need, especially on the micro-scale side, and we are happy with how much easier it allows for their integration into our machinery.” 

Choosing to partner with Kistler in order to achieve continued success has inevitably paved the way for future success and process improvement at Tessy. Passetti concludes, “I would say, from my experience, that the growing market trend favors smart technology solutions like those offered by Kistler. At Tessy, our plan is to not only integrate more Kistler pressure sensors and systems into future molds but also to retro-fit our existing molds with Kistler sensors as well. There are very few companies in the U.S. that are using micro molding in combination with sensor technology. I believe that Tessy remains ahead of the competition in terms of sensor integration on a micro-scale and micro molding machinery thanks to Kistler technology.”

2021. 6. 22.
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
2021. 6. 2.
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
2021. 4. 26.
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
2021. 4. 13.
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
2021. 3. 22.
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
2021. 2. 8.
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
2020. 10. 5.
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
2020. 9. 18.
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
2020. 8. 20.
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
2020. 7. 22.
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
2020. 6. 9.
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
2019. 11. 15.
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
2019. 10. 23.
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
2019. 8. 15.
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
2019. 7. 17.
Turkey opts for weight enforcement with WIM technology from Kistler
2019. 6. 24.
For the next manned flight to the moon: safety that can be measured
2019. 6. 20.
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
2019. 5. 14.
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
2019. 4. 18.
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
2019. 4. 2.
NFL's Jaguars boost their fitness levels with Kistler.
2019. 3. 25.
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
2019. 3. 18.
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
2018. 12. 17.
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
2018. 11. 27.
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
2018. 10. 10.
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
2018. 10. 8.
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
2018. 8. 31.
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
2018. 8. 14.
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
2018. 7. 16.
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
2018. 4. 11.
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
2017. 11. 14.
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
2017. 8. 11.
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
2017. 1. 4.
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
2016. 12. 22.
Kistler makes progress in vehicle development possible
2016. 12. 22.
Kistler Sensor Correvit® SFII measures world record
2016. 12. 20.
Kistler sensors deliver a maximum in data quality under any conditions.
2016. 11. 7.
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
2016. 10. 5.
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
2016. 8. 17.
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2016. 2. 19.
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
2015. 11. 4.
Piezoelectric Measurements with CompactRIO™
2015. 6. 15.
Measurement Solutions for Automotive Test Systems
2015. 5. 8.
Quality Assurance in the Automotive Industry
2015. 3. 2.
How Brose improves the quality of its two-component production and automatically separates defective parts
2014. 12. 2.
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
2014. 12. 2.
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
2011. 8. 23.
HEWI and its Customers Benefit from Cavity Pressure Technology
2011. 2. 15.
End-to-end process monitoring for critical medical moldings
2011. 2. 7.
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
연락처
Max 25 MB